This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM2634:ADC0通道 AIN0不工作

Guru**** 2752895 points

Other Parts Discussed in Thread: TMDSCNCD263

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1129500/am2634-adc0-channel-ain0-not-working

器件型号:AM2634
主题中讨论的其他器件:TMDSCNCD263

您好!

我正在使用 TMDSCNCD263评估板并尝试读取 ADC0 AIN0、但它无法正常工作。 我已经检查了引脚上的电压、它大约为10mV、但数字读数始终高于2400、也就是振铃。

ADC 设置为:

.base = CSL_CONTROLSS_ADC0_U_BASE、
.clkPrescale = ADC_CLK_DIV_4_0、
.resolution = ADC_resolution_12位、
signalMode = ADC_MODE_Single_ended、
.priMode = ADC_PRI_All_round_Robin、
.burstTrigger = ADC_TRIGGER_SW_ONLY、
.burstSize = 1、
.soNumber = ADC_SOC_NUMBER0、
触发= ADC_TRIGGER_EPWM0_SOCA、
通道= ADC_CH_ADCIN0、
.sampleWindow = 15、
等触发器= ADC_INT_SOC_TRIGGER_NONE、

我能够完美地读取 ADC0 AIN2、AIN4

谢谢

Baljeet