This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] EK-TM4C1294XL:USB DFU

Guru**** 2923680 points

Other Parts Discussed in Thread: EK-TM4C1294XL, EK-TM4C123GXL, TM4C1294NCPDT

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/992729/ek-tm4c1294xl-usb-dfu

器件型号:EK-TM4C1294XL
主题中讨论的其他器件: EK-TM4C123GXLTM4C1294NCPDT

我正在尝试降低使用 DFU 的步骤。 我尝试了以下操作:

1.从项目 boot_serial 开始

2.在 bl_config.h 中启用 USB update define 语句

3.将项目和闪存构建到 EK-TM4C1294XL 中

4. dfuprog -m 切换到 DFU 模式

5. dfuprog -e 在 DFU 模式下仅显示一个器件

6. dfuprog -i deviceNum -f program.bin -a 0x1800可通过命令行和 LM 闪存编程器工作

在器件管理器中、不再看到 Stellaris COM 端口。 出了什么问题?

如果我尝试将跳线更改为 OTG 模式并将 USB 电缆连接到 USB 端口 U7、我也看不到任何 COM 端口。

非常感谢您帮助您正确地执行序列。 我希望能够在需要时进入和退出 DFU 模式、并且还能在需要时使用 Stellaris ICDI。

谢谢、

Priya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    [引用 userid="318358" URL"~/support/microcontrollers/other/f/other-microcontrollers-forum/992729/ek-tm4c1294xl-usb-dfu ]\n 在器件管理器中、不再看到 Stellaris COM 端口。 出现什么问题?[/报价]

    听起来就像对 ICDI MCU 进行了编程、而不是对您的目标进行了编程。  

    [引用 userid="318358" URL"~/support/microcontrollers/other/f/other-microcontrollers-forum/992729/ek-tm4c1294xl-usb-dfu "]

    4. dfuprog -m 切换到 DFU 模式

    5. dfuprog -e 在 DFU 模式下仅显示一个器件

    [/报价]

    如果步骤4是 dfuprog -i index -m、则您执行了以下相反步骤:

    //! To illustrate runtime DFU capability, use the <tt>dfuprog</tt> tool which
    //! is part of the Tiva Windows USB Examples package (SW-USB-win-xxxx.msi)
    //! Assuming this package is installed in the default location, the
    //! <tt>dfuprog</tt> executable can be found in the
    //! <tt>C:/Program Files/Texas Instruments/Tiva/usb_examples</tt> or 
    //! <tt>C:/Program Files (x86)/Texas Instruments/Tiva/usb_examples</tt>
    //! directory.
    //!
    //! With the device connected to your PC and the device driver installed, enter
    //! the following command to enumerate DFU devices:
    //!
    //! <tt>dfuprog -e</tt>
    //!
    //! This will list all DFU-capable devices found and you should see that you
    //! have one or two devices available which are in ``Runtime'' mode.
    //!
    //! *** IMPORTANT - PLEASE READ ***
    //! If you see two devices, it is strongly recommended that you disconnect
    //! ICDI debug port from the PC, and change the POWER_SELECT jumper (JP1) 
    //! from 'ICDI' to 'OTG' in order to power the LaunchPad from the USB
    //! OTG port. The reason for this is that the ICDI chip on the board is
    //! a DFU-capable TM4C129x device, and if not careful, the firmware on the
    //! ICDI chip could be accidently erased which can not restored easily.
    //! As a result, debug capabilities would be lost!
    //! *** IMPORTANT - PLEASE READ ***
    //!
    //! If IDCI debug port is disconnected from your PC, you should see only one
    //! device from above command, and its index should be 0, and should be named
    //! as ``Mouse with Device Firmware Upgrade''. 
    //! If for any reason you need to keep the ICDI port connected, the above
    //! command should show two devices. The second device is probably named as
    //! ``In-Circuit Debug interface'', and we need to be careful not to update
    //! the firmware on that device. So please take careful note of the index for
    //! the device ``Mouse with Device Firmware Upgrade'', it could be 0 or 1, we
    //! will need this index number for the following command. 
    //! Entering the following command will switch this device into DFU mode and
    //! leave it ready to receive a new firmware image:
    //!
    //! <tt>dfuprog -i index -m</tt>
    //!
    //! After entering this command, you should notice that the device disconnects
    //! from the USB bus and reconnects again.  Running ``<tt>dfuprog -e</tt>'' a
    //! second time will show that the device is now in DFU mode and ready to
    //! receive downloads.  At this point, either LM Flash Programmer or dfuprog
    //! may be used to send a new application binary to the device.

    [引用 userid="318358" URL"~/support/microcontrollers/other/f/other-microcontrollers-forum/992729/ek-tm4c1294xl-usb-dfu "]如果我尝试将跳线更改为 OTG 模式并将 USB 电缆连接到 USB 端口 U7,我也看不到任何 COM 端口。

    将 ICDI 线缆插入电路板的调试端、使用 LM 闪存编程器并转至 其他 实用程序、然后在此选项卡的底部、您将看到  ICDI 固件更新下面的按钮。 单击 该“更新”按钮以恢复 ICDI。

    [引用 userid="318358" URL"~/support/microcontrollers/other/f/other-microcontrollers-forum/992729/ek-tm4c1294xl-usb-dfu ]非常感谢您帮助您按正确的顺序执行操作。 我希望能够在需要时进入和退出 DFU 模式、并且还能在需要时使用 Stellaris ICDI。[/QUERP]

    按照我在上面发布的顺序执行操作、该顺序来自我们的 boot_demo_usb 示例、您应该可以正常运行。 尽管还有一件事:

    [引用 userid="318358" URL"~/support/microcontrollers/other/f/other-microcontrollers-forum/992729/ek-tm4c1294xl-usb-dfu ]6. dfuprog -i deviceNum -f program.bin -a 0x1800可从命令行和 LM 闪存编程器中工作[/quot]

    对于 TM4C129x、应为0x4000、因为这是 MCU 中闪存块的最小大小。 0x1800用于 TM4C123x MCU。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    为清楚起见、您能否按正确的顺序发布步骤列表?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    我做了-请通读我的帖子上的代码块。 这是完整序列、包括如何避免在 ICDI 上触发 DFU。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这是我尝试过的。 我在文件下载结束时遇到错误。 这意味着什么?

    适用于 USB DFU 的 EK-TM4C1294 XL 步骤

    1. 从项目 boot_serial 开始
    2. 在 bl_config.h 中启用 USB update define 语句
    3. 将工程和闪存构建到 EK-TM4C1294XL 中
    4. dfuprog -e 确认在 DFU 模式下仅显示一个器件
    5. dfuprog -m 切换到 DFU 模式
    6. dfuprog -i deviceNum -f program.bin -a 0x4000可从命令行和 LM 闪存编程器中工作

     

    文件下载期间报告的错误 DFU_ERR_UNKNOWN (-4)是什么意思?

    要切换到 ICDI 模式、LM 闪存编程器其他实用程序会更新 ICDI 固件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    我执行了这些步骤、但对步骤5进行了一次修改:

    dfuprog -I 1 -m

    您应该对-m 命令使用 dfuprog -i。

    但除了这一变化之外、我也做了你所做的每一步、它对我很有用。

    我不确定到底是什么触发 了 DFU_ERR_UNKNOWN (-4)... 通常、这意味着 USB 接口不可用、就像器件由于某种原因没有响应。 如果您没有在 dfuprog -m 上执行-i、您可能已经触发 ICDI 再次进入引导模式?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我将 bootserial 闪存到 EK 中。 当我键入 dfuprog -e 时、只有一个器件显示 ICDI 接口、请参阅下面粘贴的捕获。 那么、当我切换到引导加载程序模式时、进入引导加载程序的是 ICDI 吗? 如果其它 USB 设备未列出索引、如何访问该设备?

    在我明白这一点之前、我犹豫是否要尝试另一种新的 EK。

    谢谢、

    Priya


    USB 设备固件升级示例
    版权所有(c) 2008-2017 Texas Instruments Incorporated。 保留所有权利。

    正在扫描支持的 DFU 器件的 USB 总线...


    <<<设备0 >>

    VID:0x1cbe PID:0x00fd
    器件名称:电路内调试接口
    制造商:德州仪器(TI)
    DFU 接口:< >
    序列号:0F00D8DC
    最大传输数:1024字节
    模式:运行时
    属性:
    将断开:是
    清单容错:是
    可上传:是
    可下载:是

    找到1个器件。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    是否有 USB 电缆插入与调试端口相对的目标 USB 端口?

    如果您只看到一个器件、那么这肯定是一个问题、需要有两个器件、或者只有一个器件、 则不应是 ICDI -如果您将 USB 电缆插入目标 USB 端口并将 LaunchPad 的电源跳线更改为由 OTG 而不是 ICDI 供电、就会出现这种情况。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我插入的唯一电缆是 调试 USB 端口。 我尚未将跳线设置更改为 OTG。 在闪存引导串行之后、我只看到一个器件、即 ICDI。  

    有一次、我尝试使用目标 USB 和 OTG 跳线、但设备管理器无法识别此目标 USB 端口。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    USB DFU 能通过目标 USB 端口工作。 无法通过 ICDI 端口使其正常工作。

    您有两根电缆吗? 您可以连接两个端口吗?

    如果不是、您将需要来回更改。

    如果您正确设置了项目、设备管理器应该会识别它。 您是否安装了 TivaWare 2.2.0.295中的最新驱动程序? 您可能需要在设备管理器中手动更新驱动程序。

    您能否发布 bl_config.h 文件? 我可以对其进行审阅。 如果可能、将文件作为附件发布、因为文件太长、谢谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    e2e.ti.com/.../6562.bl_5F00_config.h

    随附 bl_config.h。 我将获得另一根电缆并尝试。

    在器件管理器或 dfuprog 中看不到目标 USB 端口上的 COM 端口。 我的配置文件中必须缺少一些内容。  

    谢谢、

    Priya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    BL_CONFIG 有一些错误、这就是端口枚举的原因。

    1) 1)不启用 USB_MUX 功能、注释掉所有这些功能。

    2) 2)您在此处选择了错误的端口:

    //#define USB_DP_PORT            GPIO_PORTL_BASE            // For EK-TM4C1294XL
    #define USB_DP_PORT            GPIO_PORTD_BASE            // For EK-TM4C1294XL

    端口 D 用于 EK-TM4C123GXL。

    我正在为 EK-TM4C1294XL 连接我的 BL_CONFIG 我用于为以下帖子执行 USB DFU:

    e2e.ti.com/.../3630.bl_5F00_config.h

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您提供更正后的配置文件。 当我刷写 boot_serial 时、我仍然只能看到 ICDI 接口。 我有2条 USB 电缆连接到 EK。 我没有选择 OTG 跳线。 设置配置文件时必须执行更多操作。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    您在设备管理器中看到了什么? 您是否有无法在任何位置枚举的 USB 端口?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我继续仅将 ICDI 视为 USB 器件。 我还没有看到目标 USB。 设备管理器屏幕截图已附加。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    您是否使用了我的确切配置文件或尝试进行更改? 我再次进行了测试、我看到显示了 DFU 接口。

    用于 boot_serial 工程的目标器件是 TM4C1294NCPDT 吗?

    如果您使用  dfuprog -e、会出现什么情况?

    您能否尝试对我确认可以在硬件上工作的二进制文件进行编程?

    e2e.ti.com/.../7024.boot_5F00_serial.bin

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    使用 您发送的 bin 文件、我可以看到两个 USB 器件、并使用 DFU 对 bin 文件进行编程。 之后、我返回到我的引导串行、设备管理器现在显示了所连接的内容。

    我尝试更新了 TIVaware2.2.0.295 Windows 驱动程序中的 Windows 驱动程序、也许我需要运行另一个补丁?

    或者、如果您可以为 EK-TM4C1294XL 导出 boot_serial 工程、我将使用它。

    谢谢、

    Priya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    拉尔夫

    请告诉我、如果显示未知的器件描述符、我可以做什么。 我擦除了项目并将其重新导入到了工作区中、更新了驱动程序、卸载了未知的 USB 器件并扫描了硬件更改。 它仍显示为未知 USB 设备。 我需要能够在我的设置中编译和下载 boot_serial。 谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    当您尝试更新驱动程序时、您是否访问了未知器件的属性、转至驱动程序下、选择"更新驱动程序"、然后手动浏览您的计算机以指向 TivaWare windows_drivers 文件夹?

    现在 boot_serial 可能正常工作、问题出在枚举。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是、并且我在执行此操作时收到的消息是此设备的最佳驱动程序已安装。  

    修复枚举问题的策略是什么?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    尝试在这里拍摄一段长时间的照片,但在这里试一下司机: http://software-dl.ti.com/tiva-c/SW-TM4C/latest/exports/SW-TM4C-2.1.4.178.PATCH-1.0.zip

    如果无法正常工作、我建议先尝试另一条 USB 电缆、然后再尝试重新启动您的 PC。

    我以前看到过故障 USB 电缆会导致枚举问题(其中一些是 LaunchPad 套件附带的电缆)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    拉尔夫

    我尝试了所有操作-卸载未知设备、重新启动 PC、使用全新的 EK 应用补丁。 我在 Tiva 1294 EKS......上度过了一个幸运的时光 枚举仍然失败。  请在此处提供帮助吗? 我不知道还有什么要尝试的。

    谢谢、

    Priya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    很抱歉、您遇到了这样的问题。 所有这些测试是否都使用我发送的二进制文件?

    我提出这一问题是因为我在仔细检查可能的问题、并且报告了 TM4C1294 EK 的另一个 USB DFU 问题、但它不应影响我发送的.bin 文件。 在任何情况下、您都应该在您的末尾进行此更新

    在 bl_usbfuncs.c 中、找到第619行、并替换以下现有行:

    HWREG(USB0_BASE + USB_O_CC) = (USB_CC_CLKEN | (7 << USB_CC_CLKDIV_S));

    具有以下行:

    HWREG(USB0_BASE + USB_O_CC) = (USB_CC_CLKEN | (3 << USB_CC_CLKDIV_S));

    如果您使用的是自己的项目、请尝试重新编译并重新加载、因为它解决了闪存引导加载程序的 USB 时钟配置问题。

    我看到的另一个可能影响您的.bin 文件未解决的问题是、在 BL_CONFIG 中、闪存页大小设置不正确。 它应该是:

    #define FLASH_PAGE_SIZE         0x00004000

    我要附加一个新的二进制文件、该文件已解析:

    e2e.ti.com/.../2806.boot_5F00_serial.bin

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我仍在尝试使工作区上的 boot_serial 编译正常工作。 我更改了 USB 时钟和闪存页大小。 设备管理器仍显示未知的 USB 设备(这次配置描述符无效)。 您的 bin 文件正常工作。 您能否为 EK-TM4C1294 XL 提供导出的项目?

    我使用了您发送的确切 bl_config.h 文件。

    谢谢、

    Priya

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    查找随附的 CCS 工程: e2e.ti.com/.../3276.boot_5F00_serial.zip

    您仍需要进行我在 BL_usbfuncs.c 中概述的更改

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的参与。  该项目不会导入 CCS 10.2。 (红色 x)它确实导入 CCS 9.2。 我对 usbfuncs.c 进行了更改、构建并刷写了它。 USB 设备仍然显示为未知、无效的配置描述符。 我还尝试在工程的调试文件夹中刷写 bin 文件、但遇到相同的错误。 两个 EKS 的结果相同。 (不同的 USB 电缆)。 我可能需要尝试另一台笔记本电脑。 很抱歉、我的回答不可能。

    尽管您之前提供的两个 bootserial bin 文件可以正常工作。

    已连接是故障 enumeration.e2e.ti.com/.../invalidConfiguration.txt 的 USB 树视图

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    您现在拥有哪个版本的 TivaWare? 2.2.0或2.1.4?

    我认为我以前发送的纸槽来自2.1.4、因为我以前仍然可以使用它。

    我发送的项目来自2.2.0。

    让我在这里附加我在 PC 上验证过的另一个 bin、它来自2.2.0: e2e.ti.com/.../1185.boot_5F00_serial.bin

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您发送给我的项目使用了 tivaware 2.2.0。 我的计算机上有这个。 但我不知道您发送的项目为什么会给我枚举错误。 预编译的 bin 文件通常没有问题、我需要一个 可以编译和枚举的工程。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    所以要清楚...

    boot_serial zip 文件不适合您、但4/14中的 boot_serial.bin 文件可以正常工作?

    如果是这样、您可能没有在 TivaWare 2.2.0.295中正确保存 BL_usbfuncs.c 文件。

    我将在 此处附上我的电子邮件:e2e.ti.com/.../bl_5F00_usbfuncs.c

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    拉尔夫

    我将 USB_funcs.c 复制到 boot_serial 工程。 我仍然无法识别 USB 设备。 我已将工作区中的项目导出到该 post.e2e.ti.com/.../boot_5F00_serialPN.zip

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    您的项目在 Windows 10 PC 上的 EK-TM4C1294XL 上进行了编译和工作正常。

    我在这里有一点损耗。 您的硬件连接不好、Windows PC 有问题、原因是无法清除、或者您的 EK-TM4C1294XL 已在某种程度上损坏。 我会说同时使用两个 USB 端口、然后尝试新 PC、看看您是否可以这样做...

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我将在另一台笔记本电脑上尝试此操作。 我注意了 USB DFU 中涉及的所有步骤、并在此处列出了这些步骤、可能的 EK 损坏似乎非常令人担忧。 我目前正在处理4个新订购的 EKs。 如果问题出在 EKs、TI 需要更换它们。 笔记本电脑上的 anitvirus 是否可能导致枚举问题?

    笔记本电脑2出现相同问题。 USB 设备无法识别、 故障、Windows 无法识别。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    四 克朗不会导致该问题。 也许有人可以、但有四人当然不能。

    您能否尝试在 Code Composer 中创建新的工作区并重新导入我发送的项目?

    我没有听说过防病毒停止枚举、但这不是我们可以广泛测试的东西。

    很遗憾、因为我无法重新创建这个项目、因为发送给我的项目工作正常、所以我对在这里可以发生的事情没有任何想法...

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我很慢地想到这个-如果有一种方法可以在 Tiva 中刷写 boot_serial.bin,那么 DFU_prog 将负责对应用程序 bin 文件进行编程,对吧? 我不需要 CCS 中的工程来生成 boot_serial。 如果是这种情况、我将关闭此 TT。

    感谢您对此问题的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    是的、您可以使用 LM 闪存编程器执行此操作。

    https://www.ti.com/tool/LMFLASHPROGRAMR

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ralph -我能够使用 DFU 进行输入和编程。 如果我对 blink.bin 进行编程、则 DFU 下载后该程序不起作用。 如果我从 CCS 闪存、则闪烁正常。 这是为什么?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    您是否在链接器文件中调整了闪烁的 CCS 工程的起始地址? 请参阅 TivaWare 用户指南 https://www.ti.com/lit/pdf/spmu373的第6.1节

    请注意、对于 TM4C129x、APP_START_ADDRESS 将为0x4000。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在 blinky_ccs.cmd 中#define APP_base 0x4000

    是的、我更改了此设置、但我看到闪烁仅在 CCS 中工作、而不是通过 DFU。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    嗯。 请附加项目? 我将进行测试!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    e2e.ti.com/.../blinkyPN.zip

    Blinky 项目。 仅在从 CCS 进行刷写时有效、而不是通过 DFU 进行刷写。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Priya、

    是否在 DFU 之后对电路板进行电源循环?

    它对我来说工作正常、但它确实需要重启电源。

    您还可以使用 LMFlash 通过 DFU 刷写.bin。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、编程后对电路板进行下电上电。 我使用 dfuprog 和 LMFlash 编程器上的 USB DFU 对此进行了尝试。 Blinky 不适合我、除非我使用 ICDI。 我选择了正确的 DFU 器件进行编程。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在 LM 闪存中、您只能获得一个选项:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、在本例中、我看到器件0。 1是 ICDI 的索引。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    有趣。 我知道我以前看过 ICDI 的出现,但现在却不是。 是否可以拔下 ICDI 线缆、从 OTG 跳线供电并尝试这样做? 我认为这不重要、但如前所述、这对我来说很有用...

    我还重新下载了您的项目、并使用了您发送给我的确切 bin、但没有重新编译以确保其正常工作。