请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS570LC4357 你(们)好 我想使用以下配置进行操作。 GCLK:300MHz、HCLK:150MHz、RWIT:3 Q1:如果使用高速缓存、闪存和 SRAM 访问速度是否可以视为300MHz? 问题2:如果不使用高速缓存、闪存和 SRAM 访问速度是否可视为150MHz? 此致。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.