请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TMS570LC4357 您好!
如何将2个 IS42S86400F (每个512MB)连接到 EMIF /CS0?
16位接口、8M x 16 x 4组 SDRAM
2个 ADR[12:0]和2个[DQ[15:0]
我是否应该使用 adr13反转/CS0以获得第二个/CS0?
BR、Rene
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
如何将2个 IS42S86400F (每个512MB)连接到 EMIF /CS0?
16位接口、8M x 16 x 4组 SDRAM
2个 ADR[12:0]和2个[DQ[15:0]
我是否应该使用 adr13反转/CS0以获得第二个/CS0?
BR、Rene