This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSPM0G3107-Q1:即使设置了 PWRDN、ENC 也会在转换后自动清除

Guru**** 2538930 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1413153/mspm0g3107-q1-enc-is-automaticaly-cleared-after-convertion-even-pwrdn-is-set

器件型号:MSPM0G3107-Q1

工具与软件:

I m 使用序列模式、然后设置 CTL0的 PWRDN 和 ENC 位。 但在所有已配置的通道转换后、ENC 清除、AVEN PWRDN 自动清除。 因此、下一个其他 TRIG 事件会被忽略。

规范说明:

16 PWRDN R/W 0h Power down policy
0h = ADC is powered down on completion of a conversion if there is no pending trigger
1h = ADC remains powered on as long as it is enabled through software.

请参阅以下所有寄存器设置 ENC 位: