This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSPM0L2228:数据表中缺少64引脚 LQFP 封装

Guru**** 2927270 points

Other Parts Discussed in Thread: MSPM0L2228

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1410610/mspm0l2228-64-pin-lqfp-package-is-missing-in-the-datasheet

器件型号:MSPM0L2228

工具与软件:

尊敬的专家:

在 MSPM0L2228数据表的第一页上、它声称有0.4mm 间距的封装可用、但在检查数据表时、我不知何故只能找到0.5mm 间距的版本。

请告诉我、我在哪里可以找到64引脚和80引脚 LQFP 封装的0.4mm 间距封装图?

谢谢!

Marinus