This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
大家好:
我无法在 Httpsget 示例中设置 http 调用的超时。
HT4.12.4.12.4(¶ms) Cli_Params_;
params.tls = TLS;
params.timeout = 1;// 1秒。
是否在 任何底层文件的库中设置了超时?
在哪里以及如何在代码中设置 params.timeout statcaly?
此致
线性调频脉冲
/* * Copyright (c) 2015-2016, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /* * ======== httpsget.c ======== * HTTPS Client GET example application */ #include <string.h> #include <time.h> /* XDCtools Header files */ #include <xdc/runtime/Error.h> #include <xdc/runtime/System.h> /* TI-RTOS Header files */ #include <ti/sysbios/BIOS.h> #include <ti/sysbios/hal/Seconds.h> #include <ti/sysbios/knl/Task.h> #include <ti/sysbios/knl/Semaphore.h> #include <ti/drivers/GPIO.h> #include <ti/net/http/httpcli.h> #include <ti/net/sntp/sntp.h> /* Example/Board Header file */ #include "Board.h" #include <sys/socket.h> #define HOSTNAME "www.example.com:443" #define REQUEST_URI "/" #define USER_AGENT "HTTPCli (ARM; TI-RTOS)" #define NTP_HOSTNAME "pool.ntp.org" #define NTP_PORT "123" #define NTP_SERVERS 3 #define NTP_SERVERS_SIZE (NTP_SERVERS * sizeof(struct sockaddr_in)) #define HTTPTASKSTACKSIZE 32768 /* * USER STEP: Copy the lines in the root CA certificate between * -----BEGIN CERTIFICATE----- * ... * -----END CERTIFICATE----- */ uint8_t ca[] = "<--- add root certificate with blackslash at end of each new line -->"; uint32_t calen = sizeof(ca); unsigned char ntpServers[NTP_SERVERS_SIZE]; static Semaphore_Handle semHandle = NULL; /* * ======== printError ======== */ void printError(char *errString, int code) { System_printf("Error! code = %d, desc = %s\n", code, errString); BIOS_exit(code); } /* * ======== timeUpdateHook ======== * Called after NTP time sync */ void timeUpdateHook(void *p) { Semaphore_post(semHandle); } /* * ======== startNTP ======== */ void startNTP(void) { int ret; int currPos; time_t ts; struct sockaddr_in ntpAddr; struct addrinfo hints; struct addrinfo *addrs; struct addrinfo *currAddr; Semaphore_Params semParams; memset(&hints, 0, sizeof(struct addrinfo)); hints.ai_family = AF_INET; hints.ai_socktype = SOCK_DGRAM; ret = getaddrinfo(NTP_HOSTNAME, NTP_PORT, NULL, &addrs); if (ret != 0) { printError("startNTP: NTP host cannot be resolved!", ret); } currPos = 0; for (currAddr = addrs; currAddr != NULL; currAddr = currAddr->ai_next) { if (currPos < NTP_SERVERS_SIZE) { ntpAddr = *(struct sockaddr_in *)(currAddr->ai_addr); memcpy(ntpServers + currPos, &ntpAddr, sizeof(struct sockaddr_in)); currPos += sizeof(struct sockaddr_in); } else { break; } } freeaddrinfo(addrs); ret = SNTP_start(Seconds_get, Seconds_set, timeUpdateHook, (struct sockaddr *)&ntpServers, NTP_SERVERS, 0); if (ret == 0) { printError("startNTP: SNTP cannot be started!", -1); } Semaphore_Params_init(&semParams); semParams.mode = Semaphore_Mode_BINARY; semHandle = Semaphore_create(0, &semParams, NULL); if (semHandle == NULL) { printError("startNTP: Cannot create semaphore!", -1); } SNTP_forceTimeSync(); Semaphore_pend(semHandle, BIOS_WAIT_FOREVER); ts = time(NULL); System_printf("Current time: %s\n", ctime(&ts)); } /* * ======== httpsTask ======== * Makes an HTTP GET request */ Void httpsTask(UArg arg0, UArg arg1) { bool moreFlag = false; char data[64]; int ret; int len; struct sockaddr_in addr; TLS_Params tlsParams; TLS_Handle tls; HTTPCli_Params params; HTTPCli_Struct cli; HTTPCli_Field fields[3] = { { HTTPStd_FIELD_NAME_HOST, HOSTNAME }, { HTTPStd_FIELD_NAME_USER_AGENT, USER_AGENT }, { NULL, NULL } }; startNTP(); System_printf("Sending a HTTPS GET request to '%s'\n", HOSTNAME); System_flush(); TLS_Params_init(&tlsParams); tlsParams.ca = ca; tlsParams.calen = calen; tls = TLS_create(TLS_METHOD_CLIENT_TLSV1_2, &tlsParams, NULL); if (!tls) { printError("httpsTask: TLS create failed", -1); } HTTPCli_construct(&cli); HTTPCli_setRequestFields(&cli, fields); ret = HTTPCli_initSockAddr((struct sockaddr *)&addr, HOSTNAME, 0); if (ret < 0) { printError("httpsTask: address resolution failed", ret); } HTTPCli_Params_init(¶ms); params.tls = tls; params.timeout = 1; ret = HTTPCli_connect(&cli, (struct sockaddr *)&addr, 0, ¶ms); if (ret < 0) { printError("httpsTask: connect failed", ret); } ret = HTTPCli_sendRequest(&cli, HTTPStd_GET, REQUEST_URI, false); if (ret < 0) { printError("httpsTask: send failed", ret); } ret = HTTPCli_getResponseStatus(&cli); if (ret != HTTPStd_OK) { printError("httpsTask: cannot get status", ret); } System_printf("HTTP Response Status Code: %d\n", ret); ret = HTTPCli_getResponseField(&cli, data, sizeof(data), &moreFlag); if (ret != HTTPCli_FIELD_ID_END) { printError("httpsTask: response field processing failed", ret); } len = 0; do { ret = HTTPCli_readResponseBody(&cli, data, sizeof(data), &moreFlag); if (ret < 0) { printError("httpsTask: response body processing failed", ret); } len += ret; } while (moreFlag); System_printf("Recieved %d bytes of payload\n", len); System_flush(); HTTPCli_disconnect(&cli); HTTPCli_destruct(&cli); TLS_delete(&tls); } /* * ======== netIPAddrHook ======== * This function is called when IP Addr is added/deleted */ void netIPAddrHook(unsigned int IPAddr, unsigned int IfIdx, unsigned int fAdd) { static Task_Handle taskHandle; Task_Params taskParams; Error_Block eb; /* Create a HTTP task when the IP address is added */ if (fAdd && !taskHandle) { Error_init(&eb); Task_Params_init(&taskParams); taskParams.stackSize = HTTPTASKSTACKSIZE; taskParams.priority = 1; taskHandle = Task_create((Task_FuncPtr)httpsTask, &taskParams, &eb); if (taskHandle == NULL) { printError("netIPAddrHook: Failed to create HTTP Task\n", -1); } } } /* * ======== main ======== */ int main(void) { /* Call board init functions */ Board_initGeneral(); Board_initGPIO(); Board_initEMAC(); /* Turn on user LED */ GPIO_write(Board_LED0, Board_LED_ON); System_printf("Starting the HTTPS GET example\nSystem provider is set to " "SysMin. Halt the target to view any SysMin contents in ROV.\n"); /* SysMin will only print to the console when you call flush or exit */ System_flush(); /* Start BIOS */ BIOS_start(); return (0); }
您好!
您如何知道它无法正常工作?
您是否可以尝试其他值、如2s、3s 或5s?
您是否尝试过没有 TLS 的 HTTPGET? 超时是否有效? 我想说的是、问题与 TLS 有关、而不是与 TLS 有关。
尊敬的 Charles:
我在 HttpGet 示例中尝试了未使用 TLS 的 HTTPGET、但它在这里甚至不起作用。
此致
线性调频脉冲
您好!
能否详细阐述不起作用的问题? 如果将超时值保留为默认值0、会发生什么情况? 当您更改为1、2、3...时会发生什么情况? 它是否完全不超时或没有根据您指定的时间超时?
请查看这篇文章、看看定义 HTTPCli_LIBTYPE_MIN 是否会有所不同。 请参阅 Aashish Bhanawah 的答案。
尊敬的 Charles:
"如果将超时值保留为默认值等于0、会发生什么情况。 当您更改为1、2、3...时会发生什么情况? 它是否完全不超时或没有根据您指定的时间超时?"
最初我没有定义 HTTPCli_LIBTYPE_MIN 我的应用程序工作正常,没有定义这个宏,有几个 http 调用需要超过一分钟的时间来获得响应,所以我想增加超时到90秒。 我在 TI RTOS SDK 的 httpcli.h 文件中阅读了该 params.timeout。 我使用了 params.timeout = 1;由于我的应用平均需要2.5秒从我们的服务器获得响应、所以为了测试这个超时、我将超时定义为1秒。 它应该给我超时错误与错误代码-104或类似的错误代码。 只是通过使用这个超时而不定义宏 HTTPCli_LIBTYPE_MIN 没有 在意义上工作,即使在内部定义10秒,它没有做任何区别,它使用从内核内部获取默认超时值,我认为,所以它没有为我的应用训练。 我阅读了 Aashish Bhanawah 的答案,并尝试定义 HTTPCli_LIBTYPE_MIN 宏 ,并在 HttpGet 和 httpsget 示例中使用 params.timeout = 1指向 www.google.com 和我自己的服务器通常需要1.5秒才能得到响应。 我收到-109错误、指出无法获取状态。 当我使用 params.timeout = 0时、它得到200 resp 代码的响应。 这意味着超时设置为默认值。 如何在我的应用中使用该超时东西? 如果它适用于 HttpGet 和 https://focus.ti.com.cn 示例、那么它肯定适用于我的应用程序。 请向我建议一些解决方法。
此致
Chiranth
尊敬的 Charles:
MCU:Tm4C129ENCPDT
TIRTOS:2.16.01.14
XDC 工具:xdctools_3_32_00_06_core
这是我在 TI RTOS 的 httpcli.h 文件中的代码片段。
typedef struct HTTPCli_Params { TLS_Handle *tls; #ifndef HTTPCli_LIBTYPE_MIN HTTPCli_StatusHandler *shandle; HTTPCli_ContentHandler *chandle; HTTPCli_RedirectCallback rhandle; #ifndef __linux__ unsigned int stackSize; /*!< Async thread stack size. 0 for default */ unsigned int priority; /*!< Async thread priority. 0 for default */ #endif #endif #ifdef NET_SLP HTTPCli_Notify rnotify; /*!< Async read notify handle (6LoWPAN) */ HTTPCli_Notify wnotify; /*!< Async write notify handle (6LoWPAN) */ HTTPCli_Notify enotify; /*!< Async exception notify handle (6LowPAN)*/ #endif #ifndef NET_SLP int timeout; /*!< Timeout value (in seconds) for socket. Set 0 for default value */ #endif } HTTPCli_Params;
我在那里看到了 tls_handle *tls;这 httpcli.h 文件是不是它存在的情况下 ,其他人 Aashish Bhanawat 回答。 剂量此 TLS 事件导致错误-109?
此致
线性调频脉冲
我看到那里有 tls_handle *tls;这个 httpcli.h 文件是不是它在其他人的情况下它是不存在的,其中 Aashish Bhanawat 回答。 剂量此 TLS 事件导致错误-109 ?[/报价]请参阅 TI-RTOS 安装中的文件:///C/C:/ti/tirtos_tivac_2_16_00_08/products/ns_1_11_00_10/docs/html/httpcli_8h_source.html。 它对各种错误代码进行了说明。 我想知道 超时是否只对 TLS HTTPSGET 有效。 对于非 TLS HTTPGET、可能在没有传递 TLS 句柄的情况下无法工作。 在 Aashish Bhanawat 回答的案例中、更具体地说是针对 Wi-Fi 设备的不同设备。 我不是 HTTPCli 的专家,不确定我是否能进一步帮助。
尊敬的 Charles:
我尝试使用 http 和 https 没有使用宏 HTTPCli_LIBTYPE_min , tiemout 是 wokring with plain http 和不使用 https ,我通过改变超时值从1,2,3等测试. 对此有何建议?
此致
线性调频脉冲
Chiranth、您好!
使用纯 http 生成的 tiemout 无法使用 https、//quote]在前面的响应中、您提到 HTTP 也不能在超时的情况下工作。 现在、您说它适用于 HTTP、但不适用于 HTTPS。 对不起,我真的不知道为什么它适用于 HTTP 而不是 HTTPS。