This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
您好!
我们是否有关于 AM2634 WARMRST#引脚(C3)驱动容量的信息
数据表中提供的其他引脚(如 RGMII、GPIO、MMC 等)几乎没有变化:
例如、RGMII 引脚的最小值和最大值为3 pF /25 pF
3个 pF / 10个 pF 用于 GPIO
2个 pF / 24个 pF 用于 SPI
5 pF / 20 pF 用于 MCAN 等
您好!
我将就此问题与我们的专家进行联系。 我希望在接下来的几天里有一个答复。
谢谢!
Susan