工具/软件:
MCLK= 12.288MHz、fs = 48kHz、IOVDD = 3.3V、LDO_IN = 3.3V、AVdd = GND、 DVDD=GND、CM=0.75V
我成功通过 i2c 配置编解码器、但无法使编解码器回放 I2S。 我甚至无法在输出/输入引脚上测量配置的0.75V CM、因此我想编解码器未处于正确的配置中。
这是我当前的配置:
void codec_init(){
/* ---------- switch to page 0 ---------- */
codec_write_reg(0x00, 0x00);
// software reset
codec_write_reg(0x01, 0x01);
/*---- Clock and Interface Settings ----*/
// for Fs = 48KHz nad MCLK = 12.228MHz
// Fs = MCLK/(NDAC * MDAC * OSR)
// 48kHz = 12.288MHz/(1 * 2 * 128)
// NDAC divider = 1
codec_write_reg(0x0b, 0x81);
// MDAC divider = 2
codec_write_reg(0x0c, 0x82);
// Power up NADC divider with value 1
codec_write_reg(0x12, 0x81);
// Power up MADC divider with value 2
codec_write_reg(0x13, 0x82);
// OSR of DAC = 128
codec_write_reg(0x0d, 0x00);
codec_write_reg(0x0e, 0x80);
// OSR of ADC = 128
codec_write_reg(0x14, 0x80);
// set i2s mode
// set word length/frame size to 32bit to send 24bit audio data
// b00110000
codec_write_reg(0x1b, 0x00);
// set the DAC Mode to PRB_P8
// codec_write_reg(0x3c, 0x08);
// Select DAC PRB_P1
codec_write_reg(0x3c, 0x01);
// Select ADC PRB_R1
codec_write_reg(0x3D, 0x01);
// Select ADC PTM_R4
codec_write_reg(0x3D, 0x00);
// Set MicPGA startup delay to 3.1ms
codec_write_reg(0x47, 0x32);
/*---- Configure Power Supplies ----*/
/* ---------- switch to page 1 ---------- */
codec_write_reg(0x00, 0x01);
// Disable weak AVDD-DVDD link
codec_write_reg(0x01, 0x08);
// Power AVDD LDO
codec_write_reg(0x02, 0x01);
// set REF charging time to 40ms
codec_write_reg(0x7b, 0x01);
// HP soft stepping settings for optimal pop performance at power up
// Rpop used is 6k with N = 6 and soft step = 20usec. This should work with 47uF coupling
// capacitor. Can try N=5,6 or 7 time constants as well. Trade-off delay vs “pop” sound
codec_write_reg(0x14, 0x25);
// D7 = 0 reserved
// D6 = 1 common mode to 0.75V
// D4-5 = 00 Output Common Mode for HPL and HPR is same as full-chip common mode
// D3 = 0 Output Common Mode for LOL and LOR is same as full-chip common mode
// D2 = 0 reserved
// D1 = 1 Power HP by LDOIN
// D0 = 1 LDOIN pin range 1.8V - 3.6V
//
// 01000011 = 0x43
codec_write_reg(0x0a, 0x43);
/* ---- Routing ----*/
// route dac to line outs
// left channel
codec_write_reg(0x0e, 0x08);
// right channel
codec_write_reg(0x0f, 0x08);
// Route LINE_IN Left to LEFT_P with 20K input impedance
codec_write_reg(0x34, 0x80);
// Route LINE_IN Right to RIGHT_P with 20K input impedance
codec_write_reg(0x37, 0x80); // Use appropriate register for LINE_IN routing
// unmute line outs
// LOL: unmute, 0 dB gain
codec_write_reg(0x12, 0x00);
// LOR: unmute, 0 dB gain
codec_write_reg(0x13, 0x00);
// Power up LOL and LOR drivers
codec_write_reg(0x09, 0x3C);
/* ---------- switch to page 0 ---------- */
codec_write_reg(0x00, 0x00);
// DACL DACR -> 0dB
codec_write_reg(0x41, 0x00);
codec_write_reg(0x42, 0x00);
// Power up the Left and Right DAC Channels with route the Left Audio digital data to
// Left Channel DAC and Right Audio digital data to Right Channel DAC
// 11010101
codec_write_reg(0x3f, 0xd5);
// unmute dac digital volume control
codec_write_reg(0x40, 0x00);
// Power up Left and Right ADC Channels
// Do not use digital mic
codec_write_reg(0x51, 0xF0);
// Unmute Left and Right ADC Digital Volume Control
codec_write_reg(0x52, 0x00);
}
也许关于输入级的另一个有趣的信息是:
输入似乎处于悬空状态。 我的耦合电容器没有通过交流信号。 此外、我的运算放大器电路的作用类似于具有浮动输出(正弦信号失真到方波)。
也许我的 MCLK 的信号完整性不是很完美、我会有一点过冲/下冲、但这应该起作用?
如果 MCLK 没有正确地为系统提供时钟、编解码器是否不会应用电源和路由配置?
感谢您的参与:>