请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPA3255 您好,先生,
我设计了一个带TPA3255的放大器电路。
当 输入信号频率为1K时,系统在工作15秒后将出现故障(OTE)。 但是,当输入信号为10K时,系统可以工作20分钟。
电源:48V;
输入正弦Vpp:3.4V;
输出正弦Vpp:44V。
谢谢!
好
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.