Other Parts Discussed in Thread: TPA3136D2
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPA3136D2 大家好,
客户希望使用TPA3136。 他们希望为F0=600Hz扬声器设计高通滤波器。
如果由于DSP无法设置数字均衡器,他们想要在620Hz设置-3dB,您能否告诉我们如何设计无源RC值?
EVM输入仅放置一个交流脱耦合盖。
谢谢!
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.