This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我开始用TPA3106设计吉他放大器,我对此有一些疑问。
首先,TPA3106可以使用哪些输入信号电平...在"绝对最大额定值"中,它表示Inn和INP可以在[-0.3V至VREG + 0.5V]范围内。 这意味着我必须将我的吉他信号添加到一个小到0.3Vpp的输入缓冲区,这样它不会超过下限?
另一个问题是关于在TINA参考设计中的VREG..., 它连接到4V电源...但在数据表中,我了解到4V由TPA3106自身调节...在EVM原理图中,它直接与交流耦合接地...为什么在TINA参考设计中存在直流电源? 在仿真中,如果我从参考设计中移除该源,输出波会明显受到一些噪声的影响,并且输出电平会大量衰减:
但是,在EVM原理图中,VREG的4V电源缺失。
我该怎么办?
提前感谢您的帮助!