Other Parts Discussed in Thread: PCM9211
https://e2e.ti.com/support/audio-group/audio/f/audio-forum/628147/pcm9211-programming
部件号:PCM9211大家好,
在数据表中,PCM的FS输出为7至192KHz,此FS是否可以编程为16KHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Diego,
此外,PCM9211是否具有S/PDIF信号的音量控制?
此外, 在阅读数据表时,我们看不到TI能够在内部对16kHz进行重新采样。 当仅仅使用ADC作为信号输入时,我们相信PCM输出可以在16kHz上运行。
但使用SPDIF输入时,DIR的时钟和整个内部音频通道的其余部分似乎直接从SPDIF信号时钟导出,最高可达216KHz。 如果PCM9211可以进行重新采样并将采样率降低到16kHz,则主输出端口也可以根据我们的要求提供16kHz。 在查看数据表中的结构图时,我们只是看不到任何可以执行此操作的重新采样单元。
您能否检查主输出端口PCM时钟频率是否可以固定为16kHz (在主或从模式下),通过执行重新采样,SPDIF输入信号提供的时钟频率是多少?
谢谢。
巴西
Matthew Lam