请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TAS5558 主题中讨论的其他部件: TAS5624A
您好,
我有一个使用TAS5558和TAS5624A放大器(2N) BTL和AD调制的设计应用。 关于将差分PWM驱动到具有光电隔离的8英寸背板中,TI是否建议使用紧密耦合或松散耦合差分对以及什么端接(如果有)?
此致,我
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.