请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TLV320AIC33 是否提供了将TIBQ生成的系数与TLV320AIC33编解码器配合使用的说明?
特别是,TIBQ生成N0,N1,D1或N0,N1,N2,D1,D2系数。
我的滤波器(20Hz高通,10kHz低通)生成了两组N0,N1,D1。 我将这些设置编程为并设置N2,D2 = 0。 结果不好。
谢谢!
Randy。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是否提供了将TIBQ生成的系数与TLV320AIC33编解码器配合使用的说明?
特别是,TIBQ生成N0,N1,D1或N0,N1,N2,D1,D2系数。
我的滤波器(20Hz高通,10kHz低通)生成了两组N0,N1,D1。 我将这些设置编程为并设置N2,D2 = 0。 结果不好。
谢谢!
Randy。