Other Parts Discussed in Thread: PCM3070
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:PCM3070 您好,是否可以更改USB音频设备采样率/位深度? TAS1020位于PC和PCM3070之间;我想以不同的采样速率/位深度运行一些音频分析,但目前在44.1kHz时WCLK的最终值似乎是固定的。
在Windows设备管理器中,设置为锁定/灰色:
此致,Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Jason,
TAS1020B的固件规定了评估模块的采样率。 可以按照此Wiki条目中的步骤更改此固件,只需在步骤13中选择具有您选择的采样率的固件映像文件。
此致,
-Diego Mel é ndez López ñ a
音频应用工程师