请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPA3255 您好,
我的直流电源具有56 VDC单轨输出.. 和8欧姆低音炮负载...
TPA3255功率级电源(最大值)(V)为53.5 V。 我不想让放大器脱模...
请给我建议/原理图,如何使此PSU电压(56 VDC)下降到52/51/50 VDC..与此TPA3255 A配合使用..
提前感谢您!
埃米尔
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.