请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:PCM5102A 您好,
我在数据表(33页,11.5 .1)中发现,在1.8V模式下使用PCM5102A时,DVDD和LDOO都应连接到外部1.8V。 我不清楚的是,如果我仍然需要为DVDD和LDOO引脚安装单独的0.1 和10uF保护罩,如数据表中提供的示意图所示。 下面是我的原理图中的外观: 
这是否正确?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.