请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:PCM5100 您好,
PCM5100 DAC输出的建议LPF为470E和2.2nF,提供约154KHz的切断频率。
为了最大限度地减少BOM中的独特零件,我想使用切口约为153KHz的316E和3.3nF。
我想知道修改是否可以,或者是否会对性能产生不利影响。
谢谢!!
谨致问候,
拉温德拉
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.