请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPA6138A2 您好 TI,团队
我有一个使用 TPA6138A2 的耳机项目,将耳机连接到噪声发生器、并使用粉色噪声长达96小时、芯片损坏。
设置以下条件
频率范围:20Hz~20kHz
蜂鸣和拉特尔:0.8V±10%
时间:96小时

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.