Other Parts Discussed in Thread: TPA6133A2
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPA6133A2 您好!
TPA6133A2数据表标题中138mW 的条件是什么?
从图3中可以看出、测量条件为 VDD=3.3V、1kHz、THD+N=10%、RL=16 Ω。 对吗?
此致、
Akio Ito
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.