e2e.ti.com/.../SCH_2D00_WSS_5F00_BM20L_2D00_V02.pdfTPA2080D放大器问题如下:
1、当音量达到最大值时、失真相对较大
2.当音量达到最大值时,IC 的工作温度很高
3.当音量达到最大值时,放大器的输出不稳定
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
e2e.ti.com/.../SCH_2D00_WSS_5F00_BM20L_2D00_V02.pdfTPA2080D放大器问题如下:
1、当音量达到最大值时、失真相对较大
2.当音量达到最大值时,IC 的工作温度很高
3.当音量达到最大值时,放大器的输出不稳定
目前、我们已使用1.5uH、2.2uH、3.3uH 和4.7uH 的较大电流更改了电感、包括6A 电流的电感测试、但失真没有任何改善。
以下2.2uH 电感测试说明
1.蓝牙模块的输出频率响应和失真曲线正常。
2.验证放大器的输出频率响应和失真曲线、如下所示:
扬声器:4R
2.测试的电源电压 VBAT:4V
3.测试功率放大器的电源 VCC (VBAT)为4V,PVDD 为5.4V。
4.示波器用于验证电压是否稳定且没有杂波。 它由稳压电源供电。
5. AP-10dB 输入、功率放大器2W 输出、频率响应曲线无问题
6.在正常电源电压条件下,失真曲线应大于1%,最大值应大于5%。
7.不符合 TPA2080D1的规格(VCC 3.6V、输出失真小于1%)。
8.基极噪声太高。 请帮助列出优化建议。