请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TAS5805M 主题中讨论的其他器件:TAS5805
您好、Sirs、
如标题所示、您是否会根据19V PVCC、4 Ω 负载的测试条件建议 TAS5805的效率图?
TAS5805数据表仅指定高达12V 的效率数据。
谢谢、此致、
陈耀恩
2019年10月3日
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.