请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TAS5707 TSA5707在18V 电源、驱动6 Ω 负载的情况下、DRC 可以稳定地输出8W?
非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TSA5707在18V 电源、驱动6 Ω 负载的情况下、DRC 可以稳定地输出8W?
非常感谢。