请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPA3110D2 主题中讨论的其他器件: TPA3140D2
TPA3110D2数据表 P19描述为"该"虚拟"电源轨是 PLIMIT 引脚电压的4倍"。
请告诉我虚拟轨(PLIMIT×4)是否有所不同。
当 PLIMIT 输入为无变化电压(2V±0V)时、Vp 是否仅设置为8V?
我想知道虚拟电源轨的精度:"4倍"
此致、
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.