请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:PCM1822 ADC 低端模拟输入的绝对最大额定值为-0.3V。 建议模拟输入范围为0至 AVDD (+3.3V)。 使用2Vpp 输入时、交流耦合是否会导致输入信号摆动至-1V、从而违反规范?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADC 低端模拟输入的绝对最大额定值为-0.3V。 建议模拟输入范围为0至 AVDD (+3.3V)。 使用2Vpp 输入时、交流耦合是否会导致输入信号摆动至-1V、从而违反规范?