请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TAS6424R-Q1 您好
在数据表推荐的原理图中、自举电容器的值为1uF、但在10.2.1.2.3章节描述的说明中、当频率低于30Hz 时、自举电容器的值变为2.2uF。
现在我们需要输出音频频率20Hz~20kHz、这是否意味着我们需要正确选择值为2.2uF 的自举电容器?
如何计算自举电容值?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
在数据表推荐的原理图中、自举电容器的值为1uF、但在10.2.1.2.3章节描述的说明中、当频率低于30Hz 时、自举电容器的值变为2.2uF。
现在我们需要输出音频频率20Hz~20kHz、这是否意味着我们需要正确选择值为2.2uF 的自举电容器?
如何计算自举电容值?