This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CCS/LAUNCXL-CC2640R2:CC2640R2 SDK 1.0 安装CC2640R2 SDK 1.30 后出现程序构建错误的示例

Guru**** 2562120 points
Other Parts Discussed in Thread: SYSBIOS

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/584062/ccs-launchxl-cc2640r2-cc2640r2-sdk-1-0-0-example-program-build-errors-after-installing-cc2640r2-sdk-1-30

部件号:LAUNCHLL-CC2640R2
“Thread:SysBIOS”中讨论的其它部件

工具/软件:Code Composer Studio

您好,

  最近我安装了CC2640R2 SDK 1.3 .0。 我最近还安装了新的CCS XDC工具版本。 我在CCS工作区为CC2640R2 SDK 1.0 0构建程序,我在下面看到了这些错误。 以下错误来自CC2640R2 SDK 1.0 0简单外设示例程序。 如何在CCSV7中解决这些错误?

说明资源路径位置类型
#141函数调用app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 7281 C/C++问题
#148声明与“XDC_CPTR ti_SysBIOS_KNL_Intrinsics_SupportProxy__Delegate__S (void)”(在“C:/ti/simplelink_cc2640r2_SDK_1_30_00_25/kernel/tirtos/packages/ti/77BIOS/KNL/package/package_ccupbl_cron_cron_cron_p_crus_p_p_p_crp_p_p_crf_p_x_x_p_x_p_x_p_p_p_x_p_p_x_p_p_x_p_x_p_p_x_p_p_p_x_p
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 2700 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 2833 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 2976 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3094 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3265 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3478 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3555 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3667 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3800 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3906 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4048 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4229 C/C++问题
#18应为a“)”app_bl_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4379 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4496 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4581 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4690 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4795 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4895 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 5119 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 5377 C/C++问题
#18应为a ")" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 5619 C/C++问题
#20标识符"CT__ti_SysBIOS_BIOS_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 2700 C/C++问题
#20标识符"CT__ti_SysBIOS_family_arm_cc26xx_Boot_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 2833 C/C++问题
#20标识符"CT__ti_SysBIOS_family_arm_cc26xx_Timer_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 2976 C/C++问题
#20标识符"CT__ti_SysBIOS_family_arm_cc26xx_TimestampProvider_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3094 C/C++问题
#20标识符"CT__ti_SysBIOS_family_arm_m3_Hwi_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg行3265 C/C++问题
#20标识符"CT__ti_SysBIOS_family_arm_m3_IntrinsicsSupport_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3478 C/C++问题
#20标识符"CT__ti_SysBIOS_family_arm_m3_TaskSupport_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3555 C/C++问题
#20 identifier "CT__ti_SysBIOS_gates_GateHWI_Module__startupDoneFxn" is undefined app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 3667 C/C++ problem
#20标识符"CT__ti_SysBIOS_Gates_GateMutex_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/Pkg/package/cfg line 3800 C/C++问题
#20 identifier "CT__ti_SysBIOS_hal_HWI_Module__startupDoneFxn" is undefined app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/package/package/cfg line 3906 C/C++ problem
#20标识符"CT__ti_SysBIOS_stamps_HeapMem_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4048 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Clock_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4229 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Event_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4379 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Idle_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4496 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Intrinsics_Module__startupDoneFxn"未定义app_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/package/package/cfg line 4581 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Mailbox_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4690 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Queue_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4795 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_semaphore_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 4895 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Swi_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/package/package/cfg line 5119 C/C++问题
#20标识符"CT__ti_SysBIOS_KNL_Task_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 5377 C/C++问题
#20标识符"CT__ti_SysBIOS_ROM_cortexm_cc26xx_R2_CC26xx_Module__startupDoneFxn"未定义app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/Pkg/package/cfg line 5619 C/C++问题
gmake:***[build_1287780815]错误2 simile_peripheral_cc2640r2lp_app C/C++问题
gmake:目标'all'由于错误而没有重制。simile_peripheral_cc2640r2lp_app C/C++问题
gmake [1]:***[builp-1287780815-InProc]错误1 simile_peripheral_cc2640r2lp_app C/C++问题
xdctools_3_32_01_22_core\gmake.exe:***[package/cfg/app_pem3.oem3]错误1 simple_peripheral_cc2640r2lp_app C/C++问题
#145-D " XDC_PTR (*)(XDC_CPTR,const XDC_UChar *,XDC_SizeT,XDC_Runtime_Error_Block *)"类型的值不能用于初始化"XDC_PTR (*)(XDC_PTR,XDC_SizeT,XDC_Error_Block *)类型的实体 xdc_runtime错误块*)" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 982 C/C++问题
#145-D " XDC_PTR (*)(XDC_CPTR,const XDC_UChar *,XDC_SizeT,XDC_Runtime_Error_Block *)"类型的值不能用于初始化"XDC_PTR (*)(XDC_PTR,XDC_SizeT,XDC_Error_Block *)类型的实体 xdc_runtime错误块*)" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 1003 C/C++问题
#145-D " XDC_PTR (*)(XDC_CPTR,const XDC_UChar *,XDC_SizeT,XDC_Runtime_Error_Block *)"类型的值不能用于初始化"XDC_PTR (*)(XDC_PTR,XDC_SizeT,XDC_Error_Block *)类型的实体 xdc_runtime错误块*)" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 1025 C/C++问题
类型"const XDC_UChar *"的#169-D参数与类型"XDC_runtime _Error_Block *" app_ble_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg行7281 C/C++问题不兼容
类型为"XDC_PTR"的#169-D参数与类型为"XDC_SizeT"的参数不兼容app_bl_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 7281 C/C++问题
"XDC_SizeT"类型的#169-D参数与"const XDC_UChar *" app_bl_pem3.c /simple_peripheral_cc2640r2lp_app/FlashROM/configPkg/package/cfg line 7281 C/C++问题的参数不兼容
产品'SimpleLink CC2640R2 SDK' 1.0 v.0.22 当前未安装。 在构建过程中将使用兼容版本的1.30 .0.25。simile_peripheral_cc2640r2lp_app simile_peripheral_cc2640r2lp_app问题

- kel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好,kel:

    最后一行显示:“Product 'SimpleLink CC2640R2 SDK' 1.0 v.0.22 is not currently installed.”(当前未安装产品'SimpleLink CC2640R2 SDK' v.)。

    您能否看到它是否仍安装在C:\ti\simplelink_cc2640r2_sdk_1_00_00_22上? 如果没有,请重新安装SDK 1.0 v.0.22。

    祝你一切顺利
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    [QUOTE USER="JXs">您能否查看它是否仍安装在C:\ti\simplelink_cc2640r2_SDK_1_00_00_22上? 如果没有,请重新安装SDK 1.0 v.0.22。
    [/引述]

    它已安装。 我没有删除该文件夹。 这里是下面的。 CCS上的内容被覆盖。  

    CCS安装的产品

    - kel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    好的,谢谢确认。

    您是否可以更改:
    <property name="products" value="com.ti.SIMPLELINK_CC2640R2_SDK"/>

    <property name="products" value="com.ti.SIMPLELINK_CC2640R2_SDK:SIMP.SIMP"/> 1.00 00.22

    在应用程序和堆栈项目的.projectspec文件中?

    此外,添加到新工作空间的项目或仅是基于SDK 1.0 v的现有工作空间是否会发生这种情况?

    祝你一切顺利
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    JXS,您好!

    没用。 它发生在具有SDK 1.0 v的工作空间中。 但我已经将我的重要工作转移到SDK 1.30 工作区。

    我还想让您知道,在安装SDK 1.30 示例程序后,我的SDK 1.30 工作区发生了故障。 为了使SDK 1.30 工作区正常工作,我删除了SDK 1.30 和SDK 1.30 示例程序,然后重新安装了SDK 1.30。 我创建了一个新的CCS工作区并导入了SDK 1.30 简单外设。 它构建无错误。

    - kel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好,Kel,

    您是否可以导出您的工作区以便我们可以对其进行检查?

    祝你一切顺利
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    JXS,您好!

      很抱歉回复太晚。 我删除了我的CCS SDK 1.0 工作区和deletede 1.0 SDK安装目录。 I重新安装SDK 1.0。 我的新CCS SDK工作区1.0 的错误与此相同。  请参阅附加的CCS工作区。

    kele2e.ti.com/.../CC2640v100_5F00_Launchpad.rar