This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2564MODA:声明最大电容和电感、包括容差和电压增强电路。

Guru**** 2587345 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/950558/cc2564moda-declaration-of-maximum-capacitance-and-inductance-including-tolerances-and-voltage-enhancement-circuits

器件型号:CC2564MODA

为了支持 IEC 60079-11、需要披露该器件的最大电容和电感、包括容差和任何电压增强电路。  我可以联系谁或哪个小组进一步讨论如何获得此类声明?  如果需要、可提供经认证的身体接触以进行披露。  谢谢!