请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:CC2560 主题中讨论的其他器件:CC2564、
支持路径:/Product/Development 和故障排除/
我需要知道如何在此双模蓝牙芯片中在 BLE 和 BT 模式之间切换。 我在数据表中找不到此信息...
我是否需要重置/重新启动才能在模式之间切换?
请提供答案或指南参考。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Alexander、
感谢您的回复。 但是、在演示应用中、我可以看到 CC2564同时支持 BLE 和 BT SPP。 但我需要了解 BLE 和 BT A2DP 配置文件(辅助 A2DP)。 能否告诉我(在 CC2564中)是否同时支持 BLE 和 A2DP? 如果没有、那么我如何在这两种模式之间切换? 能否在运行时在 A2DP 和 BT 之间切换? 或者、我是否必须重置/重新启动模块?
谢谢!!