This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2340R5:是否支持 J-Link Ultra+?

Guru**** 2595770 points
Other Parts Discussed in Thread: CC2340R5, UNIFLASH, SEGGER

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1232189/cc2340r5-j-link-ultra-support

器件型号:CC2340R5
主题中讨论的其他器件: UNIFLASHSEGGER

大家好、

客户正在评估 CC2340R5、但在编程时遇到问题。

客户正在使用最近具有更新的 J-Link Ultra+、以允许 CC2340R5编程。

很遗憾、 客户无法通过 J-Flash V7.88d、CCS 12.3.0或 UniFlash 8.3.0.4307进行连接。

您能否确认应支持该功能?

Br、
斯特凡

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您发送编修。  
    我成功连接了几次,但它总是无法做更多的事情,下面的日志:  

    Application log started
    - J-Flash V7.88d (J-Flash compiled May 24 2023 15:24:22)
    - JLinkARM.dll V7.88d (DLL compiled May 24 2023 15:23:44)
    Reading flash device list [C:\Program Files\SEGGER\JLink\ETC/JFlash/Flash.csv] ...
    - List of flash devices read successfully (451 Devices)
    Reading MCU device list ...
    - List of MCU devices read successfully (10362 Devices)
    Creating new project ...
    - New project created successfully
    Connecting ...
    - Connecting via USB to probe/ programmer device 0
    - Probe/ Programmer firmware: J-Link Ultra V5-1 compiled May 23 2023 14:45:15
    - Probe/ Programmer S/N: #########
    - Device "CC2340R5" selected.
    - Target interface speed: 100 kHz (Fixed)
    - VTarget = 3.288V
    - ConfigTargetSettings() start
    - Flash breakpoints are disabled.
    - ConfigTargetSettings() end - Took 13us
    - InitTarget() start
    - CFG-AP DEVICEID: 0x1BB8402F
    - PG2.0 device detected
    - CFG-AP DEVICESTATUS: 0x030DBA05
    - Checking if AHB-AP is enabled...
    - AHB-AP enabled --> Attaching to the target...
    - InitTarget() end - Took 15.6ms
    - Found SW-DP with ID 0x6BA02477
    - DPIDR: 0x6BA02477
    - CoreSight SoC-400 or earlier
    - AP map detection skipped. Manually configured AP map found.
    - AP[0]: AHB-AP (IDR: Not set)
    - AP[0]: Core found
    - AP[0]: AHB-AP ROM base: 0xE00FF000
    - CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
    - Found Cortex-M0 r0p1, Little endian.
    - FPUnit: 4 code (BP) slots and 0 literal slots
    - CoreSight components:
    - ROMTbl[0] @ E00FF000
    - [0][0]: E000E000 CID B105E00D PID 000BB008 SCS
    - [0][2]: E0002000 CID B105E00D PID 000BB00B FPB
    - Executing init sequence ...
    - Executing Reset (0, 0 ms)
    - ResetTarget() start
    - Executing reset via SEC-AP in order to enter SACI mode...
    - O.K.
    - Executing exit SACI mode sequence...
    - O.K.
    - Checking if AHB-AP is enabled...
    - O.K.
    - Checking if debug probe loop entered...
    - O.K.
    - Invalid application entry addr detected: 0xFFFFFFFF
    - ResetTarget() end - Took 195ms
    - Initialized successfully
    - Target interface speed: 100 kHz (Fixed)
    - Found 1 JTAG device. Core ID: 0x6BA02477 (None)
    - Connected successfully
    Reading entire flash chip ...
    - 257 sectors, 2 ranges, 0x0 - 0x7FFFF, 0x4E020000 - 0x4E0207FF
    - Start of preparing flash programming
    - End of preparing flash programming
    - WARNING: Blank check not supported for this flash bank, skipped
    - ERROR: Failed to read memory (0x20000 bytes @ address 0x00000000)
    - Start of restoring
    - End of restoring
    - ERROR: Failed to read back target memory
    Disconnecting ...
    - Disconnected
    Connecting ...
    - Connecting via USB to probe/ programmer device 0
    - Probe/ Programmer firmware: J-Link Ultra V5-1 compiled May 23 2023 14:45:15
    - Probe/ Programmer S/N: #########
    - Device "CC2340R5" selected.
    - Target interface speed: 100 kHz (Fixed)
    - VTarget = 3.290V
    - ConfigTargetSettings() start
    - Flash breakpoints are disabled.
    - ConfigTargetSettings() end - Took 9us
    - InitTarget() start
    - No CFG-AP detected.
    - No SEC-AP detected.
    - Checking if AHB-AP is enabled...
    - AHB-AP enabled --> Attaching to the target...
    - InitTarget() end - Took 190ms
    - ConfigTargetSettings() start
    - Flash breakpoints are disabled.
    - ConfigTargetSettings() end - Took 9us
    - InitTarget() start
    - No CFG-AP detected.
    - No SEC-AP detected.
    - Checking if AHB-AP is enabled...
    - AHB-AP enabled --> Attaching to the target...
    - InitTarget() end - Took 190ms
    - ERROR: Failed to connect.
    Could not establish a connection to target.

    为了说明这一点、我们使用定制电路板、我们不确定晶体振荡器是否工作 正常
    这会影响编程和调试吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Mieszko:

    TI 尚未在内部验证 Segger 调试探针对 CC2340的支持。 我建议向 Segger 团队咨询、他们应该能够提供有关支持的更多信息。

    此致、

    罗格利奥