主题中讨论的其他器件: UNIFLASH、 SEGGER
大家好、
客户正在评估 CC2340R5、但在编程时遇到问题。
客户正在使用最近具有更新的 J-Link Ultra+、以允许 CC2340R5编程。
很遗憾、 客户无法通过 J-Flash V7.88d、CCS 12.3.0或 UniFlash 8.3.0.4307进行连接。
您能否确认应支持该功能?
Br、
斯特凡
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
客户正在评估 CC2340R5、但在编程时遇到问题。
客户正在使用最近具有更新的 J-Link Ultra+、以允许 CC2340R5编程。
很遗憾、 客户无法通过 J-Flash V7.88d、CCS 12.3.0或 UniFlash 8.3.0.4307进行连接。
您能否确认应支持该功能?
Br、
斯特凡
感谢您发送编修。
我成功连接了几次,但它总是无法做更多的事情,下面的日志: Application log started- J-Flash V7.88d (J-Flash compiled May 24 2023 15:24:22)- JLinkARM.dll V7.88d (DLL compiled May 24 2023 15:23:44)Reading flash device list [C:\Program Files\SEGGER\JLink\ETC/JFlash/Flash.csv] ...- List of flash devices read successfully (451 Devices)Reading MCU device list ...- List of MCU devices read successfully (10362 Devices)Creating new project ...- New project created successfullyConnecting ...- Connecting via USB to probe/ programmer device 0- Probe/ Programmer firmware: J-Link Ultra V5-1 compiled May 23 2023 14:45:15- Probe/ Programmer S/N: #########- Device "CC2340R5" selected.- Target interface speed: 100 kHz (Fixed)- VTarget = 3.288V- ConfigTargetSettings() start- Flash breakpoints are disabled.- ConfigTargetSettings() end - Took 13us- InitTarget() start- CFG-AP DEVICEID: 0x1BB8402F- PG2.0 device detected- CFG-AP DEVICESTATUS: 0x030DBA05- Checking if AHB-AP is enabled...- AHB-AP enabled --> Attaching to the target...- InitTarget() end - Took 15.6ms- Found SW-DP with ID 0x6BA02477- DPIDR: 0x6BA02477- CoreSight SoC-400 or earlier- AP map detection skipped. Manually configured AP map found.- AP[0]: AHB-AP (IDR: Not set)- AP[0]: Core found- AP[0]: AHB-AP ROM base: 0xE00FF000- CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)- Found Cortex-M0 r0p1, Little endian.- FPUnit: 4 code (BP) slots and 0 literal slots- CoreSight components:- ROMTbl[0] @ E00FF000- [0][0]: E000E000 CID B105E00D PID 000BB008 SCS- [0][2]: E0002000 CID B105E00D PID 000BB00B FPB- Executing init sequence ...- Executing Reset (0, 0 ms)- ResetTarget() start- Executing reset via SEC-AP in order to enter SACI mode...- O.K.- Executing exit SACI mode sequence...- O.K.- Checking if AHB-AP is enabled...- O.K.- Checking if debug probe loop entered...- O.K.- Invalid application entry addr detected: 0xFFFFFFFF- ResetTarget() end - Took 195ms- Initialized successfully- Target interface speed: 100 kHz (Fixed)- Found 1 JTAG device. Core ID: 0x6BA02477 (None)- Connected successfullyReading entire flash chip ...- 257 sectors, 2 ranges, 0x0 - 0x7FFFF, 0x4E020000 - 0x4E0207FF- Start of preparing flash programming- End of preparing flash programming- WARNING: Blank check not supported for this flash bank, skipped- ERROR: Failed to read memory (0x20000 bytes @ address 0x00000000)- Start of restoring- End of restoring- ERROR: Failed to read back target memoryDisconnecting ...- DisconnectedConnecting ...- Connecting via USB to probe/ programmer device 0- Probe/ Programmer firmware: J-Link Ultra V5-1 compiled May 23 2023 14:45:15- Probe/ Programmer S/N: #########- Device "CC2340R5" selected.- Target interface speed: 100 kHz (Fixed)- VTarget = 3.290V- ConfigTargetSettings() start- Flash breakpoints are disabled.- ConfigTargetSettings() end - Took 9us- InitTarget() start- No CFG-AP detected.- No SEC-AP detected.- Checking if AHB-AP is enabled...- AHB-AP enabled --> Attaching to the target...- InitTarget() end - Took 190ms- ConfigTargetSettings() start- Flash breakpoints are disabled.- ConfigTargetSettings() end - Took 9us- InitTarget() start- No CFG-AP detected.- No SEC-AP detected.- Checking if AHB-AP is enabled...- AHB-AP enabled --> Attaching to the target...- InitTarget() end - Took 190ms- ERROR: Failed to connect.Could not establish a connection to target.
为了说明这一点、我们使用定制电路板、我们不确定晶体振荡器是否工作 正常。
这会影响编程和调试吗?