This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC2652R:如何触发 UART 读回?

Guru**** 2931100 points

Other Parts Discussed in Thread: SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1378087/cc2652r-how-do-i-trigger-a-uart-readcallback

器件型号:CC2652R
主题中讨论的其他器件:SysConfig

工具与软件:

您好!

我 根据  最新的 SDK 7_41_00_17添加了 UART 驱动程序。  我曾提到 uart2callback 例程、但我想通过中断接收数据、而不是在 while 函数中轮询 UART2_read。  因此、我更改了例程、如下所示:

/*
 * Copyright (c) 2020, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ======== uart2callback.c ========
 */
#include <stdint.h>
#include <stddef.h>

/* POSIX Header files */
#include <semaphore.h>

/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/UART2.h>

/* Driver configuration */
#include "ti_drivers_config.h"

static sem_t sem;
static volatile size_t numBytesRead;

char input;
UART2_Handle uart;

/*
 *  ======== callbackFxn ========
 */
void callbackFxn(UART2_Handle handle, void *buffer, size_t count, void *userArg, int_fast16_t status)
{
    GPIO_toggle(CONFIG_GPIO_LED_0);
    if (status != UART2_STATUS_SUCCESS)
    {
        /* RX error occured in UART2_read() */
        while (1) {}
    }

    status = UART2_read(uart, &input, 1, NULL);
            if (status != UART2_STATUS_SUCCESS)
            {
                /* UART2_read() failed */
                while (1) {}
            }

    numBytesRead = count;
    sem_post(&sem);
}

/*
 *  ======== mainThread ========
 */
void *mainThread(void *arg0)
{
    const char echoPrompt[] = "Echoing characters:\r\n";
    UART2_Params uartParams;
    int32_t semStatus;
    uint32_t status = UART2_STATUS_SUCCESS;

    /* Call driver init functions */
    GPIO_init();

    /* Configure the LED pin */
    GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);

    /* Create semaphore */
    semStatus = sem_init(&sem, 0, 0);

    if (semStatus != 0)
    {
        /* Error creating semaphore */
        while (1) {}
    }

    /* Create a UART in CALLBACK read mode */
    UART2_Params_init(&uartParams);
    uartParams.readMode     = UART2_Mode_CALLBACK;
    uartParams.readCallback = callbackFxn;
    uartParams.baudRate     = 115200;
    uartParams.readReturnMode = UART2_ReadReturnMode_PARTIAL;

    uart = UART2_open(CONFIG_UART2_0, &uartParams);

    if (uart == NULL)
    {
        /* UART2_open() failed */
        while (1) {}
    }

    /* Turn on user LED to indicate successful initialization */
    GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);

    /* Pass NULL for bytesWritten since it's not used in this example */
    UART2_write(uart, echoPrompt, sizeof(echoPrompt), NULL);

    /* Loop forever echoing */
    while (1)
    {
        numBytesRead = 0;

//        /* Pass NULL for bytesRead since it's not used in this example */
//        status = UART2_read(uart, &input, 1, NULL);
//
//        if (status != UART2_STATUS_SUCCESS)
//        {
//            /* UART2_read() failed */
//            while (1) {}
//        }

        /* Do not write until read callback executes */
        sem_wait(&sem);

        if (numBytesRead > 0)
        {
            status = UART2_write(uart, &input, 1, NULL);

            if (status != UART2_STATUS_SUCCESS)
            {
                /* UART2_write() failed */
                while (1) {}
            }
        }
    }
}

不幸的是、我没有进入 callbackFxn 函数、我想知道如何触发 readCallback、或者我的配置有什么问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我是偶然解决的。

    修改了以下内容:

    /*
     * Copyright (c) 2020, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== uart2callback.c ========
     */
    #include <stdint.h>
    #include <stddef.h>
    
    /* POSIX Header files */
    #include <semaphore.h>
    
    /* Driver Header files */
    #include <ti/drivers/GPIO.h>
    #include <ti/drivers/UART2.h>
    
    /* Driver configuration */
    #include "ti_drivers_config.h"
    
    static sem_t sem;
    static volatile size_t numBytesRead;
    
    uint8_t input[100] = {0};
    UART2_Handle uart;
    
    /*
     *  ======== callbackFxn ========
     */
    void callbackFxn(UART2_Handle handle, void *buffer, size_t count, void *userArg, int_fast16_t status)
    {
        GPIO_toggle(CONFIG_GPIO_LED_0);
        if (status != UART2_STATUS_SUCCESS)
        {
            /* RX error occured in UART2_read() */
            while (1) {}
        }
    
        status = UART2_read(uart, input, sizeof(input), NULL);
                if (status != UART2_STATUS_SUCCESS)
                {
                    /* UART2_read() failed */
                    while (1) {}
                }
    
        numBytesRead = count;
        sem_post(&sem);
    }
    
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
        const char echoPrompt[] = "Echoing characters:\r\n";
        UART2_Params uartParams;
        int32_t semStatus;
        uint32_t status = UART2_STATUS_SUCCESS;
    
        /* Call driver init functions */
        GPIO_init();
    
        /* Configure the LED pin */
        GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
    
        /* Create semaphore */
        semStatus = sem_init(&sem, 0, 0);
    
        if (semStatus != 0)
        {
            /* Error creating semaphore */
            while (1) {}
        }
    
        /* Create a UART in CALLBACK read mode */
        UART2_Params_init(&uartParams);
        uartParams.readMode     = UART2_Mode_CALLBACK;
        uartParams.readCallback = callbackFxn;
        uartParams.baudRate     = 115200;
        uartParams.readReturnMode = UART2_ReadReturnMode_PARTIAL;
    
        uart = UART2_open(CONFIG_UART2_0, &uartParams);
    
        if (uart == NULL)
        {
            /* UART2_open() failed */
            while (1) {}
        }
    
        status = UART2_read(uart, input, sizeof(input), NULL);
    
        if (status != UART2_STATUS_SUCCESS)
        {
                    /* UART2_read() failed */
                    while (1) {}
        }
    
        /* Turn on user LED to indicate successful initialization */
        GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);
    
        /* Pass NULL for bytesWritten since it's not used in this example */
        UART2_write(uart, echoPrompt, sizeof(echoPrompt), NULL);
    
    
    
        /* Loop forever echoing */
        while (1)
        {
            numBytesRead = 0;
    
    //        /* Pass NULL for bytesRead since it's not used in this example */
    //        status = UART2_read(uart, &input, 1, NULL);
    //
    //        if (status != UART2_STATUS_SUCCESS)
    //        {
    //            /* UART2_read() failed */
    //            while (1) {}
    //        }
    
            /* Do not write until read callback executes */
            sem_wait(&sem);
    
            if (numBytesRead > 0)
            {
                status = UART2_write(uart, input, numBytesRead, NULL);
    
                if (status != UART2_STATUS_SUCCESS)
                {
                    /* UART2_write() failed */
                    while (1) {}
                }
            }
        }
    }
    

    您似乎必须首先调用 UART2_Read 才能进入 readCallback、这与 Nordic 的第一次回调和读取稍有不同。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Ethan:

    感谢您分享您的解决方案!

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Cl é ment:

    顺便说一下、 最新的 SDK 删除了 UART 驱动程序、只保留了 UART2、如何同时使用两个 UART?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您可以使用 SysConfig 定义两个 UART2实例。 两个 UART2实例都应使用 UART2驱动程序。

    我希望这将有所帮助、

    此致、

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的回答