This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-EM-CC2340R5:扫描期间中央设备如何显示外设名称?

Guru**** 2589280 points
Other Parts Discussed in Thread: CC2340R5, SYSCONFIG

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/1384042/lp-em-cc2340r5-how-does-the-central-display-peripheral-names-during-scanning

器件型号:LP-EM-CC2340R5
主题中讨论的其他器件:CC2340R5SysConfig

工具与软件:

尊敬的 TI 团队:

当 CC2340R5 (中央模式)扫描蓝牙设备时、为什么它无法检测到外设的名称和信号强度? 但是、智能手机应用程序(simplink)可在扫描期间显示外设的名称和信号强度。

void Central_ScanEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
    BLEAppUtil_ScanEventData_t *scanMsg = (BLEAppUtil_ScanEventData_t *)pMsgData;

    switch (event)
    {
        case BLEAPPUTIL_SCAN_ENABLED:
        {
            centralScanIndex = 0;
            MenuModule_printf(APP_MENU_SCAN_EVENT, 0, "Scan status: Scan started...");

            break;
        }

        case BLEAPPUTIL_SCAN_DISABLED:
        {
            uint8 i;

            for(i = 0; i < APP_MAX_NUM_OF_ADV_REPORTS; i++)
            {
                memset(&centralScanRes[i], 0, sizeof(App_scanResults));
            }

            // Go over the advertise reports that was saved in the host level and save it
            for (i = 0; i < scanMsg->pBuf->pScanDis.numReport; i++)
            {
              GapScan_Evt_AdvRpt_t advReport;
              // Get the address from the report
              GapScan_getAdvReport(i, &advReport);

              memcpy(watchchar[i],advReport.pData,advReport.dataLen);
              // Add the report to the scan list
              Central_addScanRes(&advReport);


            }
            UART2_write(uart, (const char *)"scan finish !!!\r\n\r\n", strlen((const char *)"scan finish !!!\r\n\r\n"), NULL);

            MenuModule_printf(APP_MENU_SCAN_EVENT, 0, "Scan status: Scan disabled - "
                              "Reason: " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET
                              "Num results: " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
                              scanMsg->pBuf->pScanDis.reason,
                              scanMsg->pBuf->pScanDis.numReport);
            break;
        }

advReport.pData = 0  advReport.dataLen = 0

memcpy(watchchar[i],advReport.pData,advReport.dataLen);