This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F2800137:PI

Guru**** 2979400 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1513581/tms320f2800137-pi

器件型号:TMS320F2800137

工具/软件:

C:\Users\Xiaohua\Desktop\013\x15\universal_motorcontrol_lab_f280013x

大家好、我之前使用了芯片 F28027F。 其速度和电流环路 PI 可直接在主函数中更改、但 f2800137的"user_mtr1.h"文件中有一些与 PI 相关的设置。 如何调整参数? 有何区别?

// Current and Speed PI Regulators Tuning Coefficient
// the low speed threshold for adjusting the Kp and Ki of the speed PI regulator
#define USER_MOTOR1_GAIN_SPEED_LOW_Hz        (60.0f)      // 10%~50% of the rated speed

// the high speed threshold for adjusting the Kp and Ki of the speed PI regulator
#define USER_MOTOR1_GAIN_SPEED_HIGH_Hz       (150.0f)     // 50%~100% of the rated speed

// the gain coefficient to adjust the Kp of the speed PI regulator for startup
#define USER_MOTOR1_KP_SPD_START_SF          (1.5f)       // 0.1~100.0

// the gain coefficient to adjust the Ki of the speed PI regulator for startup
#define USER_MOTOR1_KI_SPD_START_SF          (1.5f)       // 0.1~10.0

// the low gain coefficient  to adjust the Kp of the speed PI regulator
#define USER_MOTOR1_KP_SPD_LOW_SF            (2.0f)       // 0.1~100.0

// the low gain coefficient  to adjust the Ki of the speed PI regulator
#define USER_MOTOR1_KI_SPD_LOW_SF            (2.0f)       // 0.1~10.0

// the high gain coefficient  to adjust the Kp of the speed PI regulator
#define USER_MOTOR1_KP_SPD_HIGH_SF           (1.0f)       // 0.1~100.0

// the high gain coefficient  to adjust the Ki of the speed PI regulator
#define USER_MOTOR1_KI_SPD_HIGH_SF           (1.0f)       // 0.1~10.0

// the low current threshold to adjust the Kp and Ki of the q-axis current PI regulator
#define USER_MOTOR1_GAIN_IQ_LOW_A            (2.0f)       // 10%~50% of the rated current

// the high current threshold to adjust the Kp and Ki of the q-axis current PI regulator
#define USER_MOTOR1_GAIN_IQ_HIGH_A           (6.0f)       // 50%~100% of the rated current

// the gain coefficient to adjust the Kp of the q-axis current PI regulator for startup
#define USER_MOTOR1_KP_IQ_START_SF           (1.5f)       // 0.1~10.0

// the gain coefficient to adjust the Ki of the q-axis current PI regulator for startup
#define USER_MOTOR1_KI_IQ_START_SF           (1.5f)       // 0.1~10.0

// the low gain coefficient to adjust the Kp of the q-axis current PI regulator
#define USER_MOTOR1_KP_IQ_LOW_SF             (2.0f)       // 0.1~10.0

// the low gain coefficient to adjust the Ki of the q-axis current PI regulator
#define USER_MOTOR1_KI_IQ_LOW_SF             (2.0f)       // 0.1~10.0

// the high gain coefficient to adjust the Kp of the d-axis current PI regulator
#define USER_MOTOR1_KP_IQ_HIGH_SF            (1.0f)       // 0.1~10.0

// the high gain coefficient to adjust the Ki of the d-axis current PI regulator
#define USER_MOTOR1_KI_IQ_HIGH_SF            (1.0f)       // 0.1~10.0

// the gain coefficient to adjust the Kp of the q-axis current PI regulator
#define USER_MOTOR1_KP_ID_SF                 (1.0f)       // 0.1~10.0

// the gain coefficient to adjust the Ki of the q-axis current PI regulator
#define USER_MOTOR1_KI_ID_SF                 (1.0f)       // 0.1~10.0
是否有与 PI 相关的详细文档?   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    目前、我们没有有关这些参数的文档。 您可以尝试根据 系统性能调整参数。

    谢谢、

    Jiaxin