This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28035:使用 CLAmath 中的函数编译时显示警告"Data 正被写入自动生成的文件28035 NIMI CLA.I10"

Guru**** 2974170 points

Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1515386/tms320f28035-using-the-function-in-clamath-compiles-with-a-warning-data-is-being-written-to-auto-generated-file-28035-nimi-cla-i10

器件型号:TMS320F28035
Thread 中讨论的其他器件:controlSUITE、 C2000WARE

工具/软件:

我向工程中添加了.lib 文件" cla0 math library.lib"和.h 文件"CLAmath"。 这两个文件都可以在"D":\controlSUITE\controlSUITE\libs\math\CLAmath\v4_02_00_00"中找到、我按照手册中的说明完成配置。 但是、当我在.cla 文件中编写以下语句时、编译后会提示"数据正在写入自动生成的文件28035 NIMI CLA.I10"。 我不知道这是否有任何影响,如何摆脱这个警告,谢谢你的帮助。

_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x200
-stack 0x200

// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are. 
// CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start

MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
   RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
   RAML3       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L3 */
   OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
   FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
   FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
   FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
   FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
   FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
   FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */

   IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
   IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
   IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA	  /* IQ Math Tables in Boot ROM */

   ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */
   BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAML0       : origin = 0x008000, length = 0x000800     /* on-chip RAM block L0 */

   CLARAM0     : origin = 0x008800, length = 0x000400
   CLARAM1     : origin = 0x008C00, length = 0x000400


   CLA1_MSGRAMLOW   : origin = 0x001480, length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500, length = 0x000080
   
   FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */

}

/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/

SECTIONS
{

   /* Allocate program areas: */
   .cinit              : > FLASHA      PAGE = 0
   .pinit              : > FLASHA,     PAGE = 0
   .text               : >> FLASHC | FLASHE      PAGE = 0
   codestart           : > BEGIN       PAGE = 0
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAMM0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
			 LOAD_END(_RamfuncsLoadEnd), /* 所要加载程序在Flash里的结束地址 */
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

   csmpasswds          : > CSM_PWL_P0  PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0

   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1       PAGE = 1
   .cio                : >> RAML0 | RAMM1      PAGE = 1
   .sysmem             : > RAMM1       PAGE = 1
   .ebss               : > RAML0        PAGE = 1
   .esysmem            : > RAML0       PAGE = 1

                     
   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA      PAGE = 0
   .switch             : > FLASHA      PAGE = 0
   
   /* Allocate IQ math areas: */
   IQmath              : > FLASHA      PAGE = 0            /* Math Code */
   IQmathTables        : > IQTABLES,   PAGE = 0, TYPE = NOLOAD
   
   .bss_cla		       : > CLARAM0,   PAGE = 1
   .scratchpad         : > CLARAM0,   PAGE = 1
   
   Cla1Prog            : LOAD = FLASHD,
                         RUN = RAML3,
                         LOAD_START(_Cla1funcsLoadStart),
                         LOAD_END(_Cla1funcsLoadEnd),
                         RUN_START(_Cla1funcsRunStart),
                         LOAD_SIZE(_Cla1funcsLoadSize),
                         PAGE = 0
   
   Cla1ToCpuMsgRAM     : > CLA1_MSGRAMLOW,   PAGE = 1
   CpuToCla1MsgRAM     : > CLA1_MSGRAMHIGH,  PAGE = 1
   Cla1DataRam0		   : > CLARAM0,		  PAGE = 1
   Cla1DataRam1		   : > CLARAM1,		  PAGE = 1
   
   GROUP	           : LOAD = FLASHB,
                         RUN = CLARAM1,
                         LOAD_START(_Cla1mathTablesLoadStart),
                         LOAD_END(_Cla1mathTablesLoadEnd),
                         RUN_START(_Cla1mathTablesRunStart),
                         LOAD_SIZE(_Cla1mathTablesLoadSize),
                         PAGE = 1

   {
    CLA1mathTables
    .const_cla
   }   
	
   CLAscratch          : 
                         { *.obj(CLAscratch)
                         . += CLA_SCRATCHPAD_SIZE;
                         *.obj(CLAscratch_end) } > CLARAM0,
					     PAGE = 1
					 
  /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
/*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

   }
*/
    /* Uncomment the section below if calling the IQNasin() or IQasin()
       functions from the IQMath.lib library in order to utilize the
       relevant IQ Math table in Boot ROM (This saves space and Boot ROM
       is 1 wait-state). If this section is not uncommented, IQmathTables2
       will be loaded into other memory (SARAM, Flash, etc.) and will take
       up space, but 0 wait-state is possible.
    */
/*
    IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

               IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
*/

   /* .reset is a standard section used by the compiler.  It contains the */
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT

}
我上传了 cmd 文件

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Chengqi:

    您可以看看如何利用 C2000Ware SDK 中提供的 CLAMath 库。 请注意、C2000Ware 托管着最新的示例、库和 device _support。 不再维护 controlSUITE。 如果您仍有任何警告或错误消息、请告知我们。 如果是、请将控制台日志附加到论坛帖子。 谢谢你。

    此致、

    Ozino

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我已按照路径"D:\controlSUITE\controlSUITE\libs\math\CLAmath\v4_02_00_00\00\doc"中所述对其进行设置、但仍会发出警告。

    **** Build of configuration Debug for project 28035_NIMI_CLA ****
    
    "G:\\Ti\\ccs\\utils\\bin\\gmake" -k all 
     
    Building file: "../main.c"
    Invoking: C2000 Compiler
    "I:/ccs12.8/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla0 --float_support=softlib -Ooff --include_path="G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_headers/include" --include_path="D:/CONTROLSUITE/controlSUITE/libs/math/CLAmath/v4_02_00_00/include" --include_path="G:/DSP_Aalarg/28035_NIMI_CLA" --include_path="I:/ccs12.8/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --include_path="G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/include" --include_path="G:/DSP_Aalarg/28035_NIMI_CLA/inc" --include_path="G:/DSP_Aalarg/28035_NIMI_CLA/Debug" --include_path="C:/ti/bios_5_42_02_10/packages/ti/bios/include" --include_path="C:/ti/bios_5_42_02_10/packages/ti/rtdx/include/c2000" --advice:performance=all -g --diag_warning=225 --display_error_number --abi=coffabi --preproc_with_compile --preproc_dependency="main.d_raw"  "../main.c"
    Finished building: "../main.c"
     
    Building target: "28035_NIMI_CLA.out"
    Invoking: C2000 Linker
    "I:/ccs12.8/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla0 --float_support=softlib -Ooff --advice:performance=all -g --diag_warning=225 --display_error_number --abi=coffabi -z -m"28035_NIMI_CLA.map" --heap_size=0x400 --stack_size=0x300 --warn_sections -i"E:/DSPproject/eg1_DSP28035_GPIO/libs/math/IQmath/v160/lib" -i"E:/DSPproject/eg1_DSP28035_GPIO/libs/math/IQmath/v160/include" -i"G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/lib" -i"I:/ccs12.8/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/lib" -i"I:/ccs12.8/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" -i"C:/ti/bios_5_42_02_10/packages/ti/rtdx/lib/c2000" -i"C:/ti/bios_5_42_02_10/packages/ti/bios/lib" -i"D:/CONTROLSUITE/controlSUITE/libs/math/CLAmath/v4_02_00_00/lib" --priority --reread_libs --define=CLA_SCRATCHPAD_SIZE=0x100 --display_error_number --xml_link_info="28035_NIMI_CLA_linkInfo.xml" --rom_model -o "28035_NIMI_CLA.out" "./Controller.obj" "./main.obj" "./DSP2803x_common/source/DSP2803x_Adc.obj" "./DSP2803x_common/source/DSP2803x_CSMPasswords.obj" "./DSP2803x_common/source/DSP2803x_CodeStartBranch.obj" "./DSP2803x_common/source/DSP2803x_CpuTimers.obj" "./DSP2803x_common/source/DSP2803x_DBGIER.obj" "./DSP2803x_common/source/DSP2803x_DefaultIsr.obj" "./DSP2803x_common/source/DSP2803x_DisInt.obj" "./DSP2803x_common/source/DSP2803x_ECan.obj" "./DSP2803x_common/source/DSP2803x_ECap.obj" "./DSP2803x_common/source/DSP2803x_EPwm.obj" "./DSP2803x_common/source/DSP2803x_EQep.obj" "./DSP2803x_common/source/DSP2803x_GlobalVariableDefs.obj" "./DSP2803x_common/source/DSP2803x_Gpio.obj" "./DSP2803x_common/source/DSP2803x_HRCap.obj" "./DSP2803x_common/source/DSP2803x_I2C.obj" "./DSP2803x_common/source/DSP2803x_Lin.obj" "./DSP2803x_common/source/DSP2803x_MemCopy.obj" "./DSP2803x_common/source/DSP2803x_OscComp.obj" "./DSP2803x_common/source/DSP2803x_PieCtrl.obj" "./DSP2803x_common/source/DSP2803x_PieVect.obj" "./DSP2803x_common/source/DSP2803x_Sci.obj" "./DSP2803x_common/source/DSP2803x_Spi.obj" "./DSP2803x_common/source/DSP2803x_SysCtrl.obj" "./DSP2803x_common/source/DSP2803x_TempSensorConv.obj" "./DSP2803x_common/source/DSP2803x_usDelay.obj" "./DSP2803x_common/source/DSP2803x_user.obj" "./DSP2803x_common/source/Example_Flash2803x_API.obj" "./DSP2803x_common/source/Example_Flash2803x_CsmKeys.obj" "I:/workspace12.8/F28035_CLA_C.cmd" "../DSP2803x_common/lib/2803x_FlashAPI_BootROMSymbols.lib" "../DSP2803x_common/lib/Flash2803x_API_V100.lib" "../DSP2803x_common/lib/IQmath.lib" "../DSP2803x_common/lib/SFO_TI_Build_V6.lib" "../DSP2803x_common/lib/SFO_TI_Build_V6b.lib" "../DSP2803x_common/lib/Solar_Lib_CLA.lib" "../DSP2803x_common/lib/cla0_math_library.lib" "../DSP2803x_common/lib/cla0_math_library_datarom.lib" "../DSP2803x_headers/cmd/DSP2803x_Headers_nonBIOS.cmd"  -lrts2800_ml.lib -l"D:/CONTROLSUITE/controlSUITE/libs/math/CLAmath/v4_02_00_00/lib/cla0_math_library.lib" -l"G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/lib/2803x_FlashAPI_BootROMSymbols.lib" -l"G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/lib/IQmath.lib" -l"G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/lib/Solar_Lib_CLA.lib" -l"G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/lib/SFO_TI_Build_V6b.lib" -l"G:/DSP_Aalarg/28035_NIMI_CLA/DSP2803x_common/lib/SFO_TI_Build_V6.lib" 
    <Linking>
    Finished building target: "28035_NIMI_CLA.out"
     
    Create flash image: Intel-HEX
    "I:/ccs12.8/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/hex2000" -i "28035_NIMI_CLA.out" -o "28035_NIMI_CLA.hex" -order MS -romwidth 16
    Translating to Intel format...
       "28035_NIMI_CLA.out" Cla1Prog ==> Cla1Prog
       "28035_NIMI_CLA.out" ramfuncs ==> ramfuncs
       "28035_NIMI_CLA.out" .text ==> .text
       "28035_NIMI_CLA.out" .econst ==> .econst
       "28035_NIMI_CLA.out" .cinit ==> .cinit
       "28035_NIMI_CLA.out" IQmath ==> IQmath
       "28035_NIMI_CLA.out" csm_rsvd ==> csm_rsvd
       "28035_NIMI_CLA.out" codestart ==> codestart
       "28035_NIMI_CLA.out" csmpasswds ==> csmpasswds
       "28035_NIMI_CLA.out" CLA1mathTables ==> CLA1mathTables
     
    warning: Data is being written to auto-generated file 28035_NIMI_CLA.i10
    
    **** Build Finished ****
    

    控制台日志已上传、谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否尝试在应用程序中创建 INTEL-HEX 二进制文件? 如果是、请确保按照此论坛帖子 https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code-composer-studio-forum/909069/c2000-hex-utility-auto-generated-file 中详细介绍的步骤进行操作

    有关更多详细信息、请参阅  《C28x 汇编工具手册》 中标题为 了解存储器宽度的子章节