This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280033:代码没有&'无法从闪存引导

Guru**** 2860250 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1603915/tms320f280033-code-doesn-t-boot-from-flash

器件型号: TMS320F280033

您好、

我在为我的工程对 F280033 器件进行编程 时遇到了困难(请参阅本主题)。 推荐的解决方案是更改.cmd 文件、我根据建议更改了该文件。

但是、即使 BOOT 引脚配置正确(上拉 GPIO 24 和 GPIO 32)、该器件也不会从闪存引导。  

我建议使用 此主题、这表明修改后的.cmd 文件与引导加载程序地址不兼容。

是否可以为我提供所需的步骤和修改以使部件从闪存正确引导?

提前感谢、  

Adrien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Adrien:

    您能否共享链接器 cmd 文件进行分析?

    您是否在引导引脚为“从闪存引导“时尝试过 SDKin 闪存配置中的任何示例

    谢谢

    Aswin

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Aswin:

    这是我使用的 cmd 文件。

    /*
       Copyright (c) 2019-2021 by Plexim GmbH
       All rights reserved.
    
       A free license is granted to anyone to use this software for any legal
       non safety-critical purpose, including commercial applications, provided
       that:
       1) IT IS NOT USED TO DIRECTLY OR INDIRECTLY COMPETE WITH PLEXIM, and
       2) THIS COPYRIGHT NOTICE IS PRESERVED in its entirety.
    
       THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS
       OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
       FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE
       AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER
       LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM,
       OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
       SOFTWARE.
     */
    
    MEMORY
    {
       BEGIN          : origin = 0x088000, length = 0x000002
       BOOT_RSVD      : origin = 0x00000002, length = 0x00000126
       RAMM0          : origin = 0x00000128, length = 0x000002D8
       RAMM1          : origin = 0x00000400, length = 0x000003F8
       // RAMM1_RSVD  : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       BOOTROM          : origin = 0x003F8000, length = 0x00007FC0
       SECURE_ROM       : origin = 0x003F2000, length = 0x00006000
       RESET            : origin = 0x003FFFC0, length = 0x00000002
    
       RAMLS	         : origin = 0x008000, length = 0x003F00
       //RAMLS0       : origin = 0x008000, length = 0x000800
       //RAMLS1       : origin = 0x008800, length = 0x000800
       //RAMLS2       : origin = 0x009000, length = 0x000800
       //RAMLS3       : origin = 0x009800, length = 0x000800
       //RAMLS4       : origin = 0x00A000, length = 0x000800
       //RAMLS5       : origin = 0x00A800, length = 0x000800
       //RAMLS6       : origin = 0x00B000, length = 0x000800
       //RAMLS7       : origin = 0x00B800, length = 0x000800
       RAMLS7_RSVD    : origin = 0x00BF00, length = 0x000100  // JTAG communication buffer
    
       // we do not utilize any RAMGS RAM, as this memory is used for page 0
       // by the "ram_lnk" configuration
    
       //RESET          : origin = 0x3FFFC0, length = 0x000002
    
       //BEGIN          : origin = 0x080000, length = 0x000002     // Flash Bank 0
          /* Flash sectors */
       /* BANK 0 */
       FLASH_BANK0	    : origin = 0x088002, length = 0x007FFE	/* on-chip Flash */ 
       //FLASH_BANK0_SEC0  : origin = 0x080002, length = 0x000FFE
       //FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000
       //FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000
       //FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000
       //FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000
       //FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000
       //FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000
       //FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000
       // FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000
       // FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000
       // FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000
       // FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000
       // FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000
       // FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000
       // FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000
       // FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000
    
       /* BANK 1 */
       FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000
       FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000
       FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000
       FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000
       FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000
       FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000
       FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000
       FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000
       // FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000
       // FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000
       // FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000
       // FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000
       // FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000
       // FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000
       // FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000
       // FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000
    
      /* BANK 2 */
       // FLASH_BANK2_SEC0  : origin = 0x0A0000, length = 0x001000
       // FLASH_BANK2_SEC1  : origin = 0x0A1000, length = 0x001000
       // FLASH_BANK2_SEC2  : origin = 0x0A2000, length = 0x001000
       // FLASH_BANK2_SEC3  : origin = 0x0A3000, length = 0x001000
       // FLASH_BANK2_SEC4  : origin = 0x0A4000, length = 0x001000
       // FLASH_BANK2_SEC5  : origin = 0x0A5000, length = 0x001000
       // FLASH_BANK2_SEC6  : origin = 0x0A6000, length = 0x001000
       // FLASH_BANK2_SEC7  : origin = 0x0A7000, length = 0x001000
       // FLASH_BANK2_SEC8  : origin = 0x0A8000, length = 0x001000
       // FLASH_BANK2_SEC9  : origin = 0x0A9000, length = 0x001000
       // FLASH_BANK2_SEC10 : origin = 0x0AA000, length = 0x001000
       // FLASH_BANK2_SEC11 : origin = 0x0AB000, length = 0x001000
       // FLASH_BANK2_SEC12 : origin = 0x0AC000, length = 0x001000
       // FLASH_BANK2_SEC13 : origin = 0x0AD000, length = 0x001000
       // FLASH_BANK2_SEC14 : origin = 0x0AE000, length = 0x001000
       // FLASH_BANK2_SEC15 : origin = 0x0AF000, length = 0x000FF0
    
       //FLASH_BANK0_SEC15_RSVD     : origin = 0x0AFFF0, length = 0x000010  /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
    }
    
    SECTIONS
    {
       scope            : > RAMLS, ALIGN(2)
       step             : > FLASH_BANK0, ALIGN(4)
       dispatch         : > FLASH_BANK0, ALIGN(4)
    
       codestart        : > BEGIN, ALIGN(4)
       .text            : > FLASH_BANK0, ALIGN(4)
       .cinit           : > FLASH_BANK0, ALIGN(4)
       .switch          : > FLASH_BANK0, ALIGN(4)
    
       .stack           : > RAMM1 | RAMLS
    
    #if defined(__TI_EABI__)
       .init_array      : > FLASH_BANK0, ALIGN(4)
       .const           : > FLASH_BANK0, ALIGN(4)
       .bss             : > RAMLS
       .bss:output      : > RAMLS
       .bss:cio         : > RAMLS
       .data            : > RAMLS
       .sysmem          : > RAMLS
    #else
       .pinit           : > FLASH_BANK0, ALIGN(4)
       .econst          : > FLASH_BANK0, ALIGN(4)
       .cio             : > FLASH_BANK0, ALIGN(4)
       .ebss            : > RAMLS
       .esysmem         : > RAMLS
    #endif
    
        GROUP      : LOAD = FLASH_BANK0,
                    RUN = RAMLS,
    #if defined(__TI_EABI__)
                    LOAD_START(RamfuncsLoadStart),
                    LOAD_END(RamfuncsLoadEnd),
                    RUN_START(RamfuncsRunStart),
                    LOAD_SIZE(RamfuncsLoadSize),
    #else
                    LOAD_START(_RamfuncsLoadStart),
                    LOAD_END(_RamfuncsLoadEnd),
                    RUN_START(_RamfuncsRunStart),
                    LOAD_SIZE(_RamfuncsLoadSize),
    #endif
                    ALIGN(4)
       {
          ramfuncs
          .TI.ramfunc
       }
       .reset           : > RESET, TYPE = DSECT /* not used, */
     }
    

    它是 Plexim 作为 C2000 代码生成包的一部分提供的默认 F280039 cmd 文件的修改版本。 我根据 这个讨论主题对其进行了修改。

    据我所知、SDK 中的所有示例都使用默认的 TI F28003x cmd 文件、该文件与 F280033 不兼容。 因此,上述讨论主题。

    此致、

    Adrien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Aswin:

    很抱歉坚持,但这个问题已经变得非常紧迫。 我应该在下周向我的客户交付一个工作原型、并且在每次电源循环都不符合“工作原型“的定义时、必须重新编程微控制器。

    此外,如果你包括原来的帖子(这里),我现在知道我只得到一半的解决我的问题,这个问题已经持续了 6 个月。

    请,我真的需要这个问题修复,并迅速!

    Adrien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    一位同事发现了 这一主题、似乎与我的问题相符。

    应用建议的修复程序似乎是有效的。 但是、一旦应用、这将不会转化为将来要进行编程的电路板

    -->每次编程电路板时、如何自动完成此操作?

    -->我如何使我的同事透明(即是否有一个可应用 git-able 的文件)?

    提前感谢、

    Adrien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    有什么想法,我怎么可以做到这一点,请?

    提前感谢、

    Adrien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Adrien:

    让我向应用专家介绍一下。

    谢谢

    Aswin

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Adrien,

    请查看本应用手册 https://www.ti.com/lit/ug/sprujh3/sprujh3.pdf 、具体来说是   第 55 页上的第 5.5 节、使用闪存 API 插件在 OTP 中写入值。  这将提供修改 main.c 和.cmd 文件的说明、从而在.out 文件中包含上面提到的 OTP 所需的修改、以便在加载代码时对 OTP 进行编程。

    如果您还有其他问题、请告诉我。

    此致、

    Matthew

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Matthew、

    谢谢、工作顺利。

    此致、

    Adrien

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Aswin、Matthew、

    感谢你的帮助。 按照与客户达成的协议关闭此案例。


    此致、
    François μ s。