This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:使用最大 VS 运行时 IS08过调问题

Guru**** 2964790 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1068544/tms320f280049c-is08-overmodulation-issue-when-runing-with-max-vs

部件号:TMS320F280049C
“主题:MOTORWARE”中讨论的其它部件

您好,我有两个自定义主板,一个使用 F280054F,另一个使用 F280049C。

使用相同的电动机,相同的 PWM 频率为15KHz,我可以使用实验10a 到 F280054F 使用 US_MAX_VS_MAG_PU =0.66,最大速度/最大负载稳定。

但是,使用 Is08 by F280049C 时,我无法平稳运行 USER_MAX_VS_MAG_PU=0.66,电动机会以高相电流峰值振动很多。但电动机运行正常,但低于0.5。

唯一的区别是,我使用带有 F280049C 的内置 PGA 进行电流感应,并使用带有 F280054F 的外置运算。

我知道这两个 MCU 的区别,因此我将 PI 段从 PU 更改为 SI,以确保这两个 proj/ECTS 在速度和电流环路上都具有相同的 PI 段。

当前环路带宽    :Float32_t BWC_rps = 0.25 / user_CTRL_Period_sec;(使用摩托车解决方案保持不变)

当前的采样问题是否存在? 外部操作是否适用于过度调制情况?

我们将感谢您的任何建议。

以下是使用低侧分流器0.002Ω Ω 的电流感应电路。

以下是 user.h 代码:

//#############################################################################
// $TI Release: MotorControl SDK v3.01.00.00 $
// $Release Date: Mon Jan 11 11:23:03 CST 2021 $
// $Copyright:
// Copyright (C) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
// 
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################

#ifndef USER_H
#define USER_H

//! \file   solutions/tmdshvmtrinspin/f28004x/drivers/user.h
//! \brief  Contains the user related definitions
//!


// **************************************************************************
// the includes

// modules
#include "userParams.h"

//!
//!
//! \defgroup USER USER
//!
//@{


#ifdef __cplusplus
extern "C" {
#endif


// **************************************************************************
// the defines
//! \brief Defines the nominal DC bus voltage, V
//!
#define USER_NOMINAL_DC_BUS_VOLTAGE_V          ((float32_t)(400.0))


//! \brief Defines the maximum voltage at the AD converter
//!
#define USER_ADC_FULL_SCALE_VOLTAGE_V         ((float32_t)(592.58))         // Full scale voltage of AD converter, not the current voltage


//! \brief Defines the maximum current at the AD converter
//!
#define USER_ADC_FULL_SCALE_CURRENT_A         ((float32_t)(150.0))          // High Voltage motor control kit

//! \brief Defines the analog voltage filter pole location, Hz
//!
#define USER_VOLTAGE_FILTER_POLE_Hz           ((float32_t)(565.25))

/*#define USER_VOLTAGE_FILTER_POLE_Hz           ((float32_t)(805.5))*/



//! \brief ADC current offsets for A, B, and C phases
#define   IA_OFFSET_A    (-74.0117264)            // ~=0.5*USER_ADC_FULL_SCALE_CURRENT_A
#define   IB_OFFSET_A    (-73.5474014)            // ~=0.5*USER_ADC_FULL_SCALE_CURRENT_A
#define   IC_OFFSET_A    (-73.7967606)            // ~=0.5*USER_ADC_FULL_SCALE_CURRENT_A


//! \brief ADC voltage offsets for A, B, and C phases
#define   VA_OFFSET_V    (0.990514159)             // ~=1.0
#define   VB_OFFSET_V    (0.986255884)             // ~=1.0
#define   VC_OFFSET_V    (0.983381569)             // ~=1.0


//! \brief Vbus used to calculate the voltage offsets A, B, and C
#define   VBUS_OFFSET_V  (0.5*USER_ADC_FULL_SCALE_VOLTAGE_V)     // =0.5*USER_NOMINAL_DC_BUS_VOLTAGE_V


//! \brief Defines the maximum negative current to be applied in Id reference
//!
#define USER_MAX_NEGATIVE_ID_REF_CURRENT_A    ((float32_t)(-2.0))


//! \brief Defines the number of pwm clock ticks per isr clock tick
//!        Note: Valid values are 1, 2 or 3 only
#define USER_NUM_PWM_TICKS_PER_ISR_TICK        (1)

//! \brief Defines the number of ISR clock ticks per current controller clock tick
//!
#define USER_NUM_ISR_TICKS_PER_CURRENT_TICK     (1)


//! \brief Defines the number of ISR clock ticks per speed controller clock tick
//!
#define USER_NUM_ISR_TICKS_PER_SPEED_TICK     (16)


//! \brief Defines the number of current sensors
//!
#define USER_NUM_CURRENT_SENSORS               (3)


//! \brief Defines the number of voltage sensors
//!
#define USER_NUM_VOLTAGE_SENSORS               (3)

//! \brief Defines the system maximum input frequency, MHz
//!
#define USER_MAXIMUM_SCALE_FREQ_Hz    ((float32_t)(1000.0))

//! \brief Defines the system clock frequency, MHz
//!
#define USER_SYSTEM_FREQ_MHz       ((float32_t)(100.0))


//! \brief Defines the Pulse Width Modulation (PWM) frequency, kHz
//!
//#define USER_PWM_FREQ_kHz          ((float32_t)(5.0))              //5KHz PWM frequency
//#define USER_PWM_FREQ_kHz          ((float32_t)(10.0))              //10KHz PWM frequency
//#define USER_PWM_FREQ_kHz          ((float32_t)(12.0))              //12KHz PWM frequency
#define USER_PWM_FREQ_kHz          ((float32_t)(16.0))              //15KHz PWM frequency
//#define USER_PWM_FREQ_kHz          ((float32_t)(20.0))            //20KHz PWM frequency

//! \brief Defines the Pulse Width Modulation (PWM) period, usec
//!
#define USER_PWM_PERIOD_usec       ((float32_t)1000.0/USER_PWM_FREQ_kHz)


//! \brief Defines the Interrupt Service Routine (ISR) frequency, Hz
//!
#define USER_ISR_FREQ_Hz           (USER_PWM_FREQ_kHz * (float32_t)1000.0 / (float32_t)USER_NUM_PWM_TICKS_PER_ISR_TICK)


//! \brief Defines the Interrupt Service Routine (ISR) period, usec
//!
#define USER_ISR_PERIOD_usec       (USER_PWM_PERIOD_usec * (float32_t)USER_NUM_PWM_TICKS_PER_ISR_TICK)


#ifdef _VSF_EN_
//! \brief Defines the timer frequency for estimator, kHz
//!
#define USER_EST_FREQ_kHz       ((float32_t)(20.0))


//! \brief Defines the timer frequency for estimator, Hz
//!
#define USER_EST_FREQ_Hz        (USER_EST_FREQ_kHz * (float32_t)1000.0)


//! \brief Defines the Interrupt Service Routine (ISR) period, usec
//!
#define USER_EST_PERIOD_usec    ((float32_t)1000000.0/USER_EST_FREQ_Hz)


//! \brief Defines the timer frequency for controller, Hz
//!
#define USER_CTRL_FREQ_Hz        (USER_EST_FREQ_Hz)


//! \brief Defines the controller execution period, usec
//!
#define USER_CTRL_PERIOD_usec   (USER_EST_PERIOD_usec)


//! \brief Defines the controller execution period, sec
//!
#define USER_CTRL_PERIOD_sec    ((float32_t)USER_CTRL_PERIOD_usec/(float32_t)1000000.0)


//! \brief Defines the timer frequency for trajectory, Hz
//!
#define USER_TRAJ_FREQ_Hz       (USER_EST_FREQ_Hz)
#else
//! \brief Defines the timer frequency for estimator, kHz
//!
#define USER_EST_FREQ_Hz        (USER_ISR_FREQ_Hz)


//! \brief Defines the Interrupt Service Routine (ISR) period, usec
//!
#define USER_EST_PERIOD_usec    (USER_ISR_PERIOD_usec)


//! \brief Defines the timer frequency for controller, Hz
//!
#define USER_CTRL_FREQ_Hz        (USER_ISR_FREQ_Hz)


//! \brief Defines the controller execution period, usec
//!
#define USER_CTRL_PERIOD_usec   (USER_ISR_PERIOD_usec)


//! \brief Defines the controller execution period, sec
//!
#define USER_CTRL_PERIOD_sec    ((float32_t)USER_CTRL_PERIOD_usec/(float32_t)1000000.0)

//! \brief Defines the timer frequency for trajectory, Hz
//!
#define USER_TRAJ_FREQ_Hz       (USER_ISR_FREQ_Hz)
#endif  // _VPF_EN_


//! \brief Defines the direct voltage (Vd) scale factor
//!
#define USER_VD_SF                 ((float32_t)(0.95))


//! \brief Defines the voltage scale factor for the system
//!
#define USER_VOLTAGE_SF               (USER_ADC_FULL_SCALE_VOLTAGE_V / (float32_t)4096.0)            // 12 bit ADC, 2^12 = 4096
#define USER_DCBUS_VOLTAGE_SF         (USER_ADC_FULL_SCALE_DCBUS_VOLTAGE_V / (float32_t)4096.0)      // 12 bit ADC, 2^12 = 4096

//! \brief Defines the current scale factor for the system
//!
#define USER_CURRENT_SF               (USER_ADC_FULL_SCALE_CURRENT_A / (float32_t)4096.0)    // 12 bit ADC, 2^12 = 4096


//! \brief Defines the pole location for the DC bus filter, rad/sec
//!
#define USER_DCBUS_POLE_rps            ((float32_t)(100.0))


//! \brief Defines the pole location for the voltage and current offset estimation, rad/s
//!
#define USER_OFFSET_POLE_rps            ((float32_t)(20.0))


//| \default value 100 rps
//! \brief Defines the pole location for the speed control filter, rad/sec
//!
/*#define USER_SPEED_POLE_rps        ((float32_t)(100.0))*/
#define USER_SPEED_POLE_rps        ((float32_t)(100.0))



//! \brief Defines the analog voltage filter pole location, rad/s
//!
#define USER_VOLTAGE_FILTER_POLE_rps  (MATH_TWO_PI * USER_VOLTAGE_FILTER_POLE_Hz)

//! \brief Defines the maximum Vs magnitude in per units allowed
//!        This value sets the maximum magnitude for the output of the Id and
//!        Iq PI current controllers. The Id and Iq current controller outputs
//!        are Vd and Vq. The relationship between Vs, Vd, and Vq is:
//!        Vs = sqrt(Vd^2 + Vq^2).  In this FOC controller, the Vd value is set
//!        equal to USER_MAX_VS_MAG*USER_VD_MAG_FACTOR.
//!        so the Vq value is set equal to sqrt(USER_MAX_VS_MAG^2 - Vd^2).
//!
//!        Set USER_MAX_VS_MAG = 0.5 for a pure sinewave with a peak at
//!        SQRT(3)/2 = 86.6% duty cycle.  No current reconstruction
//!        is needed for this scenario.
//!
//!        Set USER_MAX_VS_MAG = 1/SQRT(3) = 0.5774 for a pure sinewave
//!        with a peak at 100% duty cycle.  Current reconstruction
//!        will be needed for this scenario (Lab08).
//!
//!        Set USER_MAX_VS_MAG = 2/3 = 0.6666 to create a trapezoidal
//!        voltage waveform.  Current reconstruction will be needed
//!        for this scenario (Lab08).
//!
//!        For space vector over-modulation, see lab08 for details on
//!        system requirements that will allow the SVM generator to
//!        go all the way to trapezoidal.
//!
//#define USER_MAX_VS_MAG_PU            (0.66)
//#define USER_MAX_VS_MAG_PU            (0.57)
#define USER_MAX_VS_MAG_PU              (0.66)


//! \brief Defines the reference Vs magnitude in per units allowed
//! \      Set the value equal from 0.5 to 0.95 of the maximum Vs magnitude
#define USER_VS_REF_MAG_PU              ((float32_t)(0.95) * USER_MAX_VS_MAG_PU)


//! \brief Defines the R/L excitation frequency, Hz
//!
#define USER_R_OVER_L_EXC_FREQ_Hz  ((float32_t)(300.0))


//! \brief Defines the R/L Kp scale factor, pu
//!        Kp used during R/L is USER_R_OVER_L_KP_SF * USER_NOMINAL_DC_BUS_VOLTAGE_V / USER_MOTOR_MAX_CURRENT_A;
//!
#define USER_R_OVER_L_KP_SF        ((float32_t)(0.02))


//! \brief Defines maximum acceleration for the estimation speed profiles, Hz/sec
//!
#define USER_MAX_ACCEL_Hzps        ((float32_t)(2.0))


//! \brief Defines the IdRated delta to use during estimation
//!
#define USER_IDRATED_DELTA_A       ((float32_t)(0.0001))


//! \brief Defines the forced angle frequency, Hz
//!
#define USER_FORCE_ANGLE_FREQ_Hz            ((float32_t)(3.0))


//! \brief Defines the fraction of IdRated to use during inductance estimation
//!
#define USER_IDRATED_FRACTION_FOR_L_IDENT    ((float32_t)(0.5))


//! \brief Defines the fraction of SpeedMax to use during inductance estimation
//!
#define USER_SPEEDMAX_FRACTION_FOR_L_IDENT  ((float32_t)(1.0))


//! \brief Defines the Power Warp gain for computing Id reference
//!        If motor parameters are known, set this gain to:
//!        USER_PW_GAIN = SQRT(1.0 + USER_MOTOR_Rr_Ohm / USER_MOTOR_Rs_Ohm)
//!
#define USER_PW_GAIN                        ((float32_t)(1.0))

//! \brief Defines the scale factor for the flux estimation
//! the default value is 1.0f, change the value between 0.1f and 1.25f
//!
#define USER_EST_FLUX_HF_SF                 ((float32_t)(0.125))


//! \brief Defines the scale factor for the frequency estimation
//! the default value is 1.0f, change the value between 0.5f and 1.5f
//!
#define USER_EST_FREQ_HF_SF                 ((float32_t)(1.5f))


//! \brief Defines the scale factor for the bemf estimation
//! the default value is 1.0f, change the value between 0.50f and 1.25f
//!
#define USER_EST_BEMF_HF_SF                 ((float32_t)(1.25f))

//! \brief A flag to bypass motor identification (1/0 : true/false)
//!
#define USER_BYPASS_MOTOR_ID       (1)          // No motor parameters identification
//#define USER_BYPASS_MOTOR_ID        (0)           // Do motor parameters identification

#define USER_ENABLE_MOTOR_ID        0
#define USER_DISABLE_MOTOR_ID       1


/*
//! brief Define the Kp gain for Field Weakening Control
#define USER_FWC_KP                 0.05

//! brief Define the Ki gain for Field Weakening Control
#define USER_FWC_KI                 0.0002
*/

/*
//! brief Define the Kp gain for Field Weakening Control
#define USER_FWC_KP                 0.25

//! brief Define the Ki gain for Field Weakening Control
#define USER_FWC_KI                 0.001
*/

/*
//! brief Define the Kp gain for Field Weakening Control
#define USER_FWC_KP                 0.035

//! brief Define the Ki gain for Field Weakening Control
#define USER_FWC_KI                 0.00075
*/

//! brief Define the Kp gain for Field Weakening Control
#define USER_FWC_KP                 0.05

//! brief Define the Ki gain for Field Weakening Control
#define USER_FWC_KI                 0.0002

//! \brief Defines the number of isr ticks per field weakening clock tick
//!
#define FW_NUM_ISR_TICKS_PER_CTRL_TICK   (16)


//! brief Define the maximum current vector angle for Field Weakening Control
#define USER_FWC_MAX_ANGLE          (float32_t)(-75.0)                              // degree
#define USER_FWC_MAX_ANGLE_RAD      USER_FWC_MAX_ANGLE*MATH_PI/((float32_t)(180.0))   // rad

//! brief Define the minimum current vector angle for Field Weakening Control
#define USER_FWC_MIN_ANGLE          (float32_t)(-30.0)                                // degree
#define USER_FWC_MIN_ANGLE_RAD      USER_FWC_MIN_ANGLE*MATH_PI/((float32_t)(180.0))   // rad

//! brief Define the maximum current vector angle for Field Weakening Control
#define USER_FWC_MIN_CURRENT        (float32_t)(-0.7 *USER_MOTOR_MAX_CURRENT_A)
#define USER_FWC_MAX_CURRENT        0

//============================================================================================
// Motor defines

//************** Motor Parameters **************

// PMSM motors
#define Estun_EMJ_04APB22_A         101
#define Estun_EMJ_04APB22_B         102
#define Marathon_N56PNRA10102       103
#define Anaheim_BLWS235D_160V       104

#define Teknic_M2310PLN04K          121
#define Anaheim_BLY172S_24V         122
#define Anaheim_BLY341S_48V         123
#define Anaheim_BLY341S_24V         124

#define Traxxas_Velineon_380        131
#define Traxxas_Velineon_3500       132
#define Pacific_Scientific          133
#define Regal_Beloit_5SME39DL0756   134
#define AutoRadiatorFan             135

#define philips_respirator          141
#define tekin_redline_4600KV        142

// ACIM motors
#define Marathon_5K33GN2A           201
#define Marathon_56H17T2011A        202
#define Dayton_3N352C               203

#define my_motor_1                  301

//#define USER_MOTOR Estun_EMJ_04APB22_A
//#define USER_MOTOR Estun_EMJ_04APB22_B
//#define USER_MOTOR Marathon_N56PNRA10102
//#define USER_MOTOR Anaheim_BLWS235D_160V

//#define USER_MOTOR Teknic_M2310PLN04K
//#define USER_MOTOR Anaheim_BLY172S_24V
//#define USER_MOTOR Anaheim_BLY341S_48V
//#define USER_MOTOR Anaheim_BLY341S_24V

//#define USER_MOTOR Traxxas_Velineon_380
//#define USER_MOTOR Traxxas_Velineon_3500
//#define USER_MOTOR Pacific_Scientific
//#define USER_MOTOR Regal_Beloit_5SME39DL0756
//#define USER_MOTOR AutoRadiatorFan

//#define USER_MOTOR philips_respirator
//#define USER_MOTOR tekin_redline_4600KV

//#define USER_MOTOR Marathon_5K33GN2A
//#define USER_MOTOR Marathon_56H17T2011A
//#define USER_MOTOR Dayton_3N352C

#define USER_MOTOR my_motor_1
//#define USER_MOTOR my_motor_2

#if (USER_MOTOR == Estun_EMJ_04APB22_A)
#define USER_MOTOR_TYPE                    MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (0.0)
#define USER_MOTOR_Rs_Ohm                 (2.26793718)
#define USER_MOTOR_Ls_d_H                 (0.00808008015)
#define USER_MOTOR_Ls_q_H                 (0.00808008015)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.387036026)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (3.82)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (2500.0)
#define USER_MOTOR_INERTIA_Kgm2           (3.10002e-05)

#define USER_MOTOR_FREQ_MIN_HZ             (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (400.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (30.0)          // Volt
#define USER_MOTOR_VOLT_MAX_V             (200.0)         // Volt

#elif (USER_MOTOR == my_motor_1)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.169607401)
#define USER_MOTOR_Ls_d_H                 (0.00079099607)
#define USER_MOTOR_Ls_q_H                 (0.00079099607)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.309579641)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (5.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.5)
#define USER_MOTOR_MAX_CURRENT_A          (42.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (1000)
#define USER_MOTOR_INERTIA_Kgm2           (7.06154e-06)

#define USER_MOTOR_RATED_VOLTAGE_V        (300.0)
#define USER_MOTOR_RATED_SPEED_KRPM       (8.6)

#define USER_MOTOR_FREQ_MIN_HZ            (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (800.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (20.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (400.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (300.0)          // Volt

#define USER_MOTOR_RATED_VOLTAGE_V        (400.0)
#define USER_MOTOR_RATED_SPEED_KRPM       (11.0)

#define USER_MOTOR_FREQ_MIN_HZ            (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (800.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (20.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (800.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (500.0)          // Volt

#elif (USER_MOTOR == Estun_EMJ_04APB22_B)
#define USER_MOTOR_TYPE                    MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (0.0)

// HV Kit with external OPA
#define USER_MOTOR_Rs_Ohm                 (2.98774099)
#define USER_MOTOR_Ls_d_H                 (0.008926632)
#define USER_MOTOR_Ls_q_H                 (0.008926632)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.445965141)

#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (3.82)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (2500.0)
#define USER_MOTOR_INERTIA_Kgm2           (3.10002e-05)

#define USER_MOTOR_FREQ_MIN_HZ             (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (400.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (20.0)          // Volt
#define USER_MOTOR_VOLT_MAX_V             (200.0)         // Volt

#elif (USER_MOTOR == Marathon_N56PNRA10102)
#define USER_MOTOR_TYPE                    MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (3)
#define USER_MOTOR_Rr_Ohm                 (0.0)

// HV Kit with external OPA
#define USER_MOTOR_Rs_Ohm                 (2.17462158)
#define USER_MOTOR_Ls_H                   (0.0269199051)
#define USER_MOTOR_Ls_d_H                 (0.0218)
#define USER_MOTOR_Ls_q_H                 (0.0505)
#define USER_MOTOR_RATED_FLUX_VpHz        (2.65306973)

#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (3.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-2.0)
#define USER_MOTOR_MAX_CURRENT_A          (6.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (2500.0)
#define USER_MOTOR_INERTIA_Kgm2           (2.6981376e-03)

#define USER_MOTOR_FREQ_MIN_HZ            (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (400.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (20.0)          // Volt
#define USER_MOTOR_VOLT_MAX_V             (200.0)         // Volt

#elif (USER_MOTOR == Anaheim_BLWS235D_160V)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (2)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (5.3205986)
#define USER_MOTOR_Ls_d_H                 (0.0221263766)
#define USER_MOTOR_Ls_q_H                 (0.0221263766)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.557901621)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.5)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (5.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)
#define USER_MOTOR_INERTIA_Kgm2           (3.99683e-05)     // 0.00566 oz-in-sec2

#define USER_MOTOR_FREQ_MIN_HZ            (5.0)             // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (300.0)           // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)            // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)           // Hz
#define USER_MOTOR_VOLT_MIN_V             (30.0)            // Volt
#define USER_MOTOR_VOLT_MAX_V             (200.0)           // Volt

#elif (USER_MOTOR == Teknic_M2310PLN04K)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.381334811)
#define USER_MOTOR_Ls_d_H                 (0.000169791776)
#define USER_MOTOR_Ls_q_H                 (0.000169791776)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.0398557819)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (2.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.5)
#define USER_MOTOR_MAX_CURRENT_A          (6.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (40.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (1000)
#define USER_MOTOR_INERTIA_Kgm2           (7.06154e-06)

#define USER_MOTOR_RATED_VOLTAGE_V        (24.0)
#define USER_MOTOR_RATED_SPEED_KRPM       (3.0)

#define USER_MOTOR_FREQ_MIN_HZ            (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (600.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (20.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (400.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (24.0)          // Volt

#elif (USER_MOTOR == Anaheim_BLY172S_24V)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.4)
#define USER_MOTOR_Ls_d_H                 (0.0007190173)
#define USER_MOTOR_Ls_q_H                 (0.0007190173)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.0327013217)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.5)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.5)
#define USER_MOTOR_MAX_CURRENT_A          (5.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)
#define USER_MOTOR_INERTIA_Kgm2           (3.96154e-06)

#define USER_MOTOR_FREQ_MIN_HZ             (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (300.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (400.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (24.0)          // Volt

#elif (USER_MOTOR == Anaheim_BLY341S_48V)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.463800967)
#define USER_MOTOR_Ls_d_H                 (0.00114538975)
#define USER_MOTOR_Ls_q_H                 (0.00114538975)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.0978558362)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (2.5)
#define USER_MOTOR_IND_EST_CURRENT_A      (-2.0)
#define USER_MOTOR_MAX_CURRENT_A          (20.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#define USER_MOTOR_FREQ_MIN_HZ             (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (300.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (24.0)          // Volt

#elif (USER_MOTOR == Anaheim_BLY341S_24V)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.4110007)
#define USER_MOTOR_Ls_d_H                 (0.0007092811)
#define USER_MOTOR_Ls_q_H                 (0.0007092811)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.03279636)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.5)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (10.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#define USER_MOTOR_FREQ_MIN_HZ             (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (300.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (24.0)          // Volt

#elif (USER_MOTOR == Traxxas_Velineon_380)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (1)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (TBD)
#define USER_MOTOR_Ls_d_H                 (TBD)
#define USER_MOTOR_Ls_q_H                 (TBD)
#define USER_MOTOR_RATED_FLUX_VpHz        (TBD)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (4.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-0.5)
#define USER_MOTOR_MAX_CURRENT_A          (10.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == Traxxas_Velineon_3500)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (1)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.01822988)
#define USER_MOTOR_Ls_d_H                 (8.322238e-06)
#define USER_MOTOR_Ls_q_H                 (8.322238e-06)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.010249538)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (2.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-2.0)
#define USER_MOTOR_MAX_CURRENT_A          (5.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (40.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == Pacific_Scientific)
#define USER_MOTOR_TYPE                    MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (0.0)
#define USER_MOTOR_Rs_Ohm                 (0.9428042)
#define USER_MOTOR_Ls_d_H                 (0.002196057)
#define USER_MOTOR_Ls_q_H                 (0.002196057)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.3481677)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (8.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == Regal_Beloit_5SME39DL0756)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (3)
#define USER_MOTOR_Rr_Ohm                 (0.0)
#define USER_MOTOR_Rs_Ohm                 (4.581007)
#define USER_MOTOR_Ls_d_H                 (0.03727356)
#define USER_MOTOR_Ls_q_H                 (0.03727356)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.6589699)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (2.6)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (20.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == AutoRadiatorFan)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (4)
#define USER_MOTOR_Rr_Ohm                 (0.0)
#define USER_MOTOR_Rs_Ohm                 (0.0)
#define USER_MOTOR_Ls_d_H                 (0.0)
#define USER_MOTOR_Ls_q_H                 (0.0)
#define USER_MOTOR_RATED_FLUX_VpHz        (TBD)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (10.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (50.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == philips_respirator)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (1)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.1690236)
#define USER_MOTOR_Ls_d_H                 (0.0001557156)
#define USER_MOTOR_Ls_q_H                 (0.0001557156)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.011538831)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-1.0)
#define USER_MOTOR_MAX_CURRENT_A          (5.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (40.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == tekin_redline_4600KV)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_PM
#define USER_MOTOR_NUM_POLE_PAIRS         (2)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (0.0181193)
#define USER_MOTOR_Ls_d_H                 (8.180002e-06)
#define USER_MOTOR_Ls_q_H                 (8.180002e-06)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.0041173688)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (3.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (-3.0)
#define USER_MOTOR_MAX_CURRENT_A          (5.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (60.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == Marathon_5K33GN2A)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_INDUCTION
#define USER_MOTOR_NUM_POLE_PAIRS         (2)
#define USER_MOTOR_Rr_Ohm                 (5.508003)
#define USER_MOTOR_Rs_Ohm                 (10.71121)
#define USER_MOTOR_Ls_d_H                 (0.05296588)
#define USER_MOTOR_Ls_q_H                 (0.05296588)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.8165*220.0/60.0)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (1.378)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (NULL)
#define USER_MOTOR_MAX_CURRENT_A          (3.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (5.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)
#define USER_MOTOR_INERTIA_Kgm2           (2.12002e-05)

#define USER_MOTOR_FREQ_MIN_HZ            (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (400.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (200.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (20.0)          // Volt
#define USER_MOTOR_VOLT_MAX_V             (200.0)         // Volt


#elif (USER_MOTOR == Marathon_56H17T2011A)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_INDUCTION
#define USER_MOTOR_NUM_POLE_PAIRS         (2)
#define USER_MOTOR_Rr_Ohm                 (5.159403)
#define USER_MOTOR_Rs_Ohm                 (7.924815)
#define USER_MOTOR_Ls_d_H                 (0.03904648)
#define USER_MOTOR_Ls_q_H                 (0.03904648)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.8165*220.0/60.0)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (0.9941965)
#define USER_MOTOR_RES_EST_CURRENT_A      (0.5)
#define USER_MOTOR_IND_EST_CURRENT_A      (NULL)
#define USER_MOTOR_MAX_CURRENT_A          (2.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (5.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == Dayton_3N352C)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_INDUCTION
#define USER_MOTOR_NUM_POLE_PAIRS         (2)
#define USER_MOTOR_Rr_Ohm                 (2.428799)
#define USER_MOTOR_Rs_Ohm                 (2.863202)
#define USER_MOTOR_Ls_d_H                 (0.02391323)
#define USER_MOTOR_Ls_q_H                 (0.02391323)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.8165*230.0/60.0)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (1.0)
#define USER_MOTOR_IND_EST_CURRENT_A      (NULL)
#define USER_MOTOR_MAX_CURRENT_A          (3.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (5.0)
#define USER_MOTOR_NUM_ENC_SLOTS          (NULL)

#elif (USER_MOTOR == my_motor_2)
#define USER_MOTOR_TYPE                   MOTOR_TYPE_INDUCTION
#define USER_MOTOR_NUM_POLE_PAIRS         (2)
#define USER_MOTOR_Rr_Ohm                 (NULL)
#define USER_MOTOR_Rs_Ohm                 (NULL)
#define USER_MOTOR_Ls_d_H                 (NULL)
#define USER_MOTOR_Ls_q_H                 (NULL)
#define USER_MOTOR_RATED_FLUX_VpHz        (0.8165*230.0/60.0)
#define USER_MOTOR_MAGNETIZING_CURRENT_A  (NULL)
#define USER_MOTOR_RES_EST_CURRENT_A      (0.5)
#define USER_MOTOR_IND_EST_CURRENT_A      (NULL)
#define USER_MOTOR_MAX_CURRENT_A          (5.0)
#define USER_MOTOR_FLUX_EXC_FREQ_Hz       (5.0)

// Number of lines on the motor's quadrature encoder
#define USER_MOTOR_NUM_ENC_SLOTS          (1000)

#define USER_MOTOR_FREQ_MIN_HZ             (5.0)           // Hz
#define USER_MOTOR_FREQ_MAX_HZ            (300.0)         // Hz

#define USER_MOTOR_FREQ_LOW_HZ            (10.0)          // Hz
#define USER_MOTOR_FREQ_HIGH_HZ           (400.0)         // Hz
#define USER_MOTOR_VOLT_MIN_V             (4.0)           // Volt
#define USER_MOTOR_VOLT_MAX_V             (24.0)          // Volt

#else
#error No motor type specified
#endif


//! \brief Defines the maximum current slope for Id trajectory
//!
#define USER_MAX_CURRENT_DELTA_A        (USER_MOTOR_RES_EST_CURRENT_A / USER_ISR_FREQ_Hz)


//! \brief Defines the maximum current slope for Id trajectory during power warp mode
//!
#define USER_MAX_CURRENT_DELTA_PW_A    (0.3 * USER_MOTOR_RES_EST_CURRENT_A / USER_ISR_FREQ_Hz)


#ifndef USER_MOTOR
#error Motor type is not defined in user.h
#endif

#ifndef USER_MOTOR_TYPE
#error The motor type is not defined in user.h
#endif

#ifndef USER_MOTOR_NUM_POLE_PAIRS
#error Number of motor pole pairs is not defined in user.h
#endif

#ifndef USER_MOTOR_Rr_Ohm
#error The rotor resistance is not defined in user.h
#endif

#ifndef USER_MOTOR_Rs_Ohm
#error The stator resistance is not defined in user.h
#endif

#ifndef USER_MOTOR_Ls_d_H
#error The direct stator inductance is not defined in user.h
#endif

#ifndef USER_MOTOR_Ls_q_H
#error The quadrature stator inductance is not defined in user.h
#endif

#ifndef USER_MOTOR_RATED_FLUX_VpHz
#error The rated flux of motor is not defined in user.h
#endif

#ifndef USER_MOTOR_MAGNETIZING_CURRENT_A
#error The magnetizing current is not defined in user.h
#endif

#ifndef USER_MOTOR_RES_EST_CURRENT_A
#error The resistance estimation current is not defined in user.h
#endif

#ifndef USER_MOTOR_IND_EST_CURRENT_A
#error The inductance estimation current is not defined in user.h
#endif

#ifndef USER_MOTOR_MAX_CURRENT_A
#error The maximum current is not defined in user.h
#endif

#ifndef USER_MOTOR_FLUX_EXC_FREQ_Hz
#error The flux excitation frequency is not defined in user.h
#endif

#if ((USER_NUM_CURRENT_SENSORS < 2) || (USER_NUM_CURRENT_SENSORS > 3))
#error The number of current sensors must be 2 or 3
#endif

#if (USER_NUM_VOLTAGE_SENSORS != 3)
#error The number of voltage sensors must be 3
#endif


// **************************************************************************
// the typedefs


// **************************************************************************
// the globals


// **************************************************************************
// the functions

//! \brief      Sets the user parameter values
//! \param[in]  pUserParams  The pointer to the user param structure
extern void USER_setParams(USER_Params *pUserParams);


//! \brief      Sets the private user parameter values
//! \param[in]  pUserParams  The pointer to the user param structure
extern void USER_setParams_priv(USER_Params *pUserParams);


//! \brief      Sets the private user parameter values
//! \param[in]  pUserParams  The pointer to the user param structure
extern void cla_USER_setParams_priv(USER_Params *pUserParams);


#ifdef __cplusplus
}
#endif // extern "C"

//@}  // ingroup
#endif // end of USER_H definition

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的,过度调制对电流感应信号非常敏感。 最好在 大多数硬件中将 USER_MAX_VS_MAG_PU 设置为小于0.57。