This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28020:如何缩小示例程序中的代码大小

Guru**** 2513185 points
Other Parts Discussed in Thread: TMS320F28020, TMS320F28021

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1080502/tms320f28020-how-to-reduce-code-size-in-example-programs

部件号:TMS320F28020
“线程”中讨论的其它部件: TMS320F28021测试

大家好,

在为 将需要的几个外围设备中的两个添加代码后,TMS320F28020项目的内存很快就用完了。 该项目是一个由采用 C/C++编写的 ATmega328PB-MU 处理器提供的端口。  Atmega 部件具有32kBytes 闪存,1kByte EEPROM 和2kBytes SRAM,即使所有模块都已实现并正常工作,其内存也不会被外置。

下面是 C2000方案:

I2C 实施:

1.从“资源管理器”下载的“example_2802xI2c_eeproe.c”位字段代码开始

2.在 LaunchPadXL TMS320F2802x 上

3.在 CCS 版本中 10.4.0.00006

4.使用编译器版本 TI v21.6.0LTS

5.我添加了一个开关语句以及少量相关代码, 它有相当多的存储空间。

//###########################################################################
//
// FILE:    Example_2802xI2c_eeprom.c
//
// TITLE:   f2802x I2C EEPROM Example
//
// ASSUMPTIONS:
//
//    This program requires the f2802x header files.
//
//    This program requires an external I2C EEPROM connected to
//    the I2C bus at address 0x50.
//
//    As supplied, this project is configured for "boot to SARAM"
//    operation.  The 2802x Boot Mode table is shown below.
//    For information on configuring the boot mode of an eZdsp,
//    please refer to the documentation included with the eZdsp,
//
//    $Boot_Table
//    While an emulator is connected to your device, the TRSTn pin = 1,
//    which sets the device into EMU_BOOT boot mode. In this mode, the
//    peripheral boot modes are as follows:
//
//      Boot Mode:   EMU_KEY        EMU_BMODE
//                   (0xD00)         (0xD01)
//      ---------------------------------------
//      Wait         !=0x55AA        X
//      I/O          0x55AA          0x0000
//      SCI          0x55AA          0x0001
//      Wait         0x55AA          0x0002
//      Get_Mode     0x55AA          0x0003
//      SPI          0x55AA          0x0004
//      I2C          0x55AA          0x0005
//      OTP          0x55AA          0x0006
//      Wait         0x55AA          0x0007
//      Wait         0x55AA          0x0008
//      SARAM        0x55AA          0x000A   <-- "Boot to SARAM"
//      Flash        0x55AA          0x000B
//      Wait         0x55AA          Other
//
//   Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
//   according to the Boot Mode Table above. Build/Load project,
//   Reset the device, and Run example
//
//   $End_Boot_Table
//
// DESCRIPTION:
//
//    This program will write 1-14 words to EEPROM and read them back.
//    The data written and the EEPROM address written to are contained
//    in the message structure, I2cMsgOut1. The data read back will be
//    contained in the message structure I2cMsgIn1.
//
//    This program will work with the on-board I2C EEPROM supplied on
//    the F2802x eZdsp.
//
//
//###########################################################################
// $TI Release: F2802x Support Library v3.05.00.00 $
// $Release Date: 10-19-2021 $
// $Copyright:
// Copyright (C) 2009-2021 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

//
// Note: I2C Macros used in this example can be found in the
// f2802x_I2C_defines.h file
//

//
// Function Prototypes
//
void   I2CA_Init(void);
uint16_t I2CA_WriteData(struct I2CMSG *msg);
__interrupt void i2c_int1a_isr(void);
void pass(void);
void fail(void);

//
// Defines
//
#define I2C_SLAVE_ADDR        0x50
#define I2C_NUMBYTES          2
#define I2C_EEPROM_HIGH_ADDR  0x00
#define I2C_EEPROM_LOW_ADDR   0x30

//
// Globals
//
struct I2CMSG I2cMsgOut1=
{
    I2C_MSGSTAT_SEND_WITHSTOP,
    I2C_SLAVE_ADDR,
    I2C_NUMBYTES,
    I2C_EEPROM_HIGH_ADDR,
    I2C_EEPROM_LOW_ADDR,

    //
    // Msg Byte 1
    //
    0x12,

    //
    // Msg Byte 2
    //
    0x34
};

struct I2CMSG I2cMsgIn1=
{
    I2C_MSGSTAT_SEND_NOSTOP,
    I2C_SLAVE_ADDR,
    I2C_NUMBYTES,
    I2C_EEPROM_HIGH_ADDR,
    I2C_EEPROM_LOW_ADDR
};

uint16_t				delayCounter		= 0;
volatile unsigned int	volumeCommand[40];
volatile int			redSwitchCurrent	= 0;
volatile int			redSwitchPrevious	= 0;
volatile int			greenSwitchCurrent	= 0;
volatile int			greenSwitchPrevious	= 0;
volatile int			transmitStringFlag	= 0;


//
// Used in interrupts
//
struct I2CMSG *CurrentMsgPtr;               
uint16_t PassCount;
uint16_t FailCount;

volatile uint16_t	idleCounter1;
volatile uint16_t	idleCounter2;
volatile uint16_t	tempByte = 0;

// vv Tim's code vv
//PARSING PORTION
/*****************************************************************************
 *
 *****************************************************************************/
enum Command
{
    NONE, QET, RET, SRC, QRC, QMS, IVI, DVI, SVI, QVI, SRS, QPW, SVO, IVO, DVO, QVO, SLD, SOS
} ;


/*****************************************************************************
 *
 *****************************************************************************/
struct CommandMessage
{

    enum Command cmd;
    short value1;
    short value2;
};
// ^^ Tim's code ^^

void TransmitString(int numBytes);

struct CommandMessage cm;	// This works


//
// Main
//
void main(void)
{
    uint16_t Error;
    uint16_t i;

    //
    // WARNING: Always ensure you call memcpy before running any functions from
    // RAM InitSysCtrl includes a call to a RAM based function and without a 
    // call to memcpy first, the processor will go "into the weeds"
#ifdef _FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif

//    CurrentMsgPtr = &I2cMsgOut1;

    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the f2802x_SysCtrl.c file.
    //
    InitSysCtrl();

    //
    // Step 2. Initialize GPIO:
    // This example function is found in the f2802x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    //
    //InitGpio();
    
    //
    // Setup only the GP I/O only for I2C functionality
    //
    InitI2CGpio();

    //
    // Step 3. Clear all interrupts and initialize PIE vector table:
    // Disable CPU interrupts
    //
    DINT;

    //
    // Initialize PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the f2802x_PieCtrl.c file.
    //
    InitPieCtrl();

    //
    // Disable CPU interrupts and clear all CPU interrupt flags
    //
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in f2802x_DefaultIsr.c.
    // This function is found in f2802x_PieVect.c.
    //
    InitPieVectTable();

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //
    EALLOW;            // This is needed to write to EALLOW protected registers
    PieVectTable.I2CINT1A = &i2c_int1a_isr;
    EDIS;      // This is needed to disable write to EALLOW protected registers

    //
    // Step 4. Initialize all the Device Peripherals
    //
    I2CA_Init();                    // I2C-A only

    //
    // Step 5. User specific code
    //

    //
    // Clear Counters
    //
    PassCount = 0;
    FailCount = 0;

    //
    // Clear incoming message buffer
    //
    for (i = 0; i < (I2C_MAX_BUFFER_SIZE - 2); i++)
    {
//        I2cMsgIn1.MsgBuffer[i] = 0x0000;
    }

    //
    // Enable interrupts required for this example
    //

    //
    // Enable I2C interrupt 1 in the PIE: Group 8 interrupt 1
    //
    PieCtrlRegs.PIEIER8.bit.INTx1 = 1;

    //
    //  Init GPIOs (rdv)
    //

    EALLOW;
    GpioCtrlRegs.GPAMUX1.bit.GPIO4  = 0;    // 0 configures GPIO4 as GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO4   = 0;    // 0 makes it an input
    GpioCtrlRegs.GPAPUD.bit.GPIO4   = 0;    // 0 enables pull-up

    GpioCtrlRegs.GPAMUX1.bit.GPIO5  = 0;    // 0 configures GPIO5 as GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO5   = 0;    // 0 makes it an input
    GpioCtrlRegs.GPAPUD.bit.GPIO5   = 0;    // 0 enables pull-up

    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 0;    // 0 configures GPIO19 as GPIO
    GpioCtrlRegs.GPADIR.bit.GPIO19  = 1;    // 1 makes it an output
    GpioCtrlRegs.GPAPUD.bit.GPIO19  = 0;    // 0 enables pull-up
    EDIS;

//    GpioDataRegs.GPASET.bit.GPIO19 = 1;
    GpioDataRegs.GPACLEAR.bit.GPIO19 = 1;


    //
    // Enable CPU INT8 which is connected to PIE group 8
    //
    IER |= M_INT8;
    EINT;

    //
    // Application loop
    //

    //
    // Temp debug vars
    //

    volumeCommand[0] = 0xfe;
    volumeCommand[1] = 0x51;
    volumeCommand[2] = 0xfe;
    volumeCommand[3] = 0x45;
    volumeCommand[4] = 0x00;

    volumeCommand[21] = 0xfe;
    volumeCommand[22] = 0x45;
    volumeCommand[23] = 0x40;

	cm.cmd	= 0;
	cm.value1 = 0;
	cm.value2 = 0;

    for(;;)
    {

	    if(delayCounter++ > 1)
	    {
		    delayCounter = 0;
		    redSwitchCurrent = GpioDataRegs.GPADAT.bit.GPIO4;	// Get switch states
		    greenSwitchCurrent = GpioDataRegs.GPADAT.bit.GPIO5;

			   if(redSwitchCurrent != redSwitchPrevious)			// Compare to previous state
			   {
				   if(!redSwitchCurrent & redSwitchPrevious){	// If the button change is from a press, not release...

					   transmitStringFlag = 1;

					   cm.cmd++;

					   if(cm.cmd > SOS)						// Increment to next command
					   {
						   cm.cmd = NONE;						// Roll to first command
					   }
				   }
				   redSwitchPrevious = redSwitchCurrent;		// Update previous state to current
			   }

			   if(greenSwitchCurrent != greenSwitchPrevious)			// Compare to previous state
			   {
				   if(!greenSwitchCurrent & greenSwitchPrevious){	// If the button change is from a press, not release...

					   transmitStringFlag = 1;

					   cm.cmd--;

					   if(cm.cmd <= NONE)						// Increment to next command
					   {
						   cm.cmd = SOS;						// Roll to first command
					   }
				   }
				   greenSwitchPrevious = greenSwitchCurrent;		// Update previous state to current
			   }

		   if(transmitStringFlag)
		   {
			   switch(cm.cmd)
			   {
				   case NONE:	// 0
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "     NONE       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case QET:	// 1
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      QET       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case RET:	// 2
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      RET       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case SRC:	// 3
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      SRC       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case QRC:	// 4
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      QRC       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case QMS:	// 5
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      QMS       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case IVI:	// 6
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      IVI       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case DVI:	// 7
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      DVI       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case SVI:	// 8
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      SVI       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case QVI:	// 9
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      QVI       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case SRS:	// 10
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      SRS       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case QPW:	// 11
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      QPW       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case SVO:	// 12
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      SVO       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case IVO:	// 13
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      IVO       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case DVO:	// 14
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      DVO       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case QVO:	// 15
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      QVO       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case SLD:	// 16
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      SLD       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   case SOS:	// 17
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "      SOS       ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"**Bottom  line**.  ");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
				   default:	// Anything else
				   {
					   short numBytes = 40;
					   strcpy(volumeCommand+5, "    Command     ");
									   //   1234567890123456
					   strcpy(volumeCommand+24,"was out of range");
									   //   1234567890123456
					   volumeCommand[21] = 0xfe;
					   TransmitString(numBytes);
					   transmitStringFlag = 0;
				   }
				   break;
			   }
		   }
	    }
    }
}
//
// I2CA_Init -
//
void
I2CA_Init(void)
{
    // Initialize I2C
    I2caRegs.I2CMDR.bit.IRS         = 0;	// SEE BELOW - Put I2C module in reset while making changes


    //
    // Own Address Register
    //								// Bit   15: READ ONLY - Reserved
    I2caRegs.I2COAR                 = 0x26;	// Own address = 0x28

    	    	    	    	    	    	    	    	    	// Bits 7-15: Reserved
    //
    // I2C Interrupt Enable Register
    //								// Bits 7-15: READ ONLY - Reserved
    I2caRegs.I2CIER.bit.AAS         = 0;	// Bit	 6: 1 = Addressed as slave interrupt request enabled
    I2caRegs.I2CIER.bit.SCD         = 0;	// Bit     5: 1 = Stop condition detected interrupt request enabled
    I2caRegs.I2CIER.bit.XRDY        = 0;	// Bit     4: 1 = Transmit data ready interrupt request disabled
    I2caRegs.I2CIER.bit.RRDY        = 0;	// Bit     3: 1 = W1C - Receive data ready interrupt request enabled
    I2caRegs.I2CIER.bit.ARDY        = 0;	// Bit     2: 1 = Master Only - Register access ready interrupt request enabled
    I2caRegs.I2CIER.bit.NACK        = 0;	// Bit     1: 0 = W1C - No-ack interrupt request disabled
    I2caRegs.I2CIER.bit.ARBL        = 0;	// Bit     0: 0 = W1C - Arbitration lost interrupt request disabled


    //
    // I2C Status Register
    //								// Bit   15: READ ONLY - Reserved
    I2caRegs.I2CSTR.bit.SDIR        = 1;	// Bit   14: W1C - Slave direction bit 0 = not addressed as slave transmitter
    I2caRegs.I2CSTR.bit.NACKSNT     = 1;	// Bit   13: W1C - NACK sent bit 0 = NACK not sent
    I2caRegs.I2CSTR.bit.BB          = 0;	// Bit   12: Bus Busy bit 0 = bus free
    I2caRegs.I2CSTR.bit.RSFULL      = 0;	// Bit   11: 1 = receive shift register overrun condition detected
    I2caRegs.I2CSTR.bit.XSMT        = 0;	// Bit   10: 0 = transmit shift register underflow detected (empty)
    I2caRegs.I2CSTR.bit.AAS         = 0;	// Bit    9: 1 = I2C module recognized its own slave address
    I2caRegs.I2CSTR.bit.AD0         = 0;	// Bit    8: 1 = address of all zeros (general call) was detected
    	    	    	    	    	    	    	    	    	// Bits 6-7: READ ONLY - Reserved
    I2caRegs.I2CSTR.bit.SCD         = 1;	// Bit    5: W1C - 1 = stop condition was detected
    I2caRegs.I2CSTR.bit.XRDY        = 1;	// Bit    4: 1 = Ready for more transmit data to go in I2CDXR
    I2caRegs.I2CSTR.bit.RRDY        = 1;	// Bit    3: W1C - Receive data ready int flag 1 = data is in I2CDRR
    I2caRegs.I2CSTR.bit.ARDY        = 1;	// Bit    2: Master Only - Register access ready int flag
    I2caRegs.I2CSTR.bit.NACK        = 1;	// Bit    1: W1C - 1 = NACK received
    I2caRegs.I2CSTR.bit.ARBL        = 1;	// Bit    0: W1C - 1 = arbitration lost


    //
    // I2C Clock Prescale Register
    //
    // Setup I2C data rate
    I2caRegs.I2CPSC.bit.IPSC        = 5;	// Prescaler value 60mHz SYSCLK / 6 = 10mHz (5+1=6)


    //
    // I2C Clock high-time and low-time Registers
    //
    // 10mHz / 200 = 50kHz for comm's with 2x16 debugging display
    I2caRegs.I2CCLKL                =  129;	// 129 + 5 = 136
    I2caRegs.I2CCLKH                =   61;	//  61 + 5 =  66


    //
    // Data Count Register
    //
    I2caRegs.I2CCNT                 = 1;	// Bits 0-15: Set data count (ignored in RM mode)
									// Is changed to actual number of bytes to transfer when in
									// transmit mode.
    //
    // Slave Address Register
    //   	    	    	    	    	    	    	     // Bits 10-15: READ ONLY - Reserved
    I2caRegs.I2CSAR                 = 0x28;	// Bits   0-9: Address to which data will be transmitted (Master only)


    //
    // I2C Mode Register
    //   	    	    	    	    	    	    	     // Bits 14-15:  READ ONLY - Reserved
    I2caRegs.I2CMDR.bit.NACKMOD     = 0;	// Bit   15: NACK mode
    I2caRegs.I2CMDR.bit.FREE        = 0;	// Bit   14: For debugging: 0 = I2C halts during interrupts
//    I2caRegs.I2CMDR.bit.STT         = 0;	// Bit   13: Master only - Start bit Can't be written when IRS=0
    	    	    	    	    	    	    	    	    	// Bit   12: Reserved
//    I2caRegs.I2CMDR.bit.STP         = 0;	// Bit   11: Master only - Stop bit Can't be written when IRS=0
    I2caRegs.I2CMDR.bit.MST         = 1;	// Bit   10: Remains 0 for slave mode.  1 = Master mode
    I2caRegs.I2CMDR.bit.TRX         = 1;	// Bit    9: 0 = Receive mode, 1 = Transmit mode
    I2caRegs.I2CMDR.bit.XA          = 0;	// Bit    8: 0 = 7 bit address mode
    I2caRegs.I2CMDR.bit.RM          = 1;	// Bit    7: 1 = repeat mode
    I2caRegs.I2CMDR.bit.DLB         = 0;	// Bit    6: 0 = Digital loopback mode disabled
//    I2caRegs.I2CMDR.bit.IRS         = 1;	// Bit    5: I2C module is re-enabled after making changes
    I2caRegs.I2CMDR.bit.STB         = 0;	// Bit    4: Master only - Start Byte mode
    I2caRegs.I2CMDR.bit.FDF         = 0;	// Bit    3: Keep at 0. Free data format mode
    I2caRegs.I2CMDR.bit.BC          = 0;	// Bits 0-2: Set bit count to 8 bits (0 = 8)


    //
    // I2C Extended Mode Register
    //   	    	    	    	    	    	    	     // Bits 1-15: READ ONLY - Reserved
    I2caRegs.I2CEMDR.bit.BCM         = 0;	// Bit     0: Backwards compatibility mode


    //
    // Transmit FIFO Register
    //   	    	    	    	    	    	    	     // Bits 14-15:  READ ONLY - Reserved
    	    	    	    	    	    	    	    	     // Bit 15: Reserved
    I2caRegs.I2CFFTX.bit.I2CFFEN    = 0;	// Bit    14: 1 = Enable transmit & receive FIFOs
    I2caRegs.I2CFFTX.bit.TXFFRST    = 0;	// Bit    13: 1 = Take transmit FIFO out of reset
//    I2caRegs.I2CFFTX.bit.TXFFST     = 0;	// Bits 8-12: READ ONLY - How many bytes are in the transmit FIFO
//    I2caRegs.I2CFFTX.bit.TXFFINT    = 0;	// Bit     7: READ ONLY - 1 = interrupt occurred
    I2caRegs.I2CFFTX.bit.TXFFINTCLR = 1;	// Bit     6: W1C - Clears transmit interrupt flag (do again after irs = 1)
    I2caRegs.I2CFFTX.bit.TXFFIENA   = 0;	// Bit     5: 0 = Disable transmit FIFO interrupt
    I2caRegs.I2CFFTX.bit.TXFFIL     = 0;	// Bits  0-4: Set the transmit FIFO interrupt Threshold


    //
    // Receive FIFO Register
    //   	    	    	   	    	    	    	     // Bits 14-15:  READ ONLY - Reserved
    I2caRegs.I2CFFRX.bit.RXFFRST    = 0;	// Bit     13: 1 = enable receive FIFO operation
//    I2caRegs.I2CFFRX.bit.RXFFST     = 0;	// BitS  8-12: READ ONLY - Bytes in receive FIFO
//    I2caRegs.I2CFFRX.bit.RXFFINT    = 0;	// Bit      7: READ ONLY - Receive interrupt flag 1 = int
    I2caRegs.I2CFFRX.bit.RXFFINTCLR = 1;	// Bit      6: Write 1 to clear receive int flag
    I2caRegs.I2CFFRX.bit.RXFFIENA   = 0;	// Bit      5: 1 = receive interrupt is enabled
    I2caRegs.I2CFFRX.bit.RXFFIL     = 0;	// Bits   0-4: Set the receive FIFO interrupt level


    // Clean up and exit
    I2caRegs.I2CMDR.bit.IRS         = 1;	// SEE ABOVE - I2C module is re-enabled after making changes

    I2caRegs.I2CFFTX.bit.TXFFINTCLR = 1;	// SEE ABOVE - Clears transmit interrupt flag
    I2caRegs.I2CFFRX.bit.RXFFINTCLR = 1;	// SEE ABOVE - Clears receive interrupt flag

    return;
}

//
// Transmit String -
//
void
TransmitString(int numBytes)
{
	uint16_t i;
	uint16_t i2;

	// wait for STOP condition
	while (I2caRegs.I2CMDR.bit.STP != 0); //bus is not occupied

	// generate START condition
	I2caRegs.I2CMDR.bit.STT = 1;// resets once the START condition is issued

	for(i = 0; i < numBytes; i++){
		idleCounter1 = 0;
		while(!I2caRegs.I2CSTR.bit.XRDY)
		{
			if(idleCounter1++ >= 60000)		// 30,000 ~ 12.6ms
										// When the master read happens before data is ready (after the master sends a write)
											// XRDY is never satisfied.  This algorithm senses this condition and after a time
											// (~12.6ms) reads the I2CDRR to clear the I2C bus condition.
											// Extending this delay makes the data transfer more robust, but at the expense of
											// extending the GMS trip response (during this delay).
											//
											//
											// This is to help unstick the bus when too many writes are issued
			{                               // by master w/o reading. It must be long enough to allow master

				idleCounter1 = 0;           // enough time to download bytes normally.
				tempByte = I2caRegs.I2CDRR; // It must be short enough to allow quick end to CPU hogging

				// The following resets I2C xmit buffer in case master doesn't pull all data
				I2caRegs.I2CMDR.bit.IRS         = 0;    // Put I2C module in reset while making changes
				I2caRegs.I2CCNT                 = 0;    // Set data count to 0 clears xmit buffer
				I2caRegs.I2CMDR.bit.IRS         = 1;    // I2C module is re-enabled after making changes
			}
		}

	    // wait for XRDY flag to transmit data
//	    while (I2caRegs.I2CSTR.bit.XRDY != 1);//wait for the XRDY (transmit mode ready) bit of the status register, which means that the data transmit register is ready to accept new data.

	    I2caRegs.I2CDXR = volumeCommand[i];  // Loads a value into the data xmit buffer, starting the xmit process

//		I2caRegs.I2CMDR.all = 0x6E20;

	    for(i2=0; i2<2500; i2++)
	    {
			// Do nothing, just wait
	    }
    }

    // snd stop condition here
    I2caRegs.I2CMDR.bit.STP = 1;
/*
    idleCounter2 = 0;
    while(I2caRegs.I2CSTR.bit.BB)
    {
        if(idleCounter2++ >= 1000)    // This is to help unstick the bus when xmit buffer empties
        {
            idleCounter2 = 0;
            I2caRegs.I2CDXR = 0xdb;
        }
    }
*/
    I2caRegs.I2CMDR.all = 0x06a0;	// Resets the I2C mode register
}

uint16_t I2CA_WriteData(struct I2CMSG *msg)
{
	    uint16_t i;
	    uint16_t i2;

    // wait for STOP condition
    while (I2caRegs.I2CMDR.bit.STP != 0); //bus is not occupied

    // generate START condition
    I2caRegs.I2CMDR.bit.STT = 1;// resets once the START condition is issued

    for(i = 0; i < 40; i++){
        idleCounter1 = 0;
        while(!I2caRegs.I2CSTR.bit.XRDY)
        {
            if(idleCounter1++ >= 60000)		// 30,000 ~ 12.6ms
            								// When the master read happens before data is ready (after the master sends a write)
											// XRDY is never satisfied.  This algorithm senses this condition and after a time
											// (~12.6ms) reads the I2CDRR to clear the I2C bus condition.
											// Extending this delay makes the data transfer more robust, but at the expense of
											// extending the GMS trip response (during this delay).
											//
											//
											// This is to help unstick the bus when too many writes are issued
            {                               // by master w/o reading. It must be long enough to allow master

                idleCounter1 = 0;           // enough time to download bytes normally.
                tempByte = I2caRegs.I2CDRR; // It must be short enough to allow quick end to CPU hogging

                // The following resets I2C xmit buffer in case master doesn't pull all data
                I2caRegs.I2CMDR.bit.IRS         = 0;    // Put I2C module in reset while making changes
                I2caRegs.I2CCNT                 = 0;    // Set data count to 0 clears xmit buffer
                I2caRegs.I2CMDR.bit.IRS         = 1;    // I2C module is re-enabled after making changes
            }
        }

	    // wait for XRDY flag to transmit data
//	    while (I2caRegs.I2CSTR.bit.XRDY != 1);//wait for the XRDY (transmit mode ready) bit of the status register, which means that the data transmit register is ready to accept new data.

	    // generate START condition
//	    I2caRegs.I2CMDR.bit.STT = 1;// resets once the START condition is issued

	    I2caRegs.I2CDXR = volumeCommand[i];  // Loads a value into the data xmit buffer, starting the xmit process

//		I2caRegs.I2CMDR.all = 0x6E20;

	    for(i2=0; i2<2500; i2++) {
			// Do nothing, just wait
	    }
    }

    // snd stop condition here
    I2caRegs.I2CMDR.bit.STP = 1;

    idleCounter2 = 0;
    while(I2caRegs.I2CSTR.bit.BB)
    {
        if(idleCounter2++ >= 1000)    // This is to help unstick the bus when xmit buffer empties
        {
            idleCounter2 = 0;
            I2caRegs.I2CDXR = 0xdb;
        }
    }

    I2caRegs.I2CMDR.all = 0x06a0;	// Resets the I2C mode register


    return I2C_SUCCESS;
}

//
// i2c_int1a_isr - I2C-A
//
__interrupt void
i2c_int1a_isr(void)
{
	    uint16_t IntSource, i;

	    //
	    // Read interrupt source
	    //
	    IntSource = I2caRegs.I2CISRC.all;

	    //
	    // Interrupt source = stop condition detected
	    //
	    if(IntSource == I2C_SCD_ISRC)
	    {
	        //
	        // If completed message was writing data, reset msg to inactive state
	        //
	        if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_WRITE_BUSY)
	        {
	            CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE;
	        }
	        else
	        {
	            //
	            // If a message receives a NACK during the address setup portion
	            // of the EEPROM read, the code further below included in the
	            // register access ready interrupt source code will generate a stop
	            // condition. After the stop condition is received (here), set the
	            // message status to try again. User may want to limit the number
	            // of retries before generating an error.
	            //
	            if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
	            {
	                CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_SEND_NOSTOP;
	            }

	            //
	            // If completed message was reading EEPROM data, reset msg to
	            // inactive state and read data from FIFO.
	            //
	            else if (CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_READ_BUSY)
	            {
	                CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_INACTIVE;
	                for(i=0; i < I2C_NUMBYTES; i++)
	                {
	                    CurrentMsgPtr->MsgBuffer[i] = I2caRegs.I2CDRR;
	                }

	                //
	                // Check received data
	                //
	                for(i=0; i < I2C_NUMBYTES; i++)
	                {
	                    if(I2cMsgIn1.MsgBuffer[i] == I2cMsgOut1.MsgBuffer[i])
	                    {
	                        PassCount++;
	                    }
	                    else
	                    {
	                        FailCount++;
	                    }
	                }

	                if(PassCount == I2C_NUMBYTES)
	                {
	                    pass();
	                }

	                else
	                {
	                    fail();
	                }
	            }
	        }
	    }

	    //
	    // Interrupt source = Register Access Ready
	    // This interrupt is used to determine when the EEPROM address setup
	    // portion of the read data communication is complete. Since no stop bit is
	    // commanded, this flag tells us when the message has been sent instead of
	    // the SCD flag. If a NACK is received, clear the NACK bit and command a
	    // stop. Otherwise, move on to the read data portion of the communication.
	    //
	    else if(IntSource == I2C_ARDY_ISRC)
	    {
	        if(I2caRegs.I2CSTR.bit.NACK == 1)
	        {
	            I2caRegs.I2CMDR.bit.STP = 1;
	            I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
	        }
	        else if(CurrentMsgPtr->MsgStatus == I2C_MSGSTAT_SEND_NOSTOP_BUSY)
	        {
	            CurrentMsgPtr->MsgStatus = I2C_MSGSTAT_RESTART;
	        }
	    }

	    else
	    {
	        //
	        // Generate some error due to invalid interrupt source
	        //
	        __asm("   ESTOP0");
	    }

	    //
	    // Enable future I2C (PIE Group 8) interrupts
	    //
	    PieCtrlRegs.PIEACK.all = PIEACK_GROUP8;
}

//
// pass -
//
void
pass()
{
    __asm("   ESTOP0");
    for(;;);
}

//
// fail -
//
void
fail()
{
    __asm("   ESTOP0");
    for(;;);
}


//
// End of File
//

SCIA 实施:

 1.运行从“资源管理器”下载的“example_2802xScia_FFDLB.c”位字段代码

2.在 LaunchPadXL TMS320F2802x 上

3.在 CCS 版本中 10.4.0.00006

4.使用编译器版本 TI v21.6.0LTS

由于内存不足,我无法让这两个模块一起运行。  我仍需要为以下项目添加功能:

1,ADC

2.GPIO

3.闪存 IO

4.用户界面

问题:

1. Atmega 部件是8位处理器,而28020是32位处理器。  假设8位部分的32 KB 内存中的哪些内容可以在32位部分中容纳32 KB,这是不对的?

2.在保持简单 I2C 和 SCIA 通信的能力的同时,可以消除大量的示例代码吗?  对于 I2C,28020是主数据,从数据不会响应(仅 ACK)。

3.对于64k,我可以切换到 TMS320F28021,但这是否足够?

如果有人能提供帮助,我将不胜感激。

谢谢,
罗宾

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    罗宾,你好。

    我们会将您的查询转发给专家。 请期待在一天内收到回复。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    罗宾,

    您是否可以分享您观察到的 w.r.t 内存分配错误?  

    您使用的编译器版本是什么,为编译器配置的优化级别是什么?

    此致

    西达尔斯

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Siddharth,

    感谢您的回复。

    我正在使用 TI 编译器 21.6.0.LTS 版:

     当前未设置代码优化:

    下面是编译错误的图像:

    下面是内存分配:

    作为临时解决方案,我将堆栈的默认值从512降至272。  这允许我测试代码,但如果我尝试添加任何其他代码,我将遇到另一个错误。  我还有很多代码需要添加,所以我必须严格地剪裁示例代码,以使其适合所有代码。  我可以重复使用变量并使用更有效的算法,但我希望只是简单地编写示例代码,以便快速生成有效的固件。

    想法?

    谢谢,
    罗宾

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    不知道为什么我的回复中没有显示图片。  他们又在这里:

    我正在使用 TI 编译器21.6.0.LTS 版:

    当前未设置代码优化:



    下面是编译错误的图像:



    下面是内存分配:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    罗宾,

    从错误消息中, 分配给 RAMM1部分的部分似乎无法装入内存。  

    您可以更新链接程序命令文件,以检查哪些部分分配给 RAMM1并将它们移动到更大的部分。

    您甚至可以通过在链接器命令文件中指定- RAMM0 | RAMM1来分配给两个部分

    此致

    西达尔斯  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Siddharth,

    链接程序命令文件未分配 RAML0的上限0x400字节,因此我将它们分配给了第1页。  然后为以前针对 RAMM1的部分指定 RAML0 | RAMM1。  现在代码构建和运行正常,但我仍需要帮助了解我的代码是否最终适合此部分。

    问题1:

    我的 I2C 需求很简单。  我必须向外设芯片发送 I2C 命令。  速度不重要。  外围设备无法响应(ACK 除外)。  将代码最小化以执行此功能的最佳方法是什么?  我开始使用的示例代码似乎不必要地大。  I2C 通信的简约方法示例是否存在?

    问题2:

    我的串行通信需求也有同样的问题。  我从 SCIA 示例开始,但我希望有一个简单的解决方案。

    问题3:

    我可以将一些代码保留在闪存中,然后从闪存中运行吗?

    我 需要更好地理解如何最佳利用可用内存空间,同时生成的代码将功能减少到最低限度。  您是否有任何建议,或者是否可以指出任何其他有助于我理解这种双重方法的应用说明?

    谢谢,
    罗宾

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    罗宾

    最好是让您的代码从闪存运行,这样可以避免每次开机重置后都必须将代码加载到 RAM 中。  

    为了最大限度地减少代码,一种方法是仅使用代码中所需的 driverlib API。 您可以使用预处理程序指令仅包括这些函数,并重新编译 driverlib 库。  这假设您使用的是基于驱动程序库的方法。

    您可以参考以下链接  

    https://software-dl.ti.com/C2000/docs/optimization_guide/phase3/optimization_levels.html

    此致

    西达尔斯

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    [引用 userid="108005" url="~/support/icros/c2000微控制器-组/CC2000 /f/c2000微控制器-论坛/1080502/tms320f28020 -如何减少代码大小示例程序/4010140#4010140]\n 从闪存运行代码更好,这将避免每次加载 RAM 代码后重置代码。  [/引用]

    根据您的评论,我向链接程序命令文件添加了 flash,并为其分配了.econst。  然后我能够将所有 RAML0重新分配到第0页。  所以,这是有效的,我可以尽可能/必要地将我的新代码扩展到闪存中。

    ~引用 userid="108005" url="~/support/minuters/CC2000微控制器-组/CC2000 /f/C2000 -微控制器-论坛/1080502/tms320f28020 -如何减少代码大小-示例程序/4010140#4010140]要最小化代码,一种方法是仅使用基于代码的80f/vert/example-mexample-mexample-mspaps 的程序。

    我只能找到 I2C 代码的位域示例,所以我不使用 driverlib 方法。  您是否能够使用 driverlib 方法将我指向一些 I2C 示例代码?  我能否在没有示例代码的情况下实施此方法?

    [引用 userid="108005" url="~/support/icros/c2000微控制器-group/c2000 /f/c2000微控制器-forume/1080502/tms320f28020-how-to-reduce-code-size-in-example-programs (示例中的代码大小)/4010140#4010140 ]您可以使用预处理程序指令仅包含这些函数并重新编译库[/driverlib]

    您能扩展到这一点吗?  是否有一份文档演示了预处理程序指令的使用?  此外,如何重新编译 driverlib 库?

    谢谢,
    罗宾

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    罗宾,  

    TMS320F28020 器件的 I2C 似乎没有驱动程序库示例。 您可以继续使用比特字段方法。  

    您可以将代码加载到 Flash 中,也可以使用编译器选项来优化代码。  

    此致

    西达尔斯