主题中讨论的其他部件:DRV8305, MOTORWARE
大家好,
我们的客户有兴趣将DRV8305与 TMS320F2.8027万F配合使用,但是电机驱动器目前不可用。
此致,
卡洛
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我们的客户有兴趣将DRV8305与 TMS320F2.8027万F配合使用,但是电机驱动器目前不可用。他们希望使用非TI电机驱动器,它是否可以与TMS320F2.8027万F配合使用? instaspin FOC实验室模块是否仍可与TMS320F2.8027万F和非TI电机驱动器配合使用
此致,
卡洛
是的,FAST和InstaSPIN-FOC算法与栅极驱动器无关,它们仍然可以使用 TMS320F2.8027万F控制器,只需按照以下步骤更改示例实验,并在运行InsatSPIN实验之前验证硬件板的电流和电压信号。
1.在hal.c中更改PWM和ADC配置,请参阅指南motorware_hal_tutorial.pdf。
C:\ti\motorware\motorware_1_01_00_18\docs\tutorials
2.根据user.h中的硬件板设置正确的参数
#define user_IQ_full标度电压V (xx)
#define user_voltage_filter_pole_Hz (xx)
#define user_ADC_FULL比例电压V (xx)
#define user_IQ_full比例当前A (xx)
#define user_ADC_FULL比例电流A (xx)
3.确保hal.h中HAL_readAdcData()中的电流系数符号与电流感应电路匹配。 请参阅InstaSPIN用户指南(SPRUHJ1, https://www.ti.com/lit/spruhj1)中的5.2 2电流反馈极性一章,设置电流比例因子的符号。
静态内联void HAL_readAdcData (HAL_Handle Handle,HAL_AdcData_t *pAdcData)
{
_IQ Current_SF =(+/-) HAL_getCurrentScaleFactor (句柄);
}
4.遵循instaSPIN实验指南使用lab01b和lab01c来验证您自己的硬件 ,因为您没有使用TI EVM套件,然后运行后续实验。
5.使用lab02b或lab02c并调整下面的识别变量参数以识别电动机参数,如果电流和电压感应信号经过验证且正常,则使用已识别的参数运行电动机。
#define user_motor_RES_EST_current (1.0) // A - 电机额定电流的10 30 %
#define user_motor_IND_EST_current (-MOTOR) 1.0 // A - 电动机额定电流的10 30 % , 刚好足以启用旋转
#define user_motor_MAX_current (5.0) // A - 30~150 % of rated current of the motor
#define user_motor_fluence_EST_FREQ_Hz (40.0) // Hz - 10~马达的30 % 额定频率