This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-F2.8377万S:选择微控制器

Guru**** 2929630 points

Other Parts Discussed in Thread: ADS5560, DAC7760

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/573812/launchxl-f28377s-selecting-a-microcontroller

部件号:LAUNCHXL-F2.8377万S

我有一个Launchxl-F2.8377万S,但它似乎不适合我的应用,我不知道哪个微控制器适合此应用? 在C2000系列中找到一个并不容易。

应用程序:

阻抗测量

输入硅:正弦波10MHz。 Launchpad上ADC的采集率和SNR不符合此要求,因此需要ADC,如ADS5560。

输出信号:0-10V和+/-10V。 需要双极输出DAC,例如DAC7760。

PWM,编码器在此应用中不需要。