This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHLL-F2.8027万F:是否有可用的GPIO引脚可用作ADC引脚?

Guru**** 2609165 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/572769/launchxl-f28027f-is-there-available-gpio-pin-that-can-be-muxed-as-an-adc-pin

部件号:LAUNCHTXL-F2.8027万F
主题中讨论的其他部件: BOOSTXL-DRV8305EVM

您好,

我有Launchxl-F2.8027万F和bootxl-drv8305evm,我想获取GPIO (例如29)并将其配置为ADCpin,但我看不到它可以配置为一个。

我看到有39个GPIO,但在gpio.h中看不到ADC选项。 有没有? 谢谢Asha