请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TMS320F2.8377万D 工具/软件:Code Composer Studio
有人能告诉我哪里可以买到???? 要使用ePWM1使ePWM4对称? 我应该在这里放什么???? ?
????.SYNCET.Bit.EPWM4SYNCIN=0;//000: 已选择EPWM1SYNCOUT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Code Composer Studio
有人能告诉我哪里可以买到???? 要使用ePWM1使ePWM4对称? 我应该在这里放什么???? ?
????.SYNCET.Bit.EPWM4SYNCIN=0;//000: 已选择EPWM1SYNCOUT
Hey Hongmei,
每个ePWM都可以使用进入它的同步信号,并且可以从多个源传递同步信号:
请注意,ePWM模块也可以通过信号,因此,如果您想要同步ePWM1和ePMW3,您可以执行如下操作: