This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F2.8377万D:我有关于2.8377万的一些问题

Guru**** 2585275 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/654397/tms320f28377d-i-have-some-questions-about-28377

部件号:TMS320F2.8377万D
主题中讨论的其他部件:TMS320F2.8377万S

您好,

   我对    TMS320F2.8377万S/D 的性能进行了评估, 现在我有一些如下问题:

1.您对ADC的外部参考是否有任何特定要求?
2. 2.8377万D可以挂起多少SDRAM,DMA支持的最大速率是多少?
3,您是否具有双核双端口RAM演示?
4,是否有用于2.8377万D的引导加载程序演示?
5. 2.8377万输出PWM波形的最大频率是多少? 载波频率是多少?

非常感谢!