This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMDSCNCD28.0039万C:MCAN中断源设置和触发器。(无法继续接收其他CanFD命令)

Guru**** 2989100 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1097162/tmdscncd280039c-mcan-interrupt-source-setting-and-trigger-cannot-continue-to-receive-other-canfd-commands

部件号:TMDSCNCD28.0039万C

尊敬的专家:

我目前正在尝试使用28.0039万C构建CAN FD的功能。
我的想法是使用RF0N (Rx FIFO 0 New Message)触发中断,读取中断1中的RAM FIFO数据。

问题在于,发出外部CAFD命令时,接收中断成功,但中断只执行一次,并且不能继续接收其它CAFD命令。

由于可以接收第一个中断的数据,因此可以确认我的硬件和中断设置没有问题。

问题可能出在某些固件设置或缺少某些项,我已经整理了一些基本设置,您能帮我确定我的设置是否有任何问题吗?

总体方案 如下

//#############################################################################
//
// FILE:   mcan_ex4_receive.c
//
// TITLE:  MCAN receive using Rx Buffer
//
//! \addtogroup driver_example_c28x_list
//! <h1> MCAN receive using Rx Buffer </h1>
//!
//! This example demonstrates the MCAN receive function. Communication is done
//! between two CAN nodes. The transmitting node could be another MCU or a
//! CAN bus analysis tool capable of transmitting CAN FD frames. The transmit
//! and receive pins of the MCAN module should be connected to a CAN
//! transceiver. Nominal Bit Rate of 500 kbps & Data bit rate of 1 Mbps is used
//!
//! Only Standard frame with message ID 0x4 is received.
//!
//! If another C2000 MCU is used as the transmitter, mcan_ex3_transmit.c can be
//! run on it for the transmit function.
//!
//! \b Hardware \b Required \n
//!  - A C2000 board with CAN transceiver
//!
//! \b External \b Connections \n
//!   Both nodes should communicate through CAN FD capable transceivers.
//!
//!  - MCAN is on DEVICE_GPIO_PIN_CANRXA (MCANRXA)
//!  - and DEVICE_GPIO_PIN_CANTXA (MCANTXA)
//!
//! \b Watch \b Variables \n
//!  - rxMsg
//!
//

//
// Include Files
//
#include "driverlib.h"
#include "device.h"
#include "inc/stw_types.h"
#include "inc/stw_dataTypes.h"
#include <stdint.h>
#include "inc/hw_types_mcan.h"
#include "mcan.h"
#include "debug.h"
#include "interrupt.h"
//
// Defines.
//
#define NUM_OF_MSG                    (1U)
#define MCAN_STD_ID_FILT_START_ADDR     (0x0U)
#define MCAN_STD_ID_FILTER_NUM          (1U)
#define MCAN_EXT_ID_FILT_START_ADDR     (0x14U)
#define MCAN_EXT_ID_FILTER_NUM          (1U)
#define MCAN_TX_BUFF_START_ADDR         (0x80U)
#define MCAN_TX_BUFF_SIZE               (10U)
#define MCAN_FIFO_1_START_ADDR          (0xc0U)
#define MCAN_FIFO_1_NUM                 (10U)
#define MCAN_TX_EVENT_START_ADDR        (0x100U)
#define MCAN_TX_EVENT_SIZE              (10U)
#define MCAN_EXT_ID_AND_MASK            (0x1FFFFFFFU)
#define MCAN_RX_BUFF_START_ADDR         (948U)
#define MCAN_FIFO_0_START_ADDR          (548U)
#define MCAN_FIFO_0_NUM                 (5U)
#define MCAN_MSG_INT                    (0x81200)


#define MCAN0_BASE MCAN_MSG_RAM_BASE
#define INT_MCANSS0 INT_MCAN_0
#define INT_MCANSS1 INT_MCAN_1

//
// Global Variables.
//
volatile uint32_t isrIntr0Flag = 1U;
volatile uint32_t isrIntr1Flag = 1U;
volatile uint16_t monEn = 0x0;
volatile unsigned long msgCount = 0;
int32_t     error = 0;
MCAN_RxBufElement rxMsg[NUM_OF_MSG], rxMsg1;
int32_t loopCnt = 0U;
int16_t UWSeanflag=0;
int16_t UWdataclear=0;
int16_t int0,int1;

//
// Function Prototype.
//
static void MCANConfig(void);
static void MCANIntrConfig(void);
__interrupt void MCANIntr0ISR(void);
__interrupt void MCANIntr1ISR(void);

void main()
{
    int i = 0;
    volatile uint32_t mode = 0U;
    uint32_t dataBytes = 64;
    MCAN_RxNewDataStatus newData;
    newData.statusLow = 0;

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Initialize GPIO and unlock the GPIO configuration registers
    //
    Device_initGPIO();

    //
    // Configure the divisor for the MCAN bit-clock
    //
    SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_2);
    MCANIntrConfig();

    //
    // Configure GPIO pins for MCANTX/MCANRX operation
    //
    GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANRXA);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANTXA);

    //
    // Initialize message to receive
    //
    rxMsg[loopCnt].id = 0U;
    rxMsg[loopCnt].rtr = 0U;
    rxMsg[loopCnt].xtd = 1U;
    rxMsg[loopCnt].esi = 0U;
    rxMsg[loopCnt].rxts = 0U;   // Rx Timestamp
    rxMsg[loopCnt].dlc = 0U;
    rxMsg[loopCnt].brs = 1U;
    rxMsg[loopCnt].fdf = 1U;
    rxMsg[loopCnt].fidx = 0U;   // Filter Index
                                // (of matching Rx acceptance filter element)
    rxMsg[loopCnt].anmf = 0U;   // Accepted Non-matching Frame

    for(i = 0; i < dataBytes; i++)  // Initialize receive buffer to 0
    {
        rxMsg[loopCnt].data[i]  = 0;
    }
    //
    // Configure the MCAN Module.
    //
    MCANConfig();
    //
    // Enable Interrupts.
    //
    MCAN_enableIntr(MCAN0_BASE, MCAN_INTR_MASK_ALL, 1U);
    //MCAN_enableIntr(MCAN0_BASE, MCAN_INTR_SRC_RES_ADDR_ACCESS|
                   //MCAN_INTR_SRC_TIMESTAMP_WRAPAROUND,0);
    //
    // Select Interrupt Line.
    //
    MCAN_selectIntrLine(MCAN0_BASE, MCAN_INTR_MASK_ALL, MCAN_INTR_LINE_NUM_1);

    //
    // Enable Interrupt Line.
    //
    MCAN_enableIntrLine(MCAN0_BASE, MCAN_INTR_LINE_NUM_1, 1U);
    MCAN_getNewDataStatus(MCAN0_BASE, &newData);

}

static void MCANConfig(void)
{
    MCAN_InitParams initParams;
    MCAN_MsgRAMConfigParams    msgRAMConfigParams;
    MCAN_ExtMsgIDFilterElement extFiltelem;
    MCAN_BitTimingParams       bitTimes;

    //
    // Configure MCAN initialization parameters
    //
    initParams.fdMode            = 0x1U; // FD operation enabled.
    initParams.brsEnable         = 0x1U; // Bit rate switching enabled

    //
    // Initialize Message RAM Sections Configuration Parameters
    //
    msgRAMConfigParams.flesa                = MCAN_STD_ID_FILT_START_ADDR;
    msgRAMConfigParams.lse                  = MCAN_STD_ID_FILTER_NUM;
    msgRAMConfigParams.flesa                = MCAN_EXT_ID_FILT_START_ADDR;
    msgRAMConfigParams.lse                  = MCAN_EXT_ID_FILTER_NUM;
    msgRAMConfigParams.txStartAddr          = MCAN_TX_BUFF_START_ADDR;
    msgRAMConfigParams.txBufNum             = MCAN_TX_BUFF_SIZE;
    msgRAMConfigParams.txFIFOSize           = 0U;
    msgRAMConfigParams.txBufMode            = 0U;
    msgRAMConfigParams.txBufElemSize        = MCAN_ELEM_SIZE_64BYTES;
    msgRAMConfigParams.txEventFIFOStartAddr = MCAN_TX_EVENT_START_ADDR;
    msgRAMConfigParams.txEventFIFOSize      = MCAN_TX_BUFF_SIZE;
    msgRAMConfigParams.txEventFIFOWaterMark = 3U;
    msgRAMConfigParams.rxFIFO0startAddr     = MCAN_FIFO_0_START_ADDR;
    msgRAMConfigParams.rxFIFO0size          = MCAN_FIFO_0_NUM;
    msgRAMConfigParams.rxFIFO0waterMark     = 3U;
    msgRAMConfigParams.rxFIFO0OpMode        = 0U;
    msgRAMConfigParams.rxFIFO1startAddr     = MCAN_FIFO_1_START_ADDR;
    msgRAMConfigParams.rxFIFO1size          = MCAN_FIFO_1_NUM;
    msgRAMConfigParams.rxFIFO1waterMark     = 3U;
    msgRAMConfigParams.rxFIFO1OpMode        = 0U;
    msgRAMConfigParams.rxBufStartAddr       = MCAN_RX_BUFF_START_ADDR;
    msgRAMConfigParams.rxBufElemSize        = MCAN_ELEM_SIZE_64BYTES;
    msgRAMConfigParams.rxFIFO0ElemSize      = MCAN_ELEM_SIZE_64BYTES;
    msgRAMConfigParams.rxFIFO1ElemSize      = MCAN_ELEM_SIZE_64BYTES;

    extFiltelem.efid1 = 0x18EFB324U;
    extFiltelem.eft   = 0x1U;
    extFiltelem.efec  = 0x1U;
    //
    // Initialize bit timings.
    //
    bitTimes.nomRatePrescalar   = 0x7U; // Nominal Baud Rate Pre-scaler
    bitTimes.nomTimeSeg1        = 0x9U; // Nominal Time segment before SP
    bitTimes.nomTimeSeg2        = 0x3U; // Nominal Time segment after SP
    bitTimes.nomSynchJumpWidth  = 0x4U; // Nominal SJW
    bitTimes.dataRatePrescalar  = 0x0U; // Data Baud Rate Pre-scaler
    bitTimes.dataTimeSeg1       = 0x9U; // Data Time segment before SP
    bitTimes.dataTimeSeg2       = 0x0U; // Data Time segment after SP
    bitTimes.dataSynchJumpWidth = 0x4U; // Data SJW

    //
    // Wait for memory initialization to happen.
    //
    while(FALSE == MCAN_isMemInitDone(MCAN0_BASE))
    {
    }

    //
    // Put MCAN in SW initialization mode.
    //
    MCAN_setOpMode(MCAN0_BASE, MCAN_OPERATION_MODE_SW_INIT);

    //
    // Wait till MCAN is not initialized.
    //
    while (MCAN_OPERATION_MODE_SW_INIT != MCAN_getOpMode(MCAN0_BASE))
    {}

    //
    // Initialize MCAN module.
    //
    MCAN_init(MCAN0_BASE, &initParams);

    //
    // Configure Bit timings.
    //
    MCAN_setBitTime(MCAN0_BASE, &bitTimes);

    //
    // Configure Message RAM Sections
    //
    MCAN_msgRAMConfig(MCAN0_BASE, &msgRAMConfigParams);

    //
    // Configure Standard ID filter element
    //
    //MCAN_addStdMsgIDFilter(MCAN0_BASE, 0U, &stdFiltelem);
    MCAN_addExtMsgIDFilter(MCAN0_BASE, 0U, &extFiltelem);

    //
    // Take MCAN out of the SW initialization mode
    //
    MCAN_setOpMode(MCAN0_BASE, MCAN_OPERATION_MODE_NORMAL);

    while (MCAN_OPERATION_MODE_NORMAL != MCAN_getOpMode(MCAN0_BASE))
    {

    }
}
static void MCANIntrConfig(void)
{

    Interrupt_initModule();
    Interrupt_initVectorTable();
    Interrupt_register(INT_MCANSS0,&MCANIntr0ISR);
    Interrupt_enable(INT_MCANSS0);
    Interrupt_register(INT_MCANSS1,&MCANIntr1ISR);
    Interrupt_enable(INT_MCANSS1);
    Interrupt_enableMaster();

}

//
// This is Interrupt Service Routine for MCAN interrupt 0.
//
__interrupt void MCANIntr0ISR(void)
{
    uint32_t intrStatus;
    intrStatus = MCAN_getIntrStatus(MCAN0_BASE);
    int0++;
    if (MCAN_MSG_INT != intrStatus)
    {
        error++;
    }

    //
    // Clear the interrupt Status.
    //
    MCAN_clearIntrStatus(MCAN0_BASE, intrStatus);

    //
    // Update the flag value.
    //
    isrIntr0Flag = 0U;

    //
    // Acknowledge this interrupt located in group 9
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

//
// This is Interrupt Service Routine for MCAN interrupt 1.
//
__interrupt void MCANIntr1ISR(void)
{
    uint32_t intrStatus;
    int1++;
    MCAN_RxNewDataStatus newData;
    intrStatus = MCAN_getIntrStatus(MCAN0_BASE);
    if (MCAN_MSG_INT != intrStatus)
    {
        error++;
    }
    MCAN_getNewDataStatus(MCAN0_BASE, &newData);
    MCAN_readMsgRam(MCAN0_BASE, MCAN_MEM_TYPE_FIFO, 0, MCAN_RX_FIFO_NUM_0, &rxMsg1);
    rxMsg[loopCnt] = rxMsg1;
    MCAN_writeRxFIFOAck(MCAN0_BASE, MCAN_RX_FIFO_NUM_0, 0);
    MCAN_clearNewDataStatus(MCAN0_BASE, &newData);
    //
    // Clear the interrupt Status.
    //
    HW_WR_FIELD32(MCAN0_BASE + MCAN_MCANSS_EOI, MCAN_MCANSS_EOI, 0x1U);
    MCAN_clearIntrStatus(MCAN0_BASE, intrStatus);

    //
    // Update the flag value.
    //
    isrIntr1Flag = 0U;

    //
    // Acknowledge this interrupt located in group 9
    //
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

第150行:设置 启用中断源

行156:选择Interrupt MCAN interrupt 1 (中断MCAN中断1)。

行161: 启用中断MCAN中断1。

第207行 , 第208行和 第209行: 设置ID过滤器并将信息存储在FIFO中。

第327行:读取 从信息RAM收到的信息。

第328行: 将信息从RAM复制到自定义阵列。

行329: 写入Rx FIFO确认。

行335:清除中断状态。

感谢您的帮助!!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Sean,  

    我们正在审查您的查询,我们将很快回复您。

    谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Sean,  

    看第150行

        //
        // Enable Interrupts.
        //
        MCAN_enableIntr(MCAN0_BASE, MCAN_INTR_MASK_ALL, 1U);      <<<<<<<<--------

    设置中断源时,您已选择了MCAL_INTR_MASK_ALL,这意味着所有可能的中断源都将导致对ISR进行调用。 据我所说,您的问题可能是由于在尚未收到新数据时,ISR由于其他中断源而被调用而引起的。  

    按以下方式替换行:

        //
        // Enable Interrupts.
        //
        MCAN_enableIntr(MCAN0_BASE, MCAN_IR_RF0N_MASK, 1U);

    现在,中断的源将仅在新消息写入Rx FIFO 0时(即您的意图)。

    我的想法是使用RF0N

    请尝试相同的方式并告诉我。

    谢谢。

    [/quote]
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Sahil:

    感谢您的回复,我真的没有考虑其他中断源引起的问题。

    调整后,我可以正常接收消息。 但这里出现了第二个问题,我调整了代码如下:

    //
    // Include Files
    //
    #include "driverlib.h"
    #include "device.h"
    #include "inc/stw_types.h"
    #include "inc/stw_dataTypes.h"
    #include <stdint.h>
    #include "inc/hw_types_mcan.h"
    #include "mcan.h"
    #include "debug.h"
    #include "interrupt.h"
    //
    // Defines.
    //
    #define NUM_OF_MSG                    (1U)
    #define MCAN_EXT_ID_FILT_START_ADDR     (0x14U)
    #define MCAN_EXT_ID_FILTER_NUM          (1U)
    #define MCAN_RX_BUFF_START_ADDR         (948U)
    #define MCAN_MSG_INT                    (0x81200)
    #define MCAN0_BASE MCAN_MSG_RAM_BASE
    #define INT_MCANSS1 INT_MCAN_1
    
    //
    // Global Variables.
    
    volatile uint32_t isrIntr1Flag = 1U;
    volatile unsigned long msgCount = 0;
    int32_t     error = 0;
    int32_t loopCnt = 0U;
    int16_t int1;
    //
    // Function Prototype.
    //
    static void MCANConfig(void);
    static void MCANIntrConfig(void);
    __interrupt void MCANIntr1ISR(void);
    
    MCAN_RxBufElement rxMsg[NUM_OF_MSG], rxMsg1;
    MCAN_RxFIFOStatus    RxFS;
    MCAN_RxNewDataStatus newData;
    void main()
    {
        int i = 0;
        volatile uint32_t mode = 0U;
        uint32_t dataBytes = 64;
        newData.statusLow = 0;
    
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Initialize GPIO and unlock the GPIO configuration registers
        //
        Device_initGPIO();
    
        //
        // Configure the divisor for the MCAN bit-clock
        //
        SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_1);
        MCANIntrConfig();
    
        //
        // Configure GPIO pins for MCANTX/MCANRX operation
        //
        GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANRXA);
        GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANTXA);
        GPIO_setPinConfig(DEVICE_GPIO_CFG_Test1);
        GPIO_setDirectionMode(DEVICE_GPIO_PIN_Test1, GPIO_DIR_MODE_OUT);
    
        //
        // Initialize message to receive
        //
        rxMsg[loopCnt].id = 0U;
        rxMsg[loopCnt].rtr = 0U;
        rxMsg[loopCnt].xtd = 1U;
        rxMsg[loopCnt].esi = 0U;
        rxMsg[loopCnt].rxts = 0U;   // Rx Timestamp
        rxMsg[loopCnt].dlc = 0U;
        rxMsg[loopCnt].brs = 1U;
        rxMsg[loopCnt].fdf = 1U;
        rxMsg[loopCnt].fidx = 0U;   // Filter Index
                                    // (of matching Rx acceptance filter element)
        rxMsg[loopCnt].anmf = 0U;   // Accepted Non-matching Frame
    
        for(i = 0; i < dataBytes; i++)  // Initialize receive buffer to 0
        {
            rxMsg[loopCnt].data[i]  = 0;
        }
        //
        // Configure the MCAN Module.
        //
        MCANConfig();
        //
        //
        // Enable Interrupts.
        //
        MCAN_enableIntr(MCAN0_BASE, MCAN_INTR_MASK_ALL, 0U);
        MCAN_enableIntr(MCAN0_BASE, MCAN_IR_DRX_MASK, 1U);
        // Select Interrupt Line.
        MCAN_selectIntrLine(MCAN0_BASE, MCAN_IR_DRX_MASK, MCAN_INTR_LINE_NUM_1);
        //
        // Enable Interrupt Line.
        //
        MCAN_enableIntrLine(MCAN0_BASE, MCAN_INTR_LINE_NUM_1, 1U);
        MCAN_getNewDataStatus(MCAN0_BASE, &newData);
    
    }
    
    static void MCANConfig(void)
    {
        MCAN_InitParams initParams;
        MCAN_MsgRAMConfigParams    msgRAMConfigParams;
        MCAN_ExtMsgIDFilterElement extFiltelem;
        MCAN_BitTimingParams       bitTimes;
    
        //
        // Configure MCAN initialization parameters
        //
        msgRAMConfigParams.flesa                = MCAN_EXT_ID_FILT_START_ADDR;
        msgRAMConfigParams.lse                  = MCAN_EXT_ID_FILTER_NUM;
        initParams.fdMode            = 0x1U; // FD operation enabled.
        initParams.brsEnable         = 0x1U; // Bit rate switching enabled
    
        //
        // Initialize Message RAM Sections Configuration Parameters
        //
    
        msgRAMConfigParams.rxBufStartAddr       = MCAN_RX_BUFF_START_ADDR;
        msgRAMConfigParams.rxBufElemSize        = MCAN_ELEM_SIZE_64BYTES;
    
        extFiltelem.efid2 = 0U;
        extFiltelem.efid1 = 0x18EFB324U;
        extFiltelem.eft   = 0x1U;
        extFiltelem.efec  = 0x7U;
        //
        // Initialize bit timings.
        //
        bitTimes.nomRatePrescalar   = 0x2U; // Nominal Baud Rate Pre-scaler
        bitTimes.nomTimeSeg1        = 0x3AU; // Nominal Time segment before SP
        bitTimes.nomTimeSeg2        = 0x13U; // Nominal Time segment after SP
        bitTimes.nomSynchJumpWidth  = 0x4U; // Nominal SJW
        bitTimes.dataRatePrescalar  = 0x2U; // Data Baud Rate Pre-scaler
        bitTimes.dataTimeSeg1       = 0x4U; // Data Time segment before SP
        bitTimes.dataTimeSeg2       = 0x1U; // Data Time segment after SP
        bitTimes.dataSynchJumpWidth = 0x4U; // Data SJW
    
        //
        // Put MCAN in SW initialization mode.
        //
        MCAN_setOpMode(MCAN0_BASE, MCAN_OPERATION_MODE_SW_INIT);
    
        //
        // Wait till MCAN is not initialized.
        //
        while (MCAN_OPERATION_MODE_SW_INIT != MCAN_getOpMode(MCAN0_BASE))
        {}
    
        //
        // Initialize MCAN module.
        //
        MCAN_init(MCAN0_BASE, &initParams);
    
        //
        // Configure Bit timings.
        //
        MCAN_setBitTime(MCAN0_BASE, &bitTimes);
    
        //
        // Configure Message RAM Sections
        //
        MCAN_msgRAMConfig(MCAN0_BASE, &msgRAMConfigParams);
    
        //
        // Configure Standard ID filter element
        //
        MCAN_addExtMsgIDFilter(MCAN0_BASE, 0U, &extFiltelem);
    
        //
        // Take MCAN out of the SW initialization mode
        //
        MCAN_setOpMode(MCAN0_BASE, MCAN_OPERATION_MODE_NORMAL);
    
    }
    static void MCANIntrConfig(void)
    {
    
        Interrupt_initModule();
        Interrupt_initVectorTable();
        Interrupt_register(INT_MCANSS1,&MCANIntr1ISR);
        Interrupt_enable(INT_MCANSS1);
        Interrupt_enableMaster();
    
    }
    
    //
    // This is Interrupt Service Routine for MCAN interrupt 1.
    //
    __interrupt void MCANIntr1ISR(void)
    {
        GPIO_writePin(40,1);
        uint32_t intrStatus;
        int1++;
        intrStatus = MCAN_getIntrStatus(MCAN0_BASE);
        MCAN_getNewDataStatus(MCAN0_BASE, &newData);
        MCAN_readMsgRam(MCAN0_BASE, MCAN_MEM_TYPE_BUF, 0, 0, &rxMsg1);
        rxMsg[loopCnt] = rxMsg1;
        MCAN_clearNewDataStatus(MCAN0_BASE, &newData);
        HW_WR_FIELD32(MCAN0_BASE + MCAN_MCANSS_EOI, MCAN_MCANSS_EOI, 0x2U);
        MCAN_clearIntrStatus(MCAN0_BASE, intrStatus);
    
        //
        // Update the flag value.
        //
        isrIntr1Flag = 0U;
    
        //
        // Acknowledge this interrupt located in group 9
        //
        Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
        GPIO_writePin(40,0);
    }
    

    第154行至第157行:设置 启用仅中断源 MCAN_IR_RF0N_MASK。

    行 318和347:数字输出设置。

    行320:中断计数器。

    我发现当我收到一条消息时,它会输入两次中断,我的期望是只输入一次中断。

    然后,我使用数字输出来观看CANFD信号,以及中断何时进入。 实际上,它在收到消息后中断了两次。

    我已阻止其他中断源(line154),是否有其他原因?

    非常感谢!!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Sean,  

    我们正在审查您的查询,我们将很快回复您。

    谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Sahil:

    对这个问题有什么建议? 感谢您的帮助!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Sean,

    您能否帮助我了解您正在传输多少数据包,您所附的波形不是很清楚?

    此外,您能否告诉我们,每次您点击ISR时,'intrStatus'变量的状态是什么(以了解中断的来源)?

    此致,

    Praveen