This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280049C:使用 EEPROM 的 I2C 外设

Guru**** 2529560 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1105896/tms320f280049c-i2c-peripheral-using-eeprom

器件型号:TMS320F280049C

您好!
我正在使用外设示例代码"i2c_EEPROM"。但无法从 EEPROM 读取数据。
我的 EEPROM 器件型号为24C04。
我随附以下代码、请检查一次。

I2C_ex2_EEPROM.c

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Prem、

    我们正在努力将其分配给正确的主题专家。  请给我们另外一天答复。

    最棒的

    Matthew

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Prem、

    从您的消息中不清楚您看到的是哪种故障。 EEPROM 是否为 NACKing?

    I2C_ex2_EEPROM 示例已过时。 我建议您考虑以下 EEPROM I2C 示例:

    如果首选轮询方法、请使用 i2c_ex4_EEPROM_POLLING 示例

    如果首选中断方法、请使用 i2c_ex6_EEPROM_INTERRUPT 示例。

    此致、

    曼诺伊

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生、
    首先感谢您。

    正如您说过的" i2c_ex4_EEPROM_POLLING 示例"、我正在进行这方面的工作。

    但是、对于 上述示例、我有一个疑问、即如何发送一个字节地址。

    我使用的是24C04 EEPROM、下面是写入地址格式。

    请检查一次、并向我提供建议。

    谢谢你。

     

    #include "driverlib.h"
    #include "device.h"
    
    #include "i2cLib_FIFO_polling.h"
    
    //
    // Globals
    //
    struct I2CHandle EEPROM;
    
    struct I2CHandle *currentMsgPtr;                   // Used in interrupt
    
    
    uint16_t passCount = 0;
    uint16_t failCount = 0;
    
    uint16_t AvailableI2C_slaves[1];
    uint16_t TX_MsgBuffer[MAX_BUFFER_SIZE];
    uint16_t RX_MsgBuffer[MAX_BUFFER_SIZE];
    uint32_t ControlAddr;
    uint16_t status;
    
    
    //void fail(void);
    //void pass(void);
    
    void I2C_GPIO_init(void);
    void I2Cinit(void);
    void verifyEEPROMRead(void);
    
    //
    // Main
    //
    void main(void)
    {
        //
        // Initialize device clock and peripherals
        //
        Device_init();
    
        //
        // Disable pin locks and enable internal pullups.
        //
        Device_initGPIO();
    
        //
        // Initialize I2C pins
        //
        I2C_GPIO_init();
    
        //
        // Initialize PIE and clear PIE registers. Disable CPU interrupts.
        //
        Interrupt_initModule();
    
        //
        // Initialize the PIE vector table with pointers to the shell Interrupt
        // Service Routines (ISR).
        //
        Interrupt_initVectorTable();
    
        I2Cinit();
    
        //I2Cs connected to I2CA will be found in AvailableI2C_slaves buffer
        //after you run I2CBusScan function.
        uint16_t *pAvailableI2C_slaves = AvailableI2C_slaves;
        status = I2CBusScan(I2CA_BASE, pAvailableI2C_slaves);
    
        uint16_t i;
    
        for(i=0;i<MAX_BUFFER_SIZE;i++)
        {
            TX_MsgBuffer[i] = 0;
            RX_MsgBuffer[i] = 0;
        }
    
        EEPROM.SlaveAddr      = 0x50;
        EEPROM.base           = I2CA_BASE;
        EEPROM.pControlAddr   = &ControlAddr;
        EEPROM.NumOfAddrBytes = 1;
        EEPROM.pTX_MsgBuffer  = TX_MsgBuffer;
        EEPROM.pRX_MsgBuffer  = RX_MsgBuffer;
        EEPROM.NumOfAttempts  = 5;
        EEPROM.Delay_us       = 10;
        EEPROM.WriteCycleTime_in_us = 6000;    //10ms for EEPROM this code was tested
    
        //Example 1: EEPROM Byte Write
        //Write 11 to EEPROM address 0x0
        ControlAddr = 0;
        EEPROM.NumOfDataBytes = 1;
        TX_MsgBuffer[0]       = 11;
    //    TX_MsgBuffer[1]       = 11;
        status = I2C_MasterTransmitter(&EEPROM);
    
        //Wait for EEPROM write cycle time
        //This delay is not mandatory. User can run their application code instead.
        //It is however important to wait for EEPROM write cycle time before you initiate
        //another read / write transaction
        DEVICE_DELAY_US(EEPROM.WriteCycleTime_in_us);
    
        //Example 2: EEPROM Byte Read
        //Make sure 11 is written to EEPROM address 0x0
        ControlAddr = 0;
        EEPROM.pControlAddr   = &ControlAddr;
        EEPROM.NumOfDataBytes = 1;
        status = I2C_MasterReceiver(&EEPROM);
    
        while(I2C_getStatus(EEPROM.base) & I2C_STS_BUS_BUSY);
    
        verifyEEPROMRead();
    
    //    //Example 3: EEPROM word (16-bit) write
    //    //EEPROM address 0x1 = 22 &  0x2 = 33
    //    ControlAddr = 1;   //EEPROM address to write
    //    EEPROM.NumOfDataBytes  = 2;
    //    TX_MsgBuffer[0]        = 0x11;
    //    TX_MsgBuffer[1]        = 0x22;
    //    EEPROM.pTX_MsgBuffer   = TX_MsgBuffer;
    //    status = I2C_MasterTransmitter(&EEPROM);
    //
    //    //Wait for EEPROM write cycle time
    //    //This delay is not mandatory. User can run their application code instead.
    //    //It is however important to wait for EEPROM write cycle time before you initiate
    //    //another read / write transaction
    //    DEVICE_DELAY_US(EEPROM.WriteCycleTime_in_us);
    //
    //    //Example 4: EEPROM word (16-bit) read
    //     //Make sure EEPROM address 1 has 0x11 and 2 has 0x22
    //     ControlAddr = 1;
    //     EEPROM.pControlAddr   = &ControlAddr;
    //     EEPROM.pRX_MsgBuffer  = RX_MsgBuffer;
    //     EEPROM.NumOfDataBytes = 2;
    //
    //     status = I2C_MasterReceiver(&EEPROM);
    //
    //     verifyEEPROMRead();
    
    //
    //    //Example 5: EEPROM Page write
    //    //Program address = data pattern from address 64
    //
    //    for(i=0;i<MAX_BUFFER_SIZE;i++)
    //    {
    //        TX_MsgBuffer[i] = i+64;
    //    }
    //
    //    ControlAddr = 4;   //EEPROM address to write
    //    EEPROM.NumOfDataBytes  = MAX_BUFFER_SIZE;
    //    EEPROM.pTX_MsgBuffer   = TX_MsgBuffer;
    //    status = I2C_MasterTransmitter(&EEPROM);
    //
    //    //Wait for EEPROM write cycle time
    //    //This delay is not mandatory. User can run their application code instead.
    //    //It is however important to wait for EEPROM write cycle time before you initiate
    //    //another read / write transaction
    //    DEVICE_DELAY_US(EEPROM.WriteCycleTime_in_us);
    //
    //    //Example 6: EEPROM word Paged read
    //    ControlAddr = 4;
    //    EEPROM.pControlAddr   = &ControlAddr;
    //    EEPROM.pRX_MsgBuffer  = RX_MsgBuffer;
    //    EEPROM.NumOfDataBytes = MAX_BUFFER_SIZE;
    //
    //    status = I2C_MasterReceiver(&EEPROM);
    //
    //    verifyEEPROMRead();
    //
        if(status)
        {
            fail();
        }
        else
        {
            pass();
        }
    
    }
    
    //
    // pass - Function to be called if data written matches data read
    //
    void
    pass(void)
    {
        asm("   ESTOP0");
                       for(;;);
    }
    
    //
    // fail - Function to be called if data written does NOT match data read
    //
    void fail(void)
    {
        asm("   ESTOP0");
        for(;;);
    }
    
    void verifyEEPROMRead(void)
    {
        uint16_t i;
        while(I2C_getStatus(EEPROM.base) & I2C_STS_BUS_BUSY);
    
        for(i=0;i<=EEPROM.NumOfDataBytes;i++)
        {
            if(RX_MsgBuffer[i] != TX_MsgBuffer[i])
            {
                //Transmitted data doesn't match received data
                //Fail condition. PC shouldn't reach here
                ESTOP0;
    //            fail();
            }
        }
    }
    
    
    void I2C_GPIO_init(void)
    {
        // I2CA pins (SDAA / SCLA)
        GPIO_setDirectionMode(DEVICE_GPIO_PIN_SDAA, GPIO_DIR_MODE_IN);
        GPIO_setPadConfig(DEVICE_GPIO_PIN_SDAA, GPIO_PIN_TYPE_PULLUP);
        GPIO_setQualificationMode(DEVICE_GPIO_PIN_SDAA, GPIO_QUAL_ASYNC);
    
        GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCLA, GPIO_DIR_MODE_IN);
        GPIO_setPadConfig(DEVICE_GPIO_PIN_SCLA, GPIO_PIN_TYPE_PULLUP);
        GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCLA, GPIO_QUAL_ASYNC);
    
        GPIO_setPinConfig(DEVICE_GPIO_CFG_SDAA);
        GPIO_setPinConfig(DEVICE_GPIO_CFG_SCLA);
    }
    
    void I2Cinit(void)
    {
        //myI2CA initialization
        I2C_disableModule(I2CA_BASE);
        I2C_initMaster(I2CA_BASE, DEVICE_SYSCLK_FREQ, 400000, I2C_DUTYCYCLE_50);
        I2C_setConfig(I2CA_BASE, I2C_MASTER_SEND_MODE);
        I2C_setSlaveAddress(I2CA_BASE, 0x50);
        I2C_setOwnSlaveAddress(I2CA_BASE, 96); //I2CA address
        I2C_disableLoopback(I2CA_BASE);
        I2C_setBitCount(I2CA_BASE, I2C_BITCOUNT_8);
        I2C_setDataCount(I2CA_BASE, 2);
        I2C_setAddressMode(I2CA_BASE, I2C_ADDR_MODE_7BITS);
        I2C_enableFIFO(I2CA_BASE);
        I2C_clearInterruptStatus(I2CA_BASE, I2C_INT_ARB_LOST | I2C_INT_NO_ACK);
        I2C_setFIFOInterruptLevel(I2CA_BASE, I2C_FIFO_TXEMPTY, I2C_FIFO_RX12);
        I2C_enableInterrupt(I2CA_BASE, I2C_INT_ADDR_SLAVE | I2C_INT_ARB_LOST | I2C_INT_NO_ACK | I2C_INT_STOP_CONDITION);
        I2C_setEmulationMode(I2CA_BASE, I2C_EMULATION_FREE_RUN);
        I2C_enableModule(I2CA_BASE);
    }
    
    //
    // End of File
    //
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您需要使用 示例1:EEPROM 字节写入。 它生成起始条件+ TX 目标地址 + TX 数据

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生、
    感谢你的答复。
    EEPROM 字节写入正常 SIR 我理解、但字节读取:我没有获得读取操作。
    我想在读取操作中:它读取器件地址+ RX 数据。 我是对的吗?
    您能不能支持我解决 EEPROM 的读取操作问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    首先、请确认您的设置中的 EEPROM 字节写入是否正常。

    以下是 EEPROM 读取字节命令的工作方式:

    EEPROM 字节读取:

    开始+ TX 从地址+ TX EEPROM 读取地址(MSB)+  TX EEPROM 读取地址(LSB)+重复开始+ RX 读取字节、如下所示

    您是否在逻辑分析仪上检查了 I2C 总线?

    此致、

    曼诺伊

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、先生、
    下面是我的 I2C 写入操作、我在逻辑分析仪上检查了。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    了解 EEPROM 写入操作是否正常。 希望您也能使 EEPROM 读取操作正常工作

    注意事项