This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28377S-Q1:需要重新选择 MCU 芯片、希望其功能/性能为 F28377S-Q1 + CAN FD

Guru**** 2616675 points

Other Parts Discussed in Thread: TMS320F28377S-Q1, TMS320F28384S-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1109670/tms320f28377s-q1-need-to-re-select-an-mcu-chip-hope-its-function-performance-is-f28377s-q1-can-fd

器件型号:TMS320F28377S-Q1
主题中讨论的其他器件: TMS320F28384S-Q1

当前使用的 MCU 芯片是 TMS320F28377S-Q1、因为该芯片与 CAN 2.0集成、为了与 CAN FD 兼容、需要重新选择 MCU 芯片、希望其功能/性能为 F28377S-Q1 + CAN FD、请帮助推荐 MCU 芯片。

此外、TMS320F28384S-Q1是否满足要求?

谢谢!