This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDM-1000:AMC1301的输入电压范围

Guru**** 2782615 points

Other Parts Discussed in Thread: AMC1301

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1119769/tidm-1000-the-input-voltage-range-of-amc1301

器件型号:TIDM-1000
主题中讨论的其他器件:AMC1301

您好!

VOUT 可达800V,V_ P 为400V,amc1301的输入为400/3002.74*2.74=0.365v,超出了 amc1301的输入电压范围。 即使输出电压为700V、amc1301的输入也是350/3002.74*2.74=0.3194v、这超出了 amc1301的输入电压范围。