This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LAUNCHXL-F28379D:外部电源范围和发光 LED D7和 D8的指示

Guru**** 2124380 points
Other Parts Discussed in Thread: TMS320F28379D
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1122726/launchxl-f28379d-external-power-supply-range-and-indication-of-glowing-led-d7-and-d8

器件型号:LAUNCHXL-F28379D
主题中讨论的其他器件:TMS320F28379D

外部5V 电源的最大范围是多少? 对于外部3.3V、提到4.6是允许的最大电压、但没有提供外部5V 电源的此类信息。 请尽早答复。

LED D7和 D8发光的含义是什么? 它提供了什么类型的信号? 比如 LaunchPad 已损坏或发生了一些故障?