主题中讨论的其他器件:TMS320F28379D、 C2000WARE
大家好、
我想通过 CAN 协议向本地 PC 发送 ADC 数据。 目前、我使用的是 C2000 Launchpad 板和 CAN_EXTERNAL_Transmit。c 示例文件。 我对板载收发器的代码进行了更改。 我正在使用 PCANVIEW 软件、但无法在 PC 上查看数据。 它显示状态为-错误认可并显示错误帧。 我已经在示波器上检查了 CANH 和 CANL,它们工作正常。 是否有人能帮助我纠正此问题、以便我可以在本地 PC (PCANVIEW)上查看数据。
规格-
tms320f28379d launchpad
c200ware - 4 01
CCS - 11.2
// // FILE: can_external_transmit.c // // TITLE: Example to demonstrate CAN external transmission // //! \addtogroup cpu01_example_list //! <h1>CAN-A to CAN-B External Transmit (can_external_transmit)</h1> //! //! This example initializes CAN module A and CAN module B for external //! communication. CAN-A module is setup to transmit incrementing data for "n" //! number of times to the CAN-B module, where "n" is the value of TXCOUNT. //! CAN-B module is setup to trigger an interrupt service routine (ISR) when //! data is received. An error flag will be set if the transmitted data doesn't //! match the received data. //! //! \note Both CAN modules on the device need to be //! connected to each other via CAN transceivers. //! //! \b Hardware \b Required \n //! - A C2000 board with two CAN transceivers //! //! \b External \b Connections \n //! - ControlCARD CANA is on GPIO31 (CANTXA) and GPIO30 (CANRXA) //! - ControlCARD CANB is on GPIO8 (CANTXB) and GPIO10 (CANRXB) //! //! \b Watch \b Variables \n //! - TXCOUNT - Adjust to set the number of messages to be transmitted //! - txMsgCount - A counter for the number of messages sent //! - rxMsgCount - A counter for the number of messages received //! - txMsgData - An array with the data being sent //! - rxMsgData - An array with the data that was received //! - errorFlag - A flag that indicates an error has occurred //! // //########################################################################### // $TI Release: F2837xD Support Library v3.05.00.00 $ // $Release Date: Thu Oct 18 15:48:42 CDT 2018 $ // $Copyright: // Copyright (C) 2013-2018 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //########################################################################### // // Included Files // #include "F28x_Project.h" // Device Headerfile and Examples Include File #include <stdint.h> #include <stdbool.h> #include "inc/hw_types.h" #include "inc/hw_memmap.h" #include "inc/hw_can.h" #include "driverlib/can.h" // // Defines // #define TXCOUNT 100 #define MSG_DATA_LENGTH 4 #define TX_MSG_OBJ_ID 1 #define RX_MSG_OBJ_ID 1 // // Globals // volatile unsigned long i; volatile uint32_t txMsgCount = 0; volatile uint32_t rxMsgCount = 0; volatile uint32_t errorFlag = 0; unsigned char txMsgData[4]; unsigned char rxMsgData[4]; uint32_t canBitRate = 0; uint32_t status; tCANMsgObject sTXCANMessage; tCANMsgObject sRXCANMessage; // // Function Prototypes // __interrupt void canbISR(void); // // Main // void main(void) { // // Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // InitSysCtrl(); // // Initialize GPIO and configure GPIO pins for CANTX/CANRX // on module A and B // InitGpio(); // // Setup GPIO pin mux for CAN-A TX/RX and CAN-B TX/RX // GPIO_SetupPinMux(17, GPIO_MUX_CPU1, 2); //GPIO30 - CANRXA GPIO_SetupPinOptions(17, GPIO_INPUT, GPIO_ASYNC); GPIO_SetupPinMux(12, GPIO_MUX_CPU1, 2); //GPIO31 - CANTXA GPIO_SetupPinOptions(12, GPIO_OUTPUT, GPIO_PUSHPULL); /* GPIO_SetupPinMux(10, GPIO_MUX_CPU1, 2); //GPIO10 - CANRXB GPIO_SetupPinOptions(10, GPIO_INPUT, GPIO_ASYNC); GPIO_SetupPinMux(8, GPIO_MUX_CPU1, 2); //GPIO8 - CANTXB GPIO_SetupPinOptions(8, GPIO_OUTPUT, GPIO_PUSHPULL); */ // // Initialize the CAN controllers // //CANInit(CANA_BASE); CANInit(CANB_BASE); // // Setup CAN to be clocked off the PLL output clock // //CANClkSourceSelect(CANA_BASE, 0); // 500kHz CAN-Clock CANClkSourceSelect(CANB_BASE, 0); // 500kHz CAN-Clock // // Set up the CAN bus bit rate to 500kHz for each module // This function sets up the CAN bus timing for a nominal configuration. // You can achieve more control over the CAN bus timing by using the // function CANBitTimingSet() instead of this one, if needed. // Additionally, consult the device data sheet for more information about // the CAN module clocking. // //CANBitRateSet(CANA_BASE, 200000000, 500000); canBitRate = CANBitRateSet(CANB_BASE, 200000000, 500000); // // Enable interrupts on the CAN B peripheral. // CANIntEnable(CANB_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS); // // Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts // DINT; // // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // InitPieCtrl(); // // Disable CPU interrupts and clear all CPU interrupt flags // IER = 0x0000; IFR = 0x0000; // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // InitPieVectTable(); // // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. // This registers the interrupt handler in PIE vector table. // EALLOW; PieVectTable.CANB0_INT = canbISR; EDIS; // // Enable the CAN-B interrupt on the processor (PIE). // PieCtrlRegs.PIEIER9.bit.INTx7 = 1; IER |= M_INT9; EINT; // // Enable the CAN-B interrupt signal // CANGlobalIntEnable(CANB_BASE, CAN_GLB_INT_CANINT0); // // Initialize the transmit message object used for sending CAN messages. // Message Object Parameters: // Message Identifier: 0x5555 // Message ID Mask: 0x0 // Message Object Flags: None // Message Data Length: 4 Bytes // Message Transmit data: txMsgData // sTXCANMessage.ui32MsgID = 0x0005; sTXCANMessage.ui32MsgIDMask = 0; sTXCANMessage.ui32Flags = 0; sTXCANMessage.ui32MsgLen = MSG_DATA_LENGTH; sTXCANMessage.pucMsgData = txMsgData; // // Initialize the receive message object used for receiving CAN messages. // Message Object Parameters: // Message Identifier: 0x5555 // Message ID Mask: 0x0 // Message Object Flags: Receive Interrupt // Message Data Length: 4 Bytes // Message Receive data: rxMsgData // sRXCANMessage.ui32MsgID = 0x0005; sRXCANMessage.ui32MsgIDMask = 0; sRXCANMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE; sRXCANMessage.ui32MsgLen = MSG_DATA_LENGTH; sRXCANMessage.pucMsgData = rxMsgData; //CANMessageSet(CANB_BASE, RX_MSG_OBJ_ID, &sRXCANMessage, // MSG_OBJ_TYPE_RX); // // Initialize the transmit message object data buffer to be sent // txMsgData[0] = 0x12; txMsgData[1] = 0x34; txMsgData[2] = 0x56; txMsgData[3] = 0x78; // // Start CAN module A and B operations // //CANEnable(CANA_BASE); CANEnable(CANB_BASE); // // Transmit messages from CAN-A to CAN-B // for(;;) { // // Transmit Message // CANMessageSet(CANB_BASE, TX_MSG_OBJ_ID, &sTXCANMessage, MSG_OBJ_TYPE_TX); status = CANStatusGet(CANB_BASE,CAN_STS_TXREQUEST); DELAY_US(1000 * 1000); } // // Stop application // asm(" ESTOP0"); } // // CAN B ISR - The interrupt service routine called when a CAN interrupt is // triggered on CAN module B. // __interrupt void canbISR(void) { uint32_t status; // // Read the CAN-B interrupt status to find the cause of the interrupt // status = CANIntStatus(CANB_BASE, CAN_INT_STS_CAUSE); // // If the cause is a controller status interrupt, then get the status // if(status == CAN_INT_INT0ID_STATUS) { // // Read the controller status. This will return a field of status // error bits that can indicate various errors. Error processing // is not done in this example for simplicity. Refer to the // API documentation for details about the error status bits. // The act of reading this status will clear the interrupt. // status = CANStatusGet(CANB_BASE, CAN_STS_CONTROL); // // Check to see if an error occurred. // if(((status & ~(CAN_ES_RXOK)) != 7) && ((status & ~(CAN_ES_RXOK)) != 0)) { // // Set a flag to indicate some errors may have occurred. // errorFlag = 1; } } // // Check if the cause is the CAN-B receive message object 1 // else if(status == RX_MSG_OBJ_ID) { // // Get the received message // CANMessageGet(CANB_BASE, RX_MSG_OBJ_ID, &sRXCANMessage, true); // // Getting to this point means that the RX interrupt occurred on // message object 1, and the message RX is complete. Clear the // message object interrupt. // CANIntClear(CANB_BASE, RX_MSG_OBJ_ID); // // Increment a counter to keep track of how many messages have been // received. In a real application this could be used to set flags to // indicate when a message is received. // rxMsgCount++; // // Since the message was received, clear any error flags. // errorFlag = 0; } // // If something unexpected caused the interrupt, this would handle it. // else { // // Spurious interrupt handling can go here. // } // // Clear the global interrupt flag for the CAN interrupt line // CANGlobalIntClear(CANB_BASE, CAN_GLB_INT_CANINT0); // // Acknowledge this interrupt located in group 9 // PieCtrlRegs.PIEACK.all = PIEACK_GROUP9; } // // End of File